Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Preferred power supply connections?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 188 subscribers
  • Views 1990 views
  • Users 0 members are here
Related

Preferred power supply connections?

e14 Contributor
e14 Contributor over 16 years ago

The schematic I am "capturing" are based on public domain circuits for

audio processing modules in a modular analog synthesizer. There are some

standard power connection schemes which I intend to follow consisting of

+/- 15 Vdc and ground. Typically, the +/- supplies go through a ferrite

bead and a couple of filtering capacitors before hitting the PCB's power

nets.

 

What is the best way to make a power net for the PCB components bcause it

is separated from the power input jack by the ferrite bead? If I connect

the connector pins to the supply +15 and -15 nets, I can't use them on the

PCB. So, what is the best net to use to PCB components to the other side of

the ferrite beads? Should use one of the other available supply nets or

make a unique power net?

 

I have played with different ways to do it, and they seem to work, but as

I'm new at this capture stuff, I'd like to know if there are standard or

preferred ways to accomplish this.

 

This image kind of shows what I mean.

 

Thanks

David

 

 

 

--

Browser access to CadSoft Support Forums at http://www.eaglecentral.ca

 

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 16 years ago

    Olin wrote on Thu, 25 February 2010 12:49

    dingebre wrote on Thu, 25 February 2010 11:42

    Hi Olin, you're reading too much into the "design". This is not a

    real schematic.

     

    I'm only illustrating the power connections.

     

    It is still a good idea to keep in mind that neatness counts,

    especially when you are presenting to others.  Some may look past that,

    but why allow it to be a issue when it would only have taken a extra

    minute to make things more readable?

     

    Quote:

    I only ask a little patience. I'm very new to using Eagle and want

    to learn good habits. Would you maybe take a second look? I'd like some

    advice about how to handle the power nets on the "real" circuits I'd

    like to work on.

     

    I don't use specific parts at all to label power nets.  I don't treat

    power nets any different from other nets that are drawn in separate

    pieces, although I've seen others use explicit power symbols commonly.

    In Eagle, nets in the schematic are automatically connected if they have

    the same name.  To show airwires in a Eagle schematic, I name the nets

    and then use DRAW LABEL to show the net name in the schematic.  It's

    important to use DRAW LABEL instead of TEXT because DRAW LABEL shows the

    true net name as Eagle understands it.  If you change the net name, the

    text drawn with DRAW LABEL will automatically change.

     

    For power nets I use names like "5V", "-12V", "BATT", or whatever I

    think will be most descriptive in context of that schematic.  I also like

    to show power connections on top, ground on the bottom, with signal from

    left to right to the extent this can be reasonably done.  Keep in mind

    that the schematic is not only to define the machine readable connections

    to Eagle, but it is also the primary documentation of your circuit to

    humans.  As such, neatness and clarity are very important

    considerations.

     

    Quote:

    Should I do it kind of like in that illustration? Use the supply

    library  +/- 15 for the plug and then a generic supply symbol to

    connect the +/- supplies on the components? Or is there a better way?

     

    You'll probably find as many opinions as people.  There are several

    reasonably "right" ways.  I've tried to explain what I do, but I

    recognize there are other ways that others prefer.  As long as Eagle

    understands the connections, there aren't hidden gotchas for making

    changes, and your circuit is easy to understand from the schematic, then

    it's a acceptable method.

     

    You can take a look at

    http://www.embedinc.com/products/usbprog/eusb3.pdf as a example of how I

    do things.  The first page is the main power supply.  Note all the named

    wires ending at the right side because the logical flow is out from the

    power supply.  You can see various other places in the schematic that

    connect to these power rails, usually coming in from the top or left as a

    simple visual reference that the power is coming in instead of being

    produced there.  Note that no explicit power symbols were used, just

    named nets with carefully placed labels.

     

     

     

    Thanks Olin! I am used to a different commercial application which makes

    things like this so difficult. Right now, the hardest part of my learning

    curve is accepting how much simpler and more logical Eagle is compared to

    what I have been using. I keep expecting Eagle to be much more cryptic...

     

    Thanks for taking the time to share your thoughts. They are really helping

    me get in the "Eagle" mindset. Next time I put up project, I'll clean it

    up.

     

    David

     

     

    --

    Browser access to CadSoft Support Forums at http://www.eaglecentral.ca

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 16 years ago

    Olin wrote on Thu, 25 February 2010 12:49

    dingebre wrote on Thu, 25 February 2010 11:42

    Hi Olin, you're reading too much into the "design". This is not a

    real schematic.

     

    I'm only illustrating the power connections.

     

    It is still a good idea to keep in mind that neatness counts,

    especially when you are presenting to others.  Some may look past that,

    but why allow it to be a issue when it would only have taken a extra

    minute to make things more readable?

     

    Quote:

    I only ask a little patience. I'm very new to using Eagle and want

    to learn good habits. Would you maybe take a second look? I'd like some

    advice about how to handle the power nets on the "real" circuits I'd

    like to work on.

     

    I don't use specific parts at all to label power nets.  I don't treat

    power nets any different from other nets that are drawn in separate

    pieces, although I've seen others use explicit power symbols commonly.

    In Eagle, nets in the schematic are automatically connected if they have

    the same name.  To show airwires in a Eagle schematic, I name the nets

    and then use DRAW LABEL to show the net name in the schematic.  It's

    important to use DRAW LABEL instead of TEXT because DRAW LABEL shows the

    true net name as Eagle understands it.  If you change the net name, the

    text drawn with DRAW LABEL will automatically change.

     

    For power nets I use names like "5V", "-12V", "BATT", or whatever I

    think will be most descriptive in context of that schematic.  I also like

    to show power connections on top, ground on the bottom, with signal from

    left to right to the extent this can be reasonably done.  Keep in mind

    that the schematic is not only to define the machine readable connections

    to Eagle, but it is also the primary documentation of your circuit to

    humans.  As such, neatness and clarity are very important

    considerations.

     

    Quote:

    Should I do it kind of like in that illustration? Use the supply

    library  +/- 15 for the plug and then a generic supply symbol to

    connect the +/- supplies on the components? Or is there a better way?

     

    You'll probably find as many opinions as people.  There are several

    reasonably "right" ways.  I've tried to explain what I do, but I

    recognize there are other ways that others prefer.  As long as Eagle

    understands the connections, there aren't hidden gotchas for making

    changes, and your circuit is easy to understand from the schematic, then

    it's a acceptable method.

     

    You can take a look at

    http://www.embedinc.com/products/usbprog/eusb3.pdf as a example of how I

    do things.  The first page is the main power supply.  Note all the named

    wires ending at the right side because the logical flow is out from the

    power supply.  You can see various other places in the schematic that

    connect to these power rails, usually coming in from the top or left as a

    simple visual reference that the power is coming in instead of being

    produced there.  Note that no explicit power symbols were used, just

    named nets with carefully placed labels.

     

     

     

    Thanks Olin! I am used to a different commercial application which makes

    things like this so difficult. Right now, the hardest part of my learning

    curve is accepting how much simpler and more logical Eagle is compared to

    what I have been using. I keep expecting Eagle to be much more cryptic...

     

    Thanks for taking the time to share your thoughts. They are really helping

    me get in the "Eagle" mindset. Next time I put up project, I'll clean it

    up.

     

    David

     

     

    --

    Browser access to CadSoft Support Forums at http://www.eaglecentral.ca