Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Preferred power supply connections?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 188 subscribers
  • Views 1989 views
  • Users 0 members are here
Related

Preferred power supply connections?

e14 Contributor
e14 Contributor over 16 years ago

The schematic I am "capturing" are based on public domain circuits for

audio processing modules in a modular analog synthesizer. There are some

standard power connection schemes which I intend to follow consisting of

+/- 15 Vdc and ground. Typically, the +/- supplies go through a ferrite

bead and a couple of filtering capacitors before hitting the PCB's power

nets.

 

What is the best way to make a power net for the PCB components bcause it

is separated from the power input jack by the ferrite bead? If I connect

the connector pins to the supply +15 and -15 nets, I can't use them on the

PCB. So, what is the best net to use to PCB components to the other side of

the ferrite beads? Should use one of the other available supply nets or

make a unique power net?

 

I have played with different ways to do it, and they seem to work, but as

I'm new at this capture stuff, I'd like to know if there are standard or

preferred ways to accomplish this.

 

This image kind of shows what I mean.

 

Thanks

David

 

 

 

--

Browser access to CadSoft Support Forums at http://www.eaglecentral.ca

 

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

    Gary Gofstein wrote on Thu, 25 February 2010 20:56

    Surprisingly nobody has mentioned EAGLE's gotcha with respect to power

    supplies. EAGLE parts have named power supply pins that automatically

    connect to the net of the same name.

     

    Yes, this is a nasty hidden gotcha.  I do what Gary does, which is never to

    use implicit power connections, at least not on purpose.  Unfortunately

    they can still bite you if you forget a connection.  It also helps to never

    use the Eagle supplied libraries.

    --

    Browser access to CadSoft Support Forums at http://www.eaglecentral.ca

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago

    Gary Gofstein wrote on Thu, 25 February 2010 20:56

    Surprisingly nobody has mentioned EAGLE's gotcha with respect to power

    supplies. EAGLE parts have named power supply pins that automatically

    connect to the net of the same name.

     

    Yes, this is a nasty hidden gotcha.  I do what Gary does, which is never to

    use implicit power connections, at least not on purpose.  Unfortunately

    they can still bite you if you forget a connection.  It also helps to never

    use the Eagle supplied libraries.

    --

    Browser access to CadSoft Support Forums at http://www.eaglecentral.ca