Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Circle to NET
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 850 views
  • Users 0 members are here
Related

Circle to NET

autodeskguest
autodeskguest over 16 years ago

How do I connect a circle to a NET?

I want to draw a circle and connect that circle to ground.

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

    On 4/21/2010 4:44 PM, Dang Tran wrote:

    The arc command, when trying to make a circle is not as accurate as the

    circle command.

    Say I want to use the arc command to create a circle with a radius of 9.5mm

    centered at (20mm,20mm)

    My calculation for creating the circle using the arc command are (20,29.5)

    to (20.17,29.5) Curve = -359.

    If you try it in eagle the center is off.

     

     

    just make 2 semicircles and overlap them. this is a good use for the

    COPY command ( which really duplicates objects).

     

    i don't think the 2nd coordinate is a point that is drawn, it is just

    used to define the diameter and that leads to an error since you don't

    have the correct diameter. i can't offer you a better answer since I use

    v4 which is slightly different but I can do it with semicircles exactly.

    watch out for grid settings.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago

    On 4/21/2010 4:44 PM, Dang Tran wrote:

    The arc command, when trying to make a circle is not as accurate as the

    circle command.

    Say I want to use the arc command to create a circle with a radius of 9.5mm

    centered at (20mm,20mm)

    My calculation for creating the circle using the arc command are (20,29.5)

    to (20.17,29.5) Curve = -359.

    If you try it in eagle the center is off.

     

     

    just make 2 semicircles and overlap them. this is a good use for the

    COPY command ( which really duplicates objects).

     

    i don't think the 2nd coordinate is a point that is drawn, it is just

    used to define the diameter and that leads to an error since you don't

    have the correct diameter. i can't offer you a better answer since I use

    v4 which is slightly different but I can do it with semicircles exactly.

    watch out for grid settings.