EAGLE User Chat (English) Harddrive and cdrom drive power connector.
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
  • Replies 5 replies
  • Subscribers 178 subscribers
  • Views 558 views
  • Users 0 members are here
Related

Harddrive and cdrom drive power connector.

autodeskguest
autodeskguest over 15 years ago

Hi all.

 

From past experience, I have learned that if I can not google the

problem, it does not exists.

 

Problem:

I would like to use a standard 5.25" bay power connector, the types on

IDE CD/HD Drives, on my pcb.

 

I have been unable to find the right name for it.

This is the wire-part of it:

http://en.wikipedia.org/wiki/Molex_connector#Disk_drive_connector_.28Molex_8981_Series_Power_Connector.29

 

it says it should be a molex 8981 series connector.

 

This is another page, showing the same connector:

http://www.playtool.com/pages/psuconnectors/connectors.html#peripheral

 

It says it is from the 1-48* series by AMP.

 

 

I have had no luck in finding any of them in eagle lbr's, but nor have I

found anyone else *** about the problem... So what am I doing wrong?

 

 

/Jan Rasmussen - not using eagle as much as he should.

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 15 years ago

    Den 06-06-2010 21:11, Jim Littlefield skrev:

     

    http://www.edaboard.com/ftopic309290.html

     

    Has a bunch of links...maybe one is what you are looking for? I did not

    find an obvious match in the Eagle libs...buts its only a 4 contact part

    so should not be hard to make your own.

     

     

    Yes I know, and by the looks of it, it would be more safe to get an

    connector and measure it, before making the layout, as there seams to be

    some confusion as there where it is 0.156" or 0.2" and so on.

     

    Was just hoping that Eagle had a component ready, but then again, what

    are the chances that the plug I get hold of, fits that image

     

    /Jan Rasmussen

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 15 years ago

    Den 06-06-2010 21:11, Jim Littlefield skrev:

     

    http://www.edaboard.com/ftopic309290.html

     

    Has a bunch of links...maybe one is what you are looking for? I did not

    find an obvious match in the Eagle libs...buts its only a 4 contact part

    so should not be hard to make your own.

     

     

    Yes I know, and by the looks of it, it would be more safe to get an

    connector and measure it, before making the layout, as there seams to be

    some confusion as there where it is 0.156" or 0.2" and so on.

     

    Was just hoping that Eagle had a component ready, but then again, what

    are the chances that the plug I get hold of, fits that image

     

    /Jan Rasmussen