Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Simplifying complex and many connections
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 187 subscribers
  • Views 977 views
  • Users 0 members are here
Related

Simplifying complex and many connections

autodeskguest
autodeskguest over 11 years ago

I'm working on a schematic with several pairs of 40 pin connectors where

one PCB connector connects to a 40 pin IDC ribbon cable connector (i.e.

pin 1-1, in 2-2 etc.).

In other words, an awful mess when attaching wires between these pins.

 

I seem to recall a feature in Eagle which allows for attaching the wires

correctly as usual in the PCB layout but does away with the mess in the

schematic.

Also, is there a quick way to attach those wires between the same

numbered pins of two connectors? It takes an awful long time to do it

manually.

 

I'm using Eagle 7.2.0 on the Mac OSX platform. Thanks.

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    Hi,

     

    Try to ... place one connector exactly over the another image ! And if you

    want to see the nets - shift one of them a bit.

     

    Yes, I do that for a lot of things, but for these connectors (20x2 rows)

    I can only do one side like that obviously or else both sides will

    connect together at the same places.

     

    You can define another symbol with shifted contact rows image !

     

    BR

    --

    Grzegorz Zalot

     

    complex ltd.

    office tel/fax : +48 32 2505840

    mobil : +48 501 301515

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    Logyx wrote:

     

    On 26/05/2015 11:11, Lorenz wrote:

    Logyx wrote:

     

    I'm working on a schematic with several pairs of 40 pin connectors where

    one PCB connector connects to a 40 pin IDC ribbon cable connector (i.e.

    pin 1-1, in 2-2 etc.).

    In other words, an awful mess when attaching wires between these pins.

     

     

    place your connector, create net stubs on all pins, place labels at

    all open net ends (and name the nets appropriately).

     

    you now can group and duplicate any number of nets and their

    respective labels and place them near your second connector.

     

    Thanks! Looks a whole lot better now.

    I've completed one pair of connectors and have made another copy of the

    entire group (two connectors), but of course all the label names are the

    same as before. Short of renaming each label one by one, is there a

    simpler way (e.g. renaming a whole series with J401-J440 to the new

    connector pairs as J501-J550)?

     

    not without writing (or finding) an ULP to do the job.

     

    easier would be to write an ULP to create the new set of net stubs

    with attached labels, with a nice dialog that asks for the first net

    name, the number & length of stubs to create (or accepts them from the

    command line)

     

     

    to connect the duplicated netstubs to your second connector, you need

    to pick up the connector and drop its pins on top of the open ends of

    the net stubs.

    Droping the net ends onto a pin won't connect.

     

    I couldn't wait, so even if it was time consuming I used the "Name" tool

    to click on each label and rename them, and each time I had an existing

    name somewhere else I was asked if I wanted to connect them together.

     

    if the you rename a net segment you are first ask if you want to

    rename the complete net or only the one segment.

    Then, if the new name you enter is already present in the schematic,

    you are ask if you want to connect to it (mostly to prevent

    unintentional connections).

     

     

    Isn't this what you mean?

     

    for creating the first pair yes.

     

    I normaly have dedicated signal names, so I need to (re)name the nets

    in the duplicates manually anyways.

    So in case I need to create multiple groups I do them from scratch

    separately or create them in parallel.

     

     

    If you like you can also use buses. In that case read about the bus

    command in the online help.

     

    I couldn't get anything out of the built-in help feature, but found a

    Youtube video and see how neat that feature is -having a single cable

    with several strands on at each end. Seems more complicated than with

    net ends but I suppose each has its own use depending on the circuit.

    Thanks image

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    On 26/05/2015 11:11, Lorenz wrote:

    Logyx wrote:

     

    I'm working on a schematic with several pairs of 40 pin connectors where

    one PCB connector connects to a 40 pin IDC ribbon cable connector (i.e.

    pin 1-1, in 2-2 etc.).

    In other words, an awful mess when attaching wires between these pins.

     

     

    place your connector, create net stubs on all pins, place labels at

    all open net ends (and name the nets appropriately).

     

    you now can group and duplicate any number of nets and their

    respective labels and place them near your second connector.

     

    Thanks! Looks a whole lot better now.

    I've completed one pair of connectors and have made another copy of the

    entire group (two connectors), but of course all the label names are the

    same as before. Short of renaming each label one by one, is there a

    simpler way (e.g. renaming a whole series with J401-J440 to the new

    connector pairs as J501-J550)?

     

     

    to connect the duplicated netstubs to your second connector, you need

    to pick up the connector and drop its pins on top of the open ends of

    the net stubs.

    Droping the net ends onto a pin won't connect.

     

    I couldn't wait, so even if it was time consuming I used the "Name" tool

    to click on each label and rename them, and each time I had an existing

    name somewhere else I was asked if I wanted to connect them together.

    Isn't this what you mean?

     

     

    If you like you can also use buses. In that case read about the bus

    command in the online help.

     

    I couldn't get anything out of the built-in help feature, but found a

    Youtube video and see how neat that feature is -having a single cable

    with several strands on at each end. Seems more complicated than with

    net ends but I suppose each has its own use depending on the circuit.

    Thanks image

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    On 26/05/2015 20:32, Grzegorz Zalot wrote:

     

    I seem to recall a feature in Eagle which allows for attaching the wires

    correctly as usual in the PCB layout but does away with the mess in the

    schematic.

    Also, is there a quick way to attach those wires between the same

    numbered pins of two connectors? It takes an awful long time to do it

    manually.

     

    Try to ... place one connector exactly over the another image ! And if you

    want to see the nets - shift one of them a bit.

     

    Yes, I do that for a lot of things, but for these connectors (20x2 rows)

    I can only do one side like that obviously or else both sides will

    connect together at the same places.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago

    Hi Logyx

    I'm working on a schematic with several pairs of 40 pin connectors where

    one PCB connector connects to a 40 pin IDC ribbon cable connector (i.e.

    pin 1-1, in 2-2 etc.).

    In other words, an awful mess when attaching wires between these pins.

     

    I seem to recall a feature in Eagle which allows for attaching the wires

    correctly as usual in the PCB layout but does away with the mess in the

    schematic.

    Also, is there a quick way to attach those wires between the same

    numbered pins of two connectors? It takes an awful long time to do it

    manually.

     

    Try to ... place one connector exactly over the another image ! And if you

    want to see the nets - shift one of them a bit.

     

    This is the fastest way to connect correcponding pins image !

     

    But dont expect proper working of the autorouter - in most cases the

    best routing is not the preference of the current AR ...

     

    BR

    --

    Grzegorz Zalot

     

    complex ltd.

    office tel/fax : +48 32 2505840

    mobil : +48 501 301515

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago

    Am 26.05.2015 um 10:53 schrieb Logyx:

    I'm working on a schematic with several pairs of 40 pin connectors where

    one PCB connector connects to a 40 pin IDC ribbon cable connector (i.e.

    pin 1-1, in 2-2 etc.).

    In other words, an awful mess when attaching wires between these pins.

     

    I seem to recall a feature in Eagle which allows for attaching the wires

    correctly as usual in the PCB layout but does away with the mess in the

    schematic.

    Also, is there a quick way to attach those wires between the same

    numbered pins of two connectors? It takes an awful long time to do it

    manually.

     

    I'm using Eagle 7.2.0 on the Mac OSX platform. Thanks.

     

    Hi,

    take a look about netlist.

    if you export the netlist of your porjekt you see

    some line like

    Net      Part     Pad

     

    +5V      C2       2

              C3       +

     

    If you name your nets like P1-1

     

    you can make a net list

    Net     Part     Pad

     

    P1-1     PCB1     1

         IDC1     1

     

    P2-2     PCB1     2

         IDC1     2

         

    And import this in your schmeatic.

    (i cannot proof this at the moment, but give it a try)

    HTH

    Werner

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago

    Logyx wrote:

     

    I'm working on a schematic with several pairs of 40 pin connectors where

    one PCB connector connects to a 40 pin IDC ribbon cable connector (i.e.

    pin 1-1, in 2-2 etc.).

    In other words, an awful mess when attaching wires between these pins.

     

    I seem to recall a feature in Eagle which allows for attaching the wires

    correctly as usual in the PCB layout but does away with the mess in the

    schematic.

    Also, is there a quick way to attach those wires between the same

    numbered pins of two connectors? It takes an awful long time to do it

    manually.

     

    I'm using Eagle 7.2.0 on the Mac OSX platform. Thanks.

     

    place your connector, create net stubs on all pins, place labels at

    all open net ends (and name the nets appropriately).

     

    you now can group and duplicate any number of nets and their

    respective labels and place them near your second connector.

     

    to connect the duplicated netstubs to your second connector, you need

    to pick up the connector and drop its pins on top of the open ends of

    the net stubs.

    Droping the net ends onto a pin won't connect.

     

     

     

    If you like you can also use buses. In that case read about the bus

    command in the online help.

    --

     

    Lorenz