Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Simplifying complex and many connections
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 187 subscribers
  • Views 973 views
  • Users 0 members are here
Related

Simplifying complex and many connections

autodeskguest
autodeskguest over 11 years ago

I'm working on a schematic with several pairs of 40 pin connectors where

one PCB connector connects to a 40 pin IDC ribbon cable connector (i.e.

pin 1-1, in 2-2 etc.).

In other words, an awful mess when attaching wires between these pins.

 

I seem to recall a feature in Eagle which allows for attaching the wires

correctly as usual in the PCB layout but does away with the mess in the

schematic.

Also, is there a quick way to attach those wires between the same

numbered pins of two connectors? It takes an awful long time to do it

manually.

 

I'm using Eagle 7.2.0 on the Mac OSX platform. Thanks.

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 11 years ago

    Hi Logyx

    I'm working on a schematic with several pairs of 40 pin connectors where

    one PCB connector connects to a 40 pin IDC ribbon cable connector (i.e.

    pin 1-1, in 2-2 etc.).

    In other words, an awful mess when attaching wires between these pins.

     

    I seem to recall a feature in Eagle which allows for attaching the wires

    correctly as usual in the PCB layout but does away with the mess in the

    schematic.

    Also, is there a quick way to attach those wires between the same

    numbered pins of two connectors? It takes an awful long time to do it

    manually.

     

    Try to ... place one connector exactly over the another image ! And if you

    want to see the nets - shift one of them a bit.

     

    This is the fastest way to connect correcponding pins image !

     

    But dont expect proper working of the autorouter - in most cases the

    best routing is not the preference of the current AR ...

     

    BR

    --

    Grzegorz Zalot

     

    complex ltd.

    office tel/fax : +48 32 2505840

    mobil : +48 501 301515

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    On 26/05/2015 20:32, Grzegorz Zalot wrote:

     

    I seem to recall a feature in Eagle which allows for attaching the wires

    correctly as usual in the PCB layout but does away with the mess in the

    schematic.

    Also, is there a quick way to attach those wires between the same

    numbered pins of two connectors? It takes an awful long time to do it

    manually.

     

    Try to ... place one connector exactly over the another image ! And if you

    want to see the nets - shift one of them a bit.

     

    Yes, I do that for a lot of things, but for these connectors (20x2 rows)

    I can only do one side like that obviously or else both sides will

    connect together at the same places.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    Hi,

     

    Try to ... place one connector exactly over the another image ! And if you

    want to see the nets - shift one of them a bit.

     

    Yes, I do that for a lot of things, but for these connectors (20x2 rows)

    I can only do one side like that obviously or else both sides will

    connect together at the same places.

     

    You can define another symbol with shifted contact rows image !

     

    BR

    --

    Grzegorz Zalot

     

    complex ltd.

    office tel/fax : +48 32 2505840

    mobil : +48 501 301515

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    Hi,

     

    Try to ... place one connector exactly over the another image ! And if you

    want to see the nets - shift one of them a bit.

     

    Yes, I do that for a lot of things, but for these connectors (20x2 rows)

    I can only do one side like that obviously or else both sides will

    connect together at the same places.

     

    You can define another symbol with shifted contact rows image !

     

    BR

    --

    Grzegorz Zalot

     

    complex ltd.

    office tel/fax : +48 32 2505840

    mobil : +48 501 301515