Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Would you check my design?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 188 subscribers
  • Views 1396 views
  • Users 0 members are here
Related

Would you check my design?

e14 Contributor
e14 Contributor over 11 years ago

Hi, I'm a total eagle beginner, and I've just made my first schematic and board. Could you please check it, if it's usable? Thanks image

Attachments:
blinking_led.zip
  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 20.07.2015 00:56, Jacob Sycha wrote:

    Hi, I'm a total eagle beginner, and I've just made my first schematic

    and board. Could you please check it, if it's usable? Thanks image

     

    First impressions:

    -Double sided board seems overkill for this simple circuit. See if you

    can make it single layer.

    -Track thickness is very thin. Thin tracks are harder to manufacture.

    -You can probably compress pcb size to a minimum.

    -Wire bends are a bit untidy.

    -For schematic, there is alot of unnecessary junctions. There is no need

    for junctions at pin connections, or at 90deg bends.

    -The 555 timer seems to already exist (several times) in Eagle libraries

     

    A more critical look:

    -I opened this is eagle 6.5.4, and I ERC errors:

    -consistancy error :net class parameters differs in brd vs sch

    -consistancy error :LED naming different in brd vs sch

    -U1 pin 5(CONT) is defined as an input but doesnt have any input (this

    could mean the U1 could go nuts, or library component pin direction for

    pin 5 is wrong). Taking a quick look at the datasheet, I'd suggest

    putting a capacitor on this pin to gnd, but I do not know this circit.

    Since I'm unsecure, I would just put it in and worry about soldering it

    later.

     

    ERC Warnings:

    -Missing juction at the CONN xref

    -VDD power pin of U1 connected to N$1 (Eagle expects pins with direction

    POWER to be connected to a net with same name as the pin)

    -LED1 is missing a value

     

    DRC issues:

    -For this kind of board, I would make larger distance between pads and

    wire (fill).

    -There are some weird stuff left on stop mask around pin 4 of U1. It

    seems to be in the package definition.

    -Capacitor package has capacitor symbol on pads. They will be shaved off

    by the manufacturer but if you do want silk screen, I'd remove it from

    package.

     

    Finally, I have a personal preference for SMD components for small

    projects. Drilling is just unnecessary work, and soldering SMD runs

    smooth after some practice. Im sure you can find tutorials on youtube.

    I also prefer to have sensible netnames that can quickly point you back

    to schematic when reviewing the layout.

     

    I did some homework for you and attached the cleanup I did to your

    project. Compare it with yours image Use 7zip.org to unpack.

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to autodeskguest

    Hi, thanks a lot! This really helped! Just a little issue, I can't find the attached file, Is the problem on my side, or did you forget to attach it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to autodeskguest

    Hi, thanks a lot! This really helped! Just a little issue, I can't find the attached file, Is the problem on my side, or did you forget to attach it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to e14 Contributor

    Am 20.07.2015 um 09:59 schrieb Jacob Sycha:

    Hi, thanks a lot! This really helped! Just a little issue, I can't find

    the attached file, Is the problem on my side, or did you forget to

    attach it?

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/155289

     

     

    Hi Jacob,

    the file was attached by Morton.

    It was, as usual, not linked by element14 which is imho the worst place

    to check things with eagle.

    I suggest you use:

     

    http://www.eaglecentral.ca/forums/

     

    or get a news reader like thunderbird and connect to

     

    news.cadsoft.de

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag