Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Would you check my design?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 188 subscribers
  • Views 1396 views
  • Users 0 members are here
Related

Would you check my design?

e14 Contributor
e14 Contributor over 11 years ago

Hi, I'm a total eagle beginner, and I've just made my first schematic and board. Could you please check it, if it's usable? Thanks image

Attachments:
blinking_led.zip
  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 20.07.2015 00:56, Jacob Sycha wrote:

    Hi, I'm a total eagle beginner, and I've just made my first schematic

    and board. Could you please check it, if it's usable? Thanks image

     

    First impressions:

    -Double sided board seems overkill for this simple circuit. See if you

    can make it single layer.

    -Track thickness is very thin. Thin tracks are harder to manufacture.

    -You can probably compress pcb size to a minimum.

    -Wire bends are a bit untidy.

    -For schematic, there is alot of unnecessary junctions. There is no need

    for junctions at pin connections, or at 90deg bends.

    -The 555 timer seems to already exist (several times) in Eagle libraries

     

    A more critical look:

    -I opened this is eagle 6.5.4, and I ERC errors:

    -consistancy error :net class parameters differs in brd vs sch

    -consistancy error :LED naming different in brd vs sch

    -U1 pin 5(CONT) is defined as an input but doesnt have any input (this

    could mean the U1 could go nuts, or library component pin direction for

    pin 5 is wrong). Taking a quick look at the datasheet, I'd suggest

    putting a capacitor on this pin to gnd, but I do not know this circit.

    Since I'm unsecure, I would just put it in and worry about soldering it

    later.

     

    ERC Warnings:

    -Missing juction at the CONN xref

    -VDD power pin of U1 connected to N$1 (Eagle expects pins with direction

    POWER to be connected to a net with same name as the pin)

    -LED1 is missing a value

     

    DRC issues:

    -For this kind of board, I would make larger distance between pads and

    wire (fill).

    -There are some weird stuff left on stop mask around pin 4 of U1. It

    seems to be in the package definition.

    -Capacitor package has capacitor symbol on pads. They will be shaved off

    by the manufacturer but if you do want silk screen, I'd remove it from

    package.

     

    Finally, I have a personal preference for SMD components for small

    projects. Drilling is just unnecessary work, and soldering SMD runs

    smooth after some practice. Im sure you can find tutorials on youtube.

    I also prefer to have sensible netnames that can quickly point you back

    to schematic when reviewing the layout.

     

    I did some homework for you and attached the cleanup I did to your

    project. Compare it with yours image Use 7zip.org to unpack.

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to autodeskguest

    Am 20.07.2015 um 09:22 schrieb Morten Leikvoll:

    On 20.07.2015 00:56, Jacob Sycha wrote:

    Hi, I'm a total eagle beginner, and I've just made my first schematic

    and board. Could you please check it, if it's usable? Thanks image

     

    First impressions:

    -Double sided board seems overkill for this simple circuit. See if you

    can make it single layer.

    -Track thickness is very thin. Thin tracks are harder to manufacture.

    -You can probably compress pcb size to a minimum.

    -Wire bends are a bit untidy.

    -For schematic, there is alot of unnecessary junctions. There is no need

    for junctions at pin connections, or at 90deg bends.

    -The 555 timer seems to already exist (several times) in Eagle libraries

     

    A more critical look:

    -I opened this is eagle 6.5.4, and I ERC errors:

    -consistancy error :net class parameters differs in brd vs sch

    -consistancy error :LED naming different in brd vs sch

    -U1 pin 5(CONT) is defined as an input but doesnt have any input (this

    could mean the U1 could go nuts, or library component pin direction for

    pin 5 is wrong). Taking a quick look at the datasheet, I'd suggest

    putting a capacitor on this pin to gnd, but I do not know this circit.

    Since I'm unsecure, I would just put it in and worry about soldering it

    later.

     

    ERC Warnings:

    -Missing juction at the CONN xref

    -VDD power pin of U1 connected to N$1 (Eagle expects pins with direction

    POWER to be connected to a net with same name as the pin)

    -LED1 is missing a value

     

    DRC issues:

    -For this kind of board, I would make larger distance between pads and

    wire (fill).

    -There are some weird stuff left on stop mask around pin 4 of U1. It

    seems to be in the package definition.

    -Capacitor package has capacitor symbol on pads. They will be shaved off

    by the manufacturer but if you do want silk screen, I'd remove it from

    package.

     

    Finally, I have a personal preference for SMD components for small

    projects. Drilling is just unnecessary work, and soldering SMD runs

    smooth after some practice. Im sure you can find tutorials on youtube.

    I also prefer to have sensible netnames that can quickly point you back

    to schematic when reviewing the layout.

     

    I did some homework for you and attached the cleanup I did to your

    project. Compare it with yours image Use 7zip.org to unpack.

     

     

    Hi Morton,

    despite the fact that you are verrrrry polite image

    here my critics to your layout:

    for though hole technology the bottom layer should be used

    and  you "confirm" his way of connecting the gnd connections via ratsnest.

    This method leads imho to coincidental connections specially in  higher

    density layouts.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to autodeskguest

    On 20.07.2015 10:15, Joern Paschedag wrote:

    Hi Morton,

    despite the fact that you are verrrrry polite image

    here my critics to your layout:

     

    Hey, and thanks for giving feedback image I really appreciate it starting

    to think I can do it all.

     

    for though hole technology the bottom layer should be used

     

    Yes you are right I should have moved all to bottom layer for this

    design. My excuse is mostly being in "smd" mode image For thorugh hole, its

    easier to solder at the bottom, away from components. But signal wise,

    of course it doesnt matter if you put this on top or bottom of the real

    pcb. If you choose top, you have to make sure there is solder stop or no

    unwanted exposed metal between top and components.

    Tbh, I dont know if you can put eagle to single layer mode on L16 and

    avoid the top mask vs silk DRC issues. Maybe you do?

     

    and  you "confirm" his way of connecting the gnd connections via ratsnest.

    This method leads imho to coincidental connections specially in  higher

    density layouts.

     

    Doing filled routing on layouts that doesnt have a separate solid signal

    layer may be an issue yes. But for this brd, the GND is rather easy to

    get an overview over. For a slightly larger board, I would have second

    thoughts without the full GND backup and maybe done a GND backbone wired

    thick and filled over just for the nice look (and less copper to etch off)

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to autodeskguest

    On 20.07.2015 10:15, Joern Paschedag wrote:

    Hi Morton,

    despite the fact that you are verrrrry polite image

    here my critics to your layout:

     

    Hey, and thanks for giving feedback image I really appreciate it starting

    to think I can do it all.

     

    for though hole technology the bottom layer should be used

     

    Yes you are right I should have moved all to bottom layer for this

    design. My excuse is mostly being in "smd" mode image For thorugh hole, its

    easier to solder at the bottom, away from components. But signal wise,

    of course it doesnt matter if you put this on top or bottom of the real

    pcb. If you choose top, you have to make sure there is solder stop or no

    unwanted exposed metal between top and components.

    Tbh, I dont know if you can put eagle to single layer mode on L16 and

    avoid the top mask vs silk DRC issues. Maybe you do?

     

    and  you "confirm" his way of connecting the gnd connections via ratsnest.

    This method leads imho to coincidental connections specially in  higher

    density layouts.

     

    Doing filled routing on layouts that doesnt have a separate solid signal

    layer may be an issue yes. But for this brd, the GND is rather easy to

    get an overview over. For a slightly larger board, I would have second

    thoughts without the full GND backup and maybe done a GND backbone wired

    thick and filled over just for the nice look (and less copper to etch off)

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to autodeskguest

    Am 20.07.2015 um 10:52 schrieb Morten Leikvoll:

    On 20.07.2015 10:15, Joern Paschedag wrote:

    Hi Morton,

    despite the fact that you are verrrrry polite image

    here my critics to your layout:

     

    Hey, and thanks for giving feedback image I really appreciate it starting

    to think I can do it all.

     

    image

    for though hole technology the bottom layer should be used

     

    Yes you are right I should have moved all to bottom layer for this

    design. My excuse is mostly being in "smd" mode image

     

    I was certain of that!!! image

     

    For thorugh hole, its

    easier to solder at the bottom, away from components. But signal wise,

    of course it doesnt matter if you put this on top or bottom of the real

    pcb. If you choose top, you have to make sure there is solder stop or no

    unwanted exposed metal between top and components.

    Tbh, I dont know if you can put eagle to single layer mode on L16 and

    avoid the top mask vs silk DRC issues. Maybe you do?

     

    I dunno, never done single layer...

    and  you "confirm" his way of connecting the gnd connections via

    ratsnest.

    This method leads imho to coincidental connections specially in  higher

    density layouts.

     

    Doing filled routing on layouts that doesnt have a separate solid signal

    layer may be an issue yes. But for this brd, the GND is rather easy to

    get an overview over. For a slightly larger board, I would have second

    thoughts without the full GND backup and maybe done a GND backbone wired

    thick and filled over just for the nice look (and less copper to etch off)

     

     

    Yes, for this board it's peanuts...

    But I remember some faulty boards I had to check...

    Schematics were OK but still didn't work.

    The boards carried some higher currents, where the gound wasn't as

    straight as the positive supply. Instead gnd was scattered through an

    "asteroid field" (components)  image

    And every time I heard:"I'm doing it since years that way" (gnd

    connections via ratsnest)

    A simple straight wire proved this fault.

     

    Anyway I just wanted people not to adapt this method  as a "standard" to

    avoid  trouble.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag