EAGLE User Chat (English) Unable to delete certain object.
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
  • State Verified Answer
  • Replies 20 replies
  • Answers 1 answer
  • Subscribers 181 subscribers
  • Views 5011 views
  • Users 0 members are here
  • eagle pcb
Related

Unable to delete certain object.

methias
methias over 9 years ago

Hi, I'm a new user of EAGLE. I'm trying to use EAGLE to design a PCB with Arduino Mega 2560 with some sensors. So the only thing I need for the design is the exact pin spacings and some elementary design with connectors.

 

So what I'm doing is I downloaded the EAGLE file from Arduino website, then I deleted any components that I do not want from the original file, only leaving the pad for the pin spacing. However, when I tried to delete an object from the top layer, which has some connections for it's microcontroller, no matter how I clicked the it, it wouldn't be deleted. Thus if I were to fabricate it, I would assume there would be connections that I do not want that will be printed(?)

 

Here's a capture of the layers I have, top layer is the one I want to remove.

https://s23.postimg.org/5x2mnpmwb/Capture.png

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 9 years ago in reply to methias +1 suggested
    You may want to follow a different approach and have a look here: https://www.element14.com/community/community/arduino/blog/2013/11/05/finally-an-arduino-library-for-eagle Markus
  • autodeskguest
    autodeskguest over 9 years ago in reply to methias +1
    On 10/01/17 02:29, Aaron Qwe wrote: I actually have one more question, referring to what I want to do. Do I use holes or drills if what I want to do is just introduce some connectors and make connection…
  • rachaelp
    0 rachaelp over 9 years ago

    Hi Aaron,

     

    From the picture and the description its not immediately apparent to me what you are trying to delete. There are a couple of things to try off the top of my head, first check that you have the tOrigins layer turned on. Without tOrigins you can't select a component and therefore wont be able to delete it. Secondly check that it's not locked. Right click on the object and you get get a pop up context menu. If it says "unLock" in the menu then it is currently locked. If this is the case select the "unLock" option.

     

    I assume you have both the schematic AND the board file open together? If not then they will be out of sync and will mean back annotation wont work. The other thing which could be stopping you deleting is that components should be deleted from the schematic and not from the board. If this was the error you'd get a pop-up message telling you so which as you haven't said this is probably not the case.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to rachaelp

    rachaelp wrote:

     

    I assume you have both the schematic AND the board file open together? If not then they will be out of sync and will mean back annotation wont work. The other thing which could be stopping you deleting is that components should be deleted from the schematic and not from the board. If this was the error you'd get a pop-up message telling you so which as you haven't said this is probably not the case.

    On reading back what I wrote and looking at what you are doing again, I actually now think you have just the board open and are deleting components directly from there. If so then this is probably not what you want to do. Re-download the files if you don't have an unedited copy of the board and open them both up and then delete what you don't want from the schematic. They will all be removed from the board by the automatic back annotation. Then switch to the board and tidy up and tracks and polygons which remain that you no longer need.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • methias
    0 methias over 9 years ago in reply to rachaelp

    Thanks Rachel for your input. Actually I started from deleting components from the schematic, then I realized there are few things that can only be deleted from the board window, i.e. ground pour, text, Via etc.

     

    So I'm down to this components in the schematic, https://s28.postimg.org/kgykri2i5/capture2.png.

    If the picture isn't really clear, I've uploaded a schematic of it, https://www.dropbox.com/s/1x6jtwo055v150h/Arduino_MEGA_2560-Rev3.sch?dl=0

     

    I downloaded the eagle files directly from Arduino's website, is there a chance that is prevents me from deleting some components because it comes in the package?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to methias

    Hi Aaron,

     

    So it's the 6 holes you need to be able to delete then? I downloaded and had a look at the Mega 2560 schematics from Arduino's website and I could delete the holes once I turned the holes layer (45) on.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • methias
    0 methias over 9 years ago in reply to rachaelp

    Nope, I'm referring to the top layer in the middle(red in color). I need the 6 holes as I need to do some design using the pin layout.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to methias

    Ok, I must be completely misunderstanding what you are trying to achieve. That's the pads of the ATMEGA2560 which is still in your schematic. I thought you wanted to keep this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • methias
    0 methias over 9 years ago in reply to rachaelp

    Okay maybe I'll need to rephrase my question.

     

    So in the board window, there are currently few layers on it, one of them is the top layer right? Which is in red colour(refer to the image in my very first post).

    Problem: I want to keep all the other layers except for the top layer(red color layer) for now, but the delete function does not seem to function for me.

     

    I apologize if I still sound crazy haha, this is my second try at eagle.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to methias

    Aaron Qwe wrote:

     

    I apologize if I still sound crazy haha, this is my second try at eagle.

     

    I'll be honest, it does a little but maybe that's because I don't understand what you are really trying to achieve so lets take a step back. So why don't you want the top layer of the board?

     

    The pads of the ATMEGA2560 which are on the top layer are part of the component. You can't just remove those unfortunately. Why do you want the ATMEGA2560 in the schematic if you don't want it's pads on the board?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • methias
    0 methias over 9 years ago in reply to rachaelp

    Well my objective is to only have the pin spacings from the original board layout. From there, I'll introduce some connectors that will connect to some of the I/O pins of the Arduino Mega.

     

    So my understanding on how to achieve this was to remove everything except for the drill/hole that is situated at the I/O pin, including the pads of the ATMEGA2560 because I thought that including it would have it been fabricated too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to methias

    You may want to follow a different approach and have a look here:

     

    https://www.element14.com/community/community/arduino/blog/2013/11/05/finally-an-arduino-library-for-eagle

     

    Markus

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
>