EAGLE User Chat (English) Unable to delete certain object.
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
  • State Verified Answer
  • Replies 20 replies
  • Answers 1 answer
  • Subscribers 181 subscribers
  • Views 4993 views
  • Users 0 members are here
  • eagle pcb
Related

Unable to delete certain object.

methias
methias over 9 years ago

Hi, I'm a new user of EAGLE. I'm trying to use EAGLE to design a PCB with Arduino Mega 2560 with some sensors. So the only thing I need for the design is the exact pin spacings and some elementary design with connectors.

 

So what I'm doing is I downloaded the EAGLE file from Arduino website, then I deleted any components that I do not want from the original file, only leaving the pad for the pin spacing. However, when I tried to delete an object from the top layer, which has some connections for it's microcontroller, no matter how I clicked the it, it wouldn't be deleted. Thus if I were to fabricate it, I would assume there would be connections that I do not want that will be printed(?)

 

Here's a capture of the layers I have, top layer is the one I want to remove.

https://s23.postimg.org/5x2mnpmwb/Capture.png

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 9 years ago in reply to methias +1 suggested
    You may want to follow a different approach and have a look here: https://www.element14.com/community/community/arduino/blog/2013/11/05/finally-an-arduino-library-for-eagle Markus
  • autodeskguest
    autodeskguest over 9 years ago in reply to methias +1
    On 10/01/17 02:29, Aaron Qwe wrote: I actually have one more question, referring to what I want to do. Do I use holes or drills if what I want to do is just introduce some connectors and make connection…
  • rachaelp
    0 rachaelp over 9 years ago in reply to methias

    So you just want to make a generic board template on which to base your own board which will will plug into an Arduino?

     

    If that's the case just delete the ATMEGA2560 from the schematics, nothing you have said gives any reason for it still to be there as far as i can see.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • methias
    0 methias over 9 years ago in reply to autodeskguest

    Definitely would look into it! Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • methias
    0 methias over 9 years ago in reply to rachaelp

    Yeap, I tried doing that from the schematics, but all I get is a "blank" sound notification. I cant select the ATMEGA whatsoever or do anything with it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to methias

    That's really odd as it deletes fine for me. Are you sure you are clicking near to the origin of the symbol which in this case is right in the middle of the symbol. I get the "boing" sound if I try to click too far away from the origin.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to methias

    I decided it would just be easier to do it for you as it was only a 2 minute job to clear everything out and zip it up. See the attached......

    Attachments:
    Arduino Blank.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • methias
    0 methias over 9 years ago in reply to rachaelp

    Yes, it is exactly as you said. I tried clicking way further than the origin. Thanks for the help!

     

    I actually have one more question, referring to what I want to do. Do I use holes or drills if what I want to do is just introduce some connectors and make connection to to the I/O pins?

     

    From my understanding I would need to use drills right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to methias

    Hi Aaron,

     

    It sounds like what you are describing there is plated through holes which in EAGLE can be done in the board by adding a via with a large drill size setting and giving it an appropriate name to match the net it is to connect with. Alternatively (and a better way to do it) you can create a library part for plated holes with various hole sizes specified in the part. You place this in your schematic and wire it to wherever you need and then the pads and air wires will show in the board so you can place it where you need and route it.

     

    But do you want plated through holes or do you want to place a part for a specific connector you wish to add? Again, a component can be created and then this will be added in the schematic and wired up, and will then appear in the board to be placed and routed.

     

    Let me know what you are trying to do and I will give you more specific help if you need it.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to methias

    On 10/01/17 02:29, Aaron Qwe wrote:

     

    I actually have one more question, referring to what I want to do. Do I use holes or drills if what I want to do is just introduce some connectors and make connection to to the I/O pins?

     

    From my understanding I would need to use drills right?

     

    No.

     

    Rachael has helped you achieve what you were trying to do but I note

    Markus gave the rather more significant advice that you're probably

    trying to do the wrong thing. I'm still not entirely clear on what your

    "end goal" is, but I think you're trying to create a template for

    designing shield boards? If so...

     

    Editing an existing Arduino (host) design to get a minimal board is the

    wrong approach. What you ideally want is an Arduino shield pin-out as a

    library component. This component would have the signal names of the

    Arduino as pins on the schematic symbol, and a PCB package consisting of

    holes for the mounting holes and through-hole-pads for the header pins.

    Then, for each new shield you design, just drop one of these into the

    schematic along with all your other components, wire it up, and the

    board will have a template complete with all the air wires.

     

    There are a few of these knocking about, including the one Markus linked

    to. But to be honest, I designed one from scratch (for the CooCox

    "Embedded Pi" but it's much the same) using measurements from Google

    searches, and the whole process took less time than this discussion thread.

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to autodeskguest

    Rob Pearce wrote on Tue, 10 January 2017 07:57

    On 10/01/17 02:29, Aaron Qwe wrote:

     

    I actually have one more question, referring to what I want to do.

    Do I use holes or drills if what I want to do is just introduce some

    connectors and make connection to to the I/O pins?

     

    From my understanding I would need to use drills right?

     

    No.

     

    Rachael has helped you achieve what you were trying to do but I note

    Markus gave the rather more significant advice that you're probably

    trying to do the wrong thing. I'm still not entirely clear on what

    your

    "end goal" is, but I think you're trying to create a template for

    designing shield boards? If so...

     

     

    I'm in complete agreement with Rob and Markus here, it's probably not the

    best approach as, in the process of doing what you have done, you have

    ended up with a board which is the right shape with all the connectors on

    it but it's lost the detail of what the pinout of the connectors is so

    you'll have to look up on the actual Arduino pinout every time to make sure

    you connect things to the right place. It's definitely not the ideal

    solution. Using an Arduino library component to provide the starting point

    of your shield, all the information which enables mapping of functions to

    the correct pins on the connectors is retained.

     

    Best Regards,

     

    Rachael

     

     

     

    --

    http://www.eaglecentral.ca :: The original and best browser access to CadSoft EAGLE support forums.  Supported by EAGLE licenses purchased through us :: http://www.eaglelicenses.com

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to rachaelp

    On 10/01/2017 9:16 p.m., Rachael wrote:

    Rob Pearce wrote on Tue, 10 January 2017 07:57

    On 10/01/17 02:29, Aaron Qwe wrote:

     

    I actually have one more question, referring to what I want to do.

    Do I use holes or drills if what I want to do is just introduce some

    connectors and make connection to to the I/O pins?

     

    From my understanding I would need to use drills right?

     

    No.

     

    Rachael has helped you achieve what you were trying to do but I note

    Markus gave the rather more significant advice that you're probably

    trying to do the wrong thing. I'm still not entirely clear on what

    your

    "end goal" is, but I think you're trying to create a template for

    designing shield boards? If so...

     

    I'm in complete agreement with Rob and Markus here, it's probably not the

    best approach as, in the process of doing what you have done, you have

    ended up with a board which is the right shape with all the connectors on

    it but it's lost the detail of what the pinout of the connectors is so

    you'll have to look up on the actual Arduino pinout every time to make sure

    you connect things to the right place. It's definitely not the ideal

    solution. Using an Arduino library component to provide the starting point

    of your shield, all the information which enables mapping of functions to

    the correct pins on the connectors is retained.

     

    Best Regards,

     

    Rachael

     

     

     

     

    Just to remind others following this thread, now that the OP has the

    board outline and connectors, they could run the ULP

    'make-group2pac.ulp' to make the package for the library.

     

    HTH

    Warren

     

    --

    ... use NNTP://news.cadsoft.de and a functional news reader like

    Thunderbird!

    ... or http://www.eaglecentral.ca browser access to CadSoft EAGLE

    support forums.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<