Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) EAGLE ulp generates wrong scale -- how to fix?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 1462 views
  • Users 0 members are here
  • eagle
  • ulp
  • pcb
  • cnc
  • diy
  • mill
Related

EAGLE ulp generates wrong scale -- how to fix?

e14 Contributor
e14 Contributor over 14 years ago

I'm trying to do isolation milling circuit board prototyping using Eagle lite version 6.0.0. This is the first version of Eagle I've used, so I'm a newbie!

To generate the mill control file, I'm using a script called fablab-mill-n-drill.ulp from here: http://fablab.marcboon.com/pcb/step2.html

Actual script: http://fablab.marcboon.com/pcb/fablab-mill-n-drill.ulp

 

Unfortunately, when I run this script, it generates the outlines in a very small scale in the lower-left corner of the board. I'm using the "singlesided" PCB from examples.

Image attached. The purple thing in the lower left is the generated traces; zoom image also included.

 

So, my guess is that the way scale in generating outlines works has changed between when this script was created in 2008, and version 6 in 2011.

I'm a software developer by trade, but have never used Eagle or the ULP language before. If I know how to properly compensate for scale, I could probably hack it into the program. But where do I look to figure out what the right scale should be, or how otherwise to fix this script?

 

Any suggestions or pointers more specific than "it's somewhere in the manual" would beappreciated!

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • kataze
    0 kataze over 13 years ago

    I know I'm like a year late here, but just in case another lab has the same problem and comes across this thread like I did:

     

    Change line 196 in fablab-mill-n-drill.ulp to read:

     

        eta         = 0.000003125,         // Eagle resolution in mm

     

     

    this will allow the script to cope with the change in internal resolution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kataze
    0 kataze over 13 years ago

    I know I'm like a year late here, but just in case another lab has the same problem and comes across this thread like I did:

     

    Change line 196 in fablab-mill-n-drill.ulp to read:

     

        eta         = 0.000003125,         // Eagle resolution in mm

     

     

    this will allow the script to cope with the change in internal resolution.