Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Optimizing drillholes
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 190 subscribers
  • Views 929 views
  • Users 0 members are here
  • eagle
  • layout
  • pcb
Related

Optimizing drillholes

Wolfskammer04
Wolfskammer04 over 14 years ago

I generated the Gerber files and found in the *.dri file that I have two drills with  0.0374inch (T03 0.0374inch 2). In the *.drd file I found them with this parameters:

 

T03

X10260Y24158

X10260Y26158

 

how can I found them in the board. What type of measuring unit is: X10260?

 

I want to change them to 0.0400inch.

 

Roland

  • Sign in to reply
  • Cancel
Parents
  • robotonics
    0 robotonics over 14 years ago

    Hi

     

    Im guessing you have got X and Y axis coords here in whatever units your grid is set to. If so, you could then move your cursor on the layout, and from the coords box (top left) you can read out the position that your two drills are at, you will find the pads and change the drill sizes?

     

    For example if units are in millimetres then from the cross (origin) on the pcb layout window your first drill would be at X = 102.60mm and Y at 241.58mm.

     

    Just an idea!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Wolfskammer04
    0 Wolfskammer04 over 14 years ago in reply to robotonics

    Hi,

     

    I tried to do it that way but I did not find the maching holes. I know from a webcast that all measures in the gerber files base on inches except someone set it definitly to metric measures. So I swiched from one setting to the next hoping to find the maching values but I did not. It also seems to me that eagle inside uses a better accuracy as actually is used in the gerber files. Am I right? I guess I have build a simple project with only one hole to get the secrets out of the files.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to Wolfskammer04

    Wolfskammer04 wrote:

    Hi,

     

    I tried to do it that way but I did not find the maching holes. I

    know from a webcast that all measures in the gerber files base on

    inches except someone set it definitly to metric measures. So I

    swiched from one setting to the next hoping to find the maching

    values but I did not. It also seems to me that eagle inside uses a

    better accuracy as actually is used in the gerber files. Am I right?

    I guess I have build a simple project with only one hole to get the

    secrets out of the files.

     

     

    Let Eagle do all the hard work for you

    In the Board Editor: Options> Set>Drill tab>Set

    That will give you unique drill diameter symbols.

    Then run the ULP drill-legend.ulp which places a drill legend next to your

    design.

    Finally, display the Drill layer and any others that help and locate the two

    holes with the diameter of interest

     

    HTH

    Warren

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Wolfskammer04
    0 Wolfskammer04 over 14 years ago in reply to e14 Contributor

    Many thanks, that works good!

     

    Roland

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Wolfskammer04
    0 Wolfskammer04 over 14 years ago in reply to e14 Contributor

    Many thanks, that works good!

     

    Roland