Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Help making footprint?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 965 views
  • Users 0 members are here
Related

Help making footprint?

e14 Contributor
e14 Contributor over 14 years ago

I am making my first footprint in Eagle.  I am basing it on this datasheet http://www.memoryprotectiondevices.com/datasheets/BH800S-datasheet.pdf and the problem I am having is with the pads.  The drill diagram at the top of the sheet shows a .042 drill but when I enter that into Drill on the Info screen for the pad and choose Auto for the diameter, it draws a pad that is much smaller than what it seems it should be from the diagram on the lower right. What, if anything am I doing wrong?  Also, what does 2PL mean on the drill hole callout?  

 

Next, I am confused about the three circles on the .750 diameter circle on the lower right diagram.  What are they and why is there no position or size information associated with them?  Finally, the center diagram shows a locking stake (again with the 2PL notation) but without any location or size  information. Any ideas on that?   I guess it might help if I had a device in hand to look at but at this moment I do not.

  • Sign in to reply
  • Cancel
Parents
  • robotonics
    0 robotonics over 14 years ago

    Hi

     

    Do you need to make a footprint for this? I may be wrong and will check in more detail for you, however it looks like a standard coin cell holder, sparkfun have a very useful library of footprints/parts you can download here

     

    They have some coin cell holders in BATTERY section. There is a 20mm one there BATTERYPTH20...might it do? you will find the sparkfun library useful in any case...

     

    Im guessing as far as the PCB footprint is concerned, from the datasheet it looks like there are only 2 x 1mm holes 20.50mm apart that are needed for the part, one for positive, and the other negative.

     

    Regards

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to robotonics

    Yeah, I wish Sparkfun had a footprint for this particular coin cell holder but they don't.  This holder is for two cells and it is one of the few I coud find.  It is the one closest to one from SF, which I am modifying to make this one. 

     

    So, the question remains, how do you explain the difference between the diagram on the lower right in the datasheet and the rather small holes that are drawn using .042 for the drill size?   And the other questions are still unanswered as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • robotonics
    0 robotonics over 14 years ago in reply to e14 Contributor

    Thats the trouble...lol...never enough detail...And that datasheet is bad. If you have the part in front of you its a lot easier obviously.

     

    However, I am looking at the PCB LAYOUT part, and ignoring the rest.

     

    I can see holes drilled in 2 places 20.50mm apart and approx 1mm in dia...you will want pads round them as well obviously.

     

    Are there any more than 2 connections for this part?

     

    The holes at lower right are probably not holes but just the dimension of the top of the pin, a bit like a flat head nail...the hole you see on PCB layout is the actual dimension of the pin that will go through the PCB..the pin end.

     

    The other 3 holes seem to be in the plastic only and carry the locking pins that hold the whole assembly in place.

     

    Am I making sense?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • robotonics
    0 robotonics over 14 years ago in reply to e14 Contributor

    Thats the trouble...lol...never enough detail...And that datasheet is bad. If you have the part in front of you its a lot easier obviously.

     

    However, I am looking at the PCB LAYOUT part, and ignoring the rest.

     

    I can see holes drilled in 2 places 20.50mm apart and approx 1mm in dia...you will want pads round them as well obviously.

     

    Are there any more than 2 connections for this part?

     

    The holes at lower right are probably not holes but just the dimension of the top of the pin, a bit like a flat head nail...the hole you see on PCB layout is the actual dimension of the pin that will go through the PCB..the pin end.

     

    The other 3 holes seem to be in the plastic only and carry the locking pins that hold the whole assembly in place.

     

    Am I making sense?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer