Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Help making footprint?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 958 views
  • Users 0 members are here
Related

Help making footprint?

e14 Contributor
e14 Contributor over 14 years ago

I am making my first footprint in Eagle.  I am basing it on this datasheet http://www.memoryprotectiondevices.com/datasheets/BH800S-datasheet.pdf and the problem I am having is with the pads.  The drill diagram at the top of the sheet shows a .042 drill but when I enter that into Drill on the Info screen for the pad and choose Auto for the diameter, it draws a pad that is much smaller than what it seems it should be from the diagram on the lower right. What, if anything am I doing wrong?  Also, what does 2PL mean on the drill hole callout?  

 

Next, I am confused about the three circles on the .750 diameter circle on the lower right diagram.  What are they and why is there no position or size information associated with them?  Finally, the center diagram shows a locking stake (again with the 2PL notation) but without any location or size  information. Any ideas on that?   I guess it might help if I had a device in hand to look at but at this moment I do not.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Richard Herman Inscribed thus:

     

    Op Tue, 10 Apr 2012 19:45:42 +0200 schreef Don French

    <noreply-101094@element14.com>:

     

    >> I am making my first footprint in Eagle.  I am basing it on this

    >> datasheet

    >>

    http://www.memoryprotectiondevices.com/datasheets/BH800S-datasheet.pdf

    >> and the problem I am having is with the pads.  The drill diagram at

    >> the top of the sheet shows a .042 drill but when I enter that into

    >> Drill on the Info screen for the pad and choose Auto for the

    >> diameter, it draws a pad that is much smaller than what it seems it

    >> should be from the diagram on the lower right.

     

    Then don't enter 'auto' but simply give the pad the diameter you want.

    There is no 'right' size here. Larger pads are easier to etch and give

    better mechanical hold for the battery holder, but use more space on

    the PCB. You have to decide on the correct compromise.

    if you use auto, the DRC will decide on what size the pad will be.

    Look at the 'restring' tab.

     

    >> what does 2PL mean on the drill hole callout?

     

    I assume they mean 2 PLaces, as in two pads/pins?

     

    >> Next, I am confused about the three circles on the .750 diameter

    >> circle

    >> on the lower right diagram.  What are they and why is there no

    >> position or size information associated with them?

     

    Since they are drawn in blue, they are most likely part of the holder,

    I'm guessing just plastic standoffs, as you can see in the center

    diagram.

     

      Finally, the center diagram

    >> shows a locking stake (again with the 2PL notation) but without any

    >> location or size  information. Any ideas on that?

     

    Aren't those just the pins on the device shown from a different angle?

     

     

     

    Richard

     

    They are retainers to stop the part falling off the board.

     

    --

    Best Regards:

                         Baron.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Thanks, guys!  It looks like I am good to go then. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Op Tue, 10 Apr 2012 19:45:42 +0200 schreef Don French 

    <noreply-101094@element14.com>:

     

    I am making my first footprint in Eagle.  I am basing it on this 

    datasheet 

    http://www.memoryprotectiondevices.com/datasheets/BH800S-datasheet.pdf 

    and the problem I am having is with the pads.  The drill diagram at the 

    top of the sheet shows a .042 drill but when I enter that into Drill on 

    the Info screen for the pad and choose Auto for the diameter, it draws a 

    pad that is much smaller than what it seems it should be from the 

    diagram on the lower right.

     

    Then don't enter 'auto' but simply give the pad the diameter you want. 

    There is no 'right' size here. Larger pads are easier to etch and give 

    better mechanical hold for the battery holder, but use more space on the 

    PCB. You have to decide on the correct compromise.

    if you use auto, the DRC will decide on what size the pad will be. Look at 

    the 'restring' tab.

     

    what does 2PL mean on the drill hole callout?

     

    I assume they mean 2 PLaces, as in two pads/pins?

     

    Next, I am confused about the three circles on the .750 diameter circle 

    on the lower right diagram.  What are they and why is there no position 

    or size information associated with them?

     

    Since they are drawn in blue, they are most likely part of the holder, I'm 

    guessing just plastic standoffs, as you can see in the center diagram.

     

      Finally, the center diagram

    shows a locking stake (again with the 2PL notation) but without any 

    location or size  information. Any ideas on that?

     

    Aren't those just the pins on the device shown from a different angle?

     

     

     

    Richard

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Looks like a standard battery holder for a CR2032 3.0V Lithium Coin Cell.

    All the the ones I have seen of that style are pretty much the same.

    2PL means "2 Places", the holes in the lower right diagram are exagerated, the 3 circles in the lower right diagram are molded feet (part of the holder) that keeps the holder up slightly off the surface of the board for an air gap. I'm not positive what the locking stake is except maybe the portion of the contact pin that is slightly wider than at the point of entry Never really seen it used for anything specific except to keep the pins from going too far into the pad..

     

    If it's for 2 coin cells then it would be 2 ea. CR2016's stacked one on top of the other to make 6V instead of 3V.

     

    lol....correcting myself 2 ea. CR2032's stacked, it's too deep for 2 CR2016's.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • robotonics
    0 robotonics over 14 years ago in reply to e14 Contributor

    Thats the trouble...lol...never enough detail...And that datasheet is bad. If you have the part in front of you its a lot easier obviously.

     

    However, I am looking at the PCB LAYOUT part, and ignoring the rest.

     

    I can see holes drilled in 2 places 20.50mm apart and approx 1mm in dia...you will want pads round them as well obviously.

     

    Are there any more than 2 connections for this part?

     

    The holes at lower right are probably not holes but just the dimension of the top of the pin, a bit like a flat head nail...the hole you see on PCB layout is the actual dimension of the pin that will go through the PCB..the pin end.

     

    The other 3 holes seem to be in the plastic only and carry the locking pins that hold the whole assembly in place.

     

    Am I making sense?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to robotonics

    Yeah, I wish Sparkfun had a footprint for this particular coin cell holder but they don't.  This holder is for two cells and it is one of the few I coud find.  It is the one closest to one from SF, which I am modifying to make this one. 

     

    So, the question remains, how do you explain the difference between the diagram on the lower right in the datasheet and the rather small holes that are drawn using .042 for the drill size?   And the other questions are still unanswered as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • robotonics
    0 robotonics over 14 years ago

    Hi

     

    Do you need to make a footprint for this? I may be wrong and will check in more detail for you, however it looks like a standard coin cell holder, sparkfun have a very useful library of footprints/parts you can download here

     

    They have some coin cell holders in BATTERY section. There is a 20mm one there BATTERYPTH20...might it do? you will find the sparkfun library useful in any case...

     

    Im guessing as far as the PCB footprint is concerned, from the datasheet it looks like there are only 2 x 1mm holes 20.50mm apart that are needed for the part, one for positive, and the other negative.

     

    Regards

    David