Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Help making footprint?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 960 views
  • Users 0 members are here
Related

Help making footprint?

e14 Contributor
e14 Contributor over 14 years ago

I am making my first footprint in Eagle.  I am basing it on this datasheet http://www.memoryprotectiondevices.com/datasheets/BH800S-datasheet.pdf and the problem I am having is with the pads.  The drill diagram at the top of the sheet shows a .042 drill but when I enter that into Drill on the Info screen for the pad and choose Auto for the diameter, it draws a pad that is much smaller than what it seems it should be from the diagram on the lower right. What, if anything am I doing wrong?  Also, what does 2PL mean on the drill hole callout?  

 

Next, I am confused about the three circles on the .750 diameter circle on the lower right diagram.  What are they and why is there no position or size information associated with them?  Finally, the center diagram shows a locking stake (again with the 2PL notation) but without any location or size  information. Any ideas on that?   I guess it might help if I had a device in hand to look at but at this moment I do not.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Richard Herman Inscribed thus:

     

    Op Tue, 10 Apr 2012 19:45:42 +0200 schreef Don French

    <noreply-101094@element14.com>:

     

    >> I am making my first footprint in Eagle.  I am basing it on this

    >> datasheet

    >>

    http://www.memoryprotectiondevices.com/datasheets/BH800S-datasheet.pdf

    >> and the problem I am having is with the pads.  The drill diagram at

    >> the top of the sheet shows a .042 drill but when I enter that into

    >> Drill on the Info screen for the pad and choose Auto for the

    >> diameter, it draws a pad that is much smaller than what it seems it

    >> should be from the diagram on the lower right.

     

    Then don't enter 'auto' but simply give the pad the diameter you want.

    There is no 'right' size here. Larger pads are easier to etch and give

    better mechanical hold for the battery holder, but use more space on

    the PCB. You have to decide on the correct compromise.

    if you use auto, the DRC will decide on what size the pad will be.

    Look at the 'restring' tab.

     

    >> what does 2PL mean on the drill hole callout?

     

    I assume they mean 2 PLaces, as in two pads/pins?

     

    >> Next, I am confused about the three circles on the .750 diameter

    >> circle

    >> on the lower right diagram.  What are they and why is there no

    >> position or size information associated with them?

     

    Since they are drawn in blue, they are most likely part of the holder,

    I'm guessing just plastic standoffs, as you can see in the center

    diagram.

     

      Finally, the center diagram

    >> shows a locking stake (again with the 2PL notation) but without any

    >> location or size  information. Any ideas on that?

     

    Aren't those just the pins on the device shown from a different angle?

     

     

     

    Richard

     

    They are retainers to stop the part falling off the board.

     

    --

    Best Regards:

                         Baron.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Richard Herman Inscribed thus:

     

    Op Tue, 10 Apr 2012 19:45:42 +0200 schreef Don French

    <noreply-101094@element14.com>:

     

    >> I am making my first footprint in Eagle.  I am basing it on this

    >> datasheet

    >>

    http://www.memoryprotectiondevices.com/datasheets/BH800S-datasheet.pdf

    >> and the problem I am having is with the pads.  The drill diagram at

    >> the top of the sheet shows a .042 drill but when I enter that into

    >> Drill on the Info screen for the pad and choose Auto for the

    >> diameter, it draws a pad that is much smaller than what it seems it

    >> should be from the diagram on the lower right.

     

    Then don't enter 'auto' but simply give the pad the diameter you want.

    There is no 'right' size here. Larger pads are easier to etch and give

    better mechanical hold for the battery holder, but use more space on

    the PCB. You have to decide on the correct compromise.

    if you use auto, the DRC will decide on what size the pad will be.

    Look at the 'restring' tab.

     

    >> what does 2PL mean on the drill hole callout?

     

    I assume they mean 2 PLaces, as in two pads/pins?

     

    >> Next, I am confused about the three circles on the .750 diameter

    >> circle

    >> on the lower right diagram.  What are they and why is there no

    >> position or size information associated with them?

     

    Since they are drawn in blue, they are most likely part of the holder,

    I'm guessing just plastic standoffs, as you can see in the center

    diagram.

     

      Finally, the center diagram

    >> shows a locking stake (again with the 2PL notation) but without any

    >> location or size  information. Any ideas on that?

     

    Aren't those just the pins on the device shown from a different angle?

     

     

     

    Richard

     

    They are retainers to stop the part falling off the board.

     

    --

    Best Regards:

                         Baron.