Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) How to make footprint for a jack with rectangular tabs?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 1368 views
  • Users 0 members are here
Related

How to make footprint for a jack with rectangular tabs?

e14 Contributor
e14 Contributor over 14 years ago

I am trying to create a footprint for this phono jack http://www.switchcraft.com/Drawings/35rapc__hn2_cd.pdf.  And instead of pins that go through circular holes, it has tabs that go through rectangular holes.  How do I do this in the footprint editor? 

 

Also, the jack has five round pegs that appear to be for positioning.  Is there a way to indicate this on the footprint in such a way that they will be drilled no matter where I place the jack (as opposed to putting holes on the board that would have to be re-positioned if I moved the jack)?  I suppose that I could make them fake pads  - so what if they get plated through?  - but is there another way?   Or maybe I will just ignore the pegs and let the piece sit 1 mm above the board. But I fear that the pegs are important for handling the stress of plugging a phono plug in and out all the time.

 

Finally, how are these pieces soldered in?  Do the tabs have to be folded over before soldering?  If so, this has impications for the board design too - there has to be a pad on the back side but only on one side of the hole. 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Don French wrote:

    I am trying to create a footprint for this phono jack

    http://www.switchcraft.com/Drawings/35rapc__hn2_cd.pdf. And instead

    of pins that go through circular holes, it has tabs that go through

    rectangular holes. How do I do this in the footprint editor?

     

     

    Draw the rectangles or wires in the milling layer and ensure you include and

    explain the presence of the routing layer to the board house

    Verify the dimensions of your slots are greater than the minimums of the

    board house.

    Take guidance here from the board house you intend to use.

     

    Also, the jack has five round pegs that appear to be for positioning.

    Is there a way to indicate this on the footprint in such a way that

    they will be drilled no matter where I place the jack (as opposed to

    putting holes on the board that would have to be re-positioned if I

    moved the jack)? I suppose that I could make them fake pads - so what

    if they get plated through? - but is there another way?

     

    Place "holes: when you design the package. They wont be plated through and

    copper pours will keep away from them as determined by your DRC settings

    You could use pads if you see some advantage or use a cheap board service

    option that does not offer un-plated holes (Its an additonal later stage

    they remove to keep the cost down)

     

    Or maybe I

    will just ignore the pegs and let the piece sit 1 mm above the board.

    But I fear that the pegs are important for handling the stress of

    plugging a phono plug in and out all the time.

     

    Finally, how are these pieces soldered in? Do the tabs have to be

    folded over before soldering? If so, this has impications for the

    board design too - there has to be a pad on the back side but only on

    one side of the hole.

     

    Usually the tabs are given a twist to hold the part in place for manual or

    wave soldering

     

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Don French wrote:

    I am trying to create a footprint for this phono jack

    http://www.switchcraft.com/Drawings/35rapc__hn2_cd.pdf. And instead

    of pins that go through circular holes, it has tabs that go through

    rectangular holes. How do I do this in the footprint editor?

     

     

    Draw the rectangles or wires in the milling layer and ensure you include and

    explain the presence of the routing layer to the board house

    Verify the dimensions of your slots are greater than the minimums of the

    board house.

    Take guidance here from the board house you intend to use.

     

    Also, the jack has five round pegs that appear to be for positioning.

    Is there a way to indicate this on the footprint in such a way that

    they will be drilled no matter where I place the jack (as opposed to

    putting holes on the board that would have to be re-positioned if I

    moved the jack)? I suppose that I could make them fake pads - so what

    if they get plated through? - but is there another way?

     

    Place "holes: when you design the package. They wont be plated through and

    copper pours will keep away from them as determined by your DRC settings

    You could use pads if you see some advantage or use a cheap board service

    option that does not offer un-plated holes (Its an additonal later stage

    they remove to keep the cost down)

     

    Or maybe I

    will just ignore the pegs and let the piece sit 1 mm above the board.

    But I fear that the pegs are important for handling the stress of

    plugging a phono plug in and out all the time.

     

    Finally, how are these pieces soldered in? Do the tabs have to be

    folded over before soldering? If so, this has impications for the

    board design too - there has to be a pad on the back side but only on

    one side of the hole.

     

    Usually the tabs are given a twist to hold the part in place for manual or

    wave soldering

     

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de