Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) How to make footprint for a jack with rectangular tabs?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 1368 views
  • Users 0 members are here
Related

How to make footprint for a jack with rectangular tabs?

e14 Contributor
e14 Contributor over 14 years ago

I am trying to create a footprint for this phono jack http://www.switchcraft.com/Drawings/35rapc__hn2_cd.pdf.  And instead of pins that go through circular holes, it has tabs that go through rectangular holes.  How do I do this in the footprint editor? 

 

Also, the jack has five round pegs that appear to be for positioning.  Is there a way to indicate this on the footprint in such a way that they will be drilled no matter where I place the jack (as opposed to putting holes on the board that would have to be re-positioned if I moved the jack)?  I suppose that I could make them fake pads  - so what if they get plated through?  - but is there another way?   Or maybe I will just ignore the pegs and let the piece sit 1 mm above the board. But I fear that the pegs are important for handling the stress of plugging a phono plug in and out all the time.

 

Finally, how are these pieces soldered in?  Do the tabs have to be folded over before soldering?  If so, this has impications for the board design too - there has to be a pad on the back side but only on one side of the hole. 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    As an example have  a look within  the library con-shiua-chyuan

    There is a single package there with milled slots through pads. That

    technique may work for you if you do not need the slot to be plated

     

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    As an example have  a look within  the library con-shiua-chyuan

    There is a single package there with milled slots through pads. That

    technique may work for you if you do not need the slot to be plated

     

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de