EAGLE User Chat (English) Eagle and Laser cutter
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
  • State Verified Answer
  • Replies 18 replies
  • Answers 1 answer
  • Subscribers 181 subscribers
  • Views 3911 views
  • Users 0 members are here
  • eagle
  • pcb
  • laser
Related

Eagle and Laser cutter

Former Member
Former Member over 11 years ago

Has anyone here used a laser cutter in conjunction with eagle to make pcbs?

 

im using pcb-gcode to create the code to use with a milling machine (modding it to turn the laser on and off once it generates the code), then running it through EMC2 that controls our 40w cutter. I spray paint the side of the copper board I intend to use and vaporize the traces with the laser...

 

im just curious if anyone else has a similar workflow, the only real problem I'm having is spotting/marking the holes so enough copper gets etched away so my hand drilling is a bit more accurate (yes I could completely use a drill press but I don't have one image )

 

MAybe a modified method that results in bigger holes being marked?

 

 

 

thanks for reading!

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 11 years ago in reply to dougw +1
    Well I haven't really messed with trace thickness since throughout my PCB making I've purposely made the traces as long as I could because I was using the toner transfer method... But here's some pictures…
  • Problemchild
    Problemchild over 11 years ago in reply to dragonstyne +1
    Steve if you are interested we can do something with my spare one so that you can get the electronics then the mechanics sounded out with out too many dependencies !
  • Problemchild
    Problemchild over 11 years ago in reply to dragonstyne +1
    Most of the parts are available from EBAY. If you feel confident of making an X-Y mechanism with a head on it then you are a winner for the rest. Even the Laser part aint too bad as long as you don't stick…
  • dougw
    0 dougw over 11 years ago

    Very interesting approach.

    I would like to see an example picture of a finished pcb to see how it compares to mechanical machining/engraving methods.

    What kind of trace width and spacing can you achieve?

    How fast does it vaporize (mm / minute)?

    Maybe a needle-point center-punch would improve drilling accuracy....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to dougw

    Well I haven't really messed with trace thickness since throughout my PCB making I've purposely made the traces as long as I could because I was using the toner transfer method...

     

    But here's some pictures of the first board I have done and messed up image

     

    image

     

    image

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 11 years ago in reply to Former Member

    Looks good.

    It also looks like you have enough laser accuracy to make the pads a bit bigger and easier to drill. A smaller drill bit might help as well.

    I would try to go through the copper with a center punch to provide a drill guide, but might also try a secondary punch to break the copper circles so the drill doesn't tear up the copper.

    You could make the second punch with a broken drill bit shaft (with the correct hole diameter) - grind it flat or concave if you can and use it as a punch just to break through the copper layer, or at least define where the copper will get cut.

    Another trick is to stick a piece of clear tape on the copper side (or both sides) before drilling - this reinforces the copper you don't want removed and minimizes burrs.

    I guess it is too much to ask the laser to burn all the way through the copper so you could skip the etching step?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to dougw

    40W just doesn't seem like it will... Now I am scared to put it at full power though

     

    after a night of poorly reading their code and the better part of this morning hacking together some code, I have managed to modify pcb-gcode to do what i want... It's currently being tested but at least I can go from Eagle to my laser cutter without manually editing the output now image

     

    Ill post results a bit later

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago

    You said here you are using the Toner transfer method I assume you haven't tried the laser yet then . If that is the Laser then I'm pretty impressed. I would also say stay with vector formats and avoid raster like the plague as although you have enough accuracy you do cannot switch off the beam fast enough for a clean edge as it takes several ms to stop lasing and just messes up the etch resist.

     

    Most of the laser software don't take GCode at least the Chinese variety if you can create a DXF then you can import that into almost all the Software. BTW eagle provided a load of tools to do this but I've not tried as it was windows only..

     

    Good luck ....Do you have a link to the pcb-gcode thing BTW?????

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Problemchild

    Previously I was using toner transfers to do PCBs. The images posted here are from my first attempt at lasered PCB's (which still need to be etched afterwards anyway image )

     

    The original place for the pcb-gcode plugin is pcbgcode.org, which is meant for milling the board using a mechanical cutter.

     

     

    My modified version can be found https://www.dropbox.com/s/jsx7z02rd623boq/pcb-gcode3.6.2.4-laser.zip  and should have a bunch of warnings attached to it but doesn't image

    (My cutter is setup to where that spindle on/off turns the laser on/off; the modified code turns the laser on when the Z is negative and off when the Z is positive)

    I would dry run any output from this first...

     

    Here's a board from the newer code, its not perfect but my hand drilled holes are a little better since I had better markers...

    image

     

     

    Perhaps later I can try putting the board back after etching and have the laser cut the holes since theres no copper protecting them now image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to Former Member

    That's a good result then. I'm sure you can remove the resist at least as accurately as any hope process can remove the underlying copper so you are good there. The laser hole thing may well be a pain as you will need some lugs or some such on the bed to align the board again to get the correct registration. Another issue I find is that the FR4 has a tendency to char, maybe that wont be such an issue for just the holes and after all you will be soldering over them any way image

     

    Thanks for the links BTW!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to Problemchild

    How did you give yourself a "helpful answer" on your reply .... you could make a ton of points by answering your own question ....BUG TIMe ..LOL image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Problemchild

    Well at least for now it does what I want and now I can move on to more interesting things like building a new controller board for this cutter image

    It was a cheap 500USD one that came with a crummy proprietary driver board and software, so we've had this scabbed together breakout board to get it to a parallel port to make it usable...

     

     

    The original idea for using a laser cutter and paint was from these two instructables links, the first one has you cut a temp jig out of acrylic so you can put the board in and the other uses some kind of snap jig. But they are both useless if you happen to turn off your machine lol

    Nothing Labs (Rich Olson): 2-Layer Circuit Boards Using Laser Cutter / Chemical Etching

    Double-sided PCBs with a laser cutter

     

    But at least this is a getting stuff done season for me and not procrastinating

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to Former Member

    Are you aware you can get those generic laser cutter controller boards off EBAY that normally already supported in a given set of software... I nearly bought one to repair one of mine!

    Then again it's only a spare of a spare so I'm still intending to do something similar to your self ..good luck

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>