Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) making oval SMD Pads in V6
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 189 subscribers
  • Views 1411 views
  • Users 0 members are here
Related

making oval SMD Pads in V6

e14 Contributor
e14 Contributor over 12 years ago

Hi Everyone,

 

I want to make oval pads for a QFN package.  The recommended approach I have seen is to create an official SMD INSIDE a polygon on TOP layer.  I have done this but there are 2 noticeable issues.

 

1) The resulting pad does not look smooth in gerber viewer in the arc region

2) I get many Eagle DRC and PCB mfg errors because I used a width of 0 for the polygon.  If I use bigger widths then it will look even more choppy.

 

Do I have the methodology correct or is there another way?  Why doesn't Eagle allow oval shaped or arbitrary shaped pads to start with?

 

Best regards,

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to autodeskguest

    Warren,

     

    NOW I get it.  Thanks very much for the detailed response!

     

    Sadry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to e14 Contributor

    On 2/06/2014 10:52 a.m., ezrcer wrote:

    Thanks All for your responses.

     

    I knew that the solution for this is to use a SMD pad and a polygon.

    HOWEVER, the main issue with this as I mentioned in my original post is

    that it generates a lot of DRC errors if I use a thin wire or a thin

    width polygon (below DRC setting) to have a clean small pad.  I was

    trying to make a 0.28x0.85mm oval pad with the arc only on one side so

    any thickness on the polygon or wire was not going to result in a

    clean/accurate rounded pad.  The other side was to be square.

     

    I was able to make a clean pad by using the "roundness" property of an

    SMD pad but the arc is on BOTH sides and I have really no control on the

    arc radius like I would with a wire etc.

     

    Best,

    Sadry

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/114850

     

    I see you ignored my pointer and continued to try to use a polygon. With

    the scale (small sizes_) you are working with, that will not work well

    as you have found out. So you have to use the wire method to create an

    arbitrary pad shape.

     

    Lets use your pad size of 0.28x0.85mm for this walk through:

     

    Place an SMD of size 0.28 x0.28 (yes it's a square one and has no rounding)

    From the center of the SMD drag a wire with a width of 0.28mm.

    (orthogonal)  that is 0.57mm long (0.85 - 0.28 = 0.57)

    That gives you your pad shape. Square at one end, round at the other.

    0.28mm wide and 0.85mm long.

     

    Because the wire is about 11mil wide and that is greater than the

    minimum wire sizes we usually specify in the Design rules there is no

    DRC error because of that wire.

     

    The wire is considered part of the pad because it has one end located on

    the SMD centre.

     

    But there is more to do.

     

    We need to address the solder stop and cream masks as these are not

    generated automatically for the wire, only for the SMD.

     

    As this component is small pitched I would consider defining it all here

    and letting the DRC setting take care of the rest of the board.

    The first thing to do is turn off the stopmask generation for the SMD.

    Uncheck that in the properties of the SMD.

     

    So for the solder mask: Assuming a 0.07mm stop mask distance.

     

    On the tStop layer draw a wire between the same two points as the

    previous wire. Make its width 0.42mm

     

    Next draw a rectangle (tStop layer) over the SMD. You can do this by eye

    being guided by the stopmask of the wire.

     

    Cream is done in a similar way on layer tCream but the sizes are less

    than the size of the wire and SMD.

     

    This is only one pad and you need to handle this group of objects as one

    while in the library. Placing that first SMD in the correct place makes

    copying the pad (group) along the remainder of that row easy, by setting

    the grid size to the pitch of the pads.

     

     

    All the best

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to autodeskguest

    Thanks All for your responses.

     

    I knew that the solution for this is to use a SMD pad and a polygon.  HOWEVER, the main issue with this as I mentioned in my original post is that it generates a lot of DRC errors if I use a thin wire or a thin width polygon (below DRC setting) to have a clean small pad.  I was trying to make a 0.28x0.85mm oval pad with the arc only on one side so any thickness on the polygon or wire was not going to result in a clean/accurate rounded pad.  The other side was to be square.

     

    I was able to make a clean pad by using the "roundness" property of an SMD pad but the arc is on BOTH sides and I have really no control on the arc radius like I would with a wire etc.

     

    Best,

    Sadry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to jameslittlefield

    On 31/05/2014 12:15 p.m., James Littlefield wrote:

    Its sort of a messy solution but what I do is create two pads for each

    actual pad.   One pad is rectangular and of the proper dimension.    I then

    overlay one end of the pad with a circular pad of the right diameter and

    offset from the inside edge by one radius.    This gives you an overall

    shape that has right angle corners on one end and rounded on the other end.

        In eagle 6.x you can assign multiple pads to the same pin on the

    symbol.

     

    Regards,

    Jim

     

     

    ...Or use one SMD and a wire. See HELP > PAD > Arbitrary Pad Shapes

     

    For the outer part of the pad with the square edge you use an SMD with

    no rounding. Then with a wire the same width as the SMD  and starting at

    the SMD point pull out the wire the desired length. The wire has the

    desired round end. The only precaution is to have an SMD that is long

    enough so the rounding of the wire at the SMD end does not show and

    spoil  your square end.

     

    HTH

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to jameslittlefield

    James Littlefield wrote on Fri, 30 May 2014 20:15

    Its sort of a messy solution but what I do is create two pads for each

    actual pad.   One pad is rectangular and of the proper dimension.    I

    then overlay one end of the pad with a circular pad of the right diameter

    and offset from the inside edge by one radius.    This gives you an

    overall shape that has right angle corners on one end and rounded on the

    other end.    In eagle 6.x you can assign multiple pads to the same pin

    on the symbol.

     

     

    Or use one pad and a polygon of any shape to get what you are looking for.

    The centre of the SMD must be within the polygon.  And the width of the

    polygon should be something that won't give you a DRC error--that can be

    tricky when the pads get small.

     

    I think this is the best way as it won't give you and DRC errors.

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

     

    Take advantage of v7 License Promotion right now at

    http://www.eaglecentral.ca

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to jameslittlefield

    Thanks Jim,

     

    What width do you use for the circle?  If you use anything small then you get a lot of DRC errors in layout and from PCB house review.  My rectangular pads are 0.3 x 0.8mm to start with

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jameslittlefield
    0 jameslittlefield over 12 years ago in reply to e14 Contributor

    Its sort of a messy solution but what I do is create two pads for each

    actual pad.   One pad is rectangular and of the proper dimension.    I then

    overlay one end of the pad with a circular pad of the right diameter and

    offset from the inside edge by one radius.    This gives you an overall

    shape that has right angle corners on one end and rounded on the other end.

       In eagle 6.x you can assign multiple pads to the same pin on the

    symbol.

     

    Regards,

    Jim

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    OK,  found out that you can change the roundness % in SMD properties to create oval pads by setting it to 100%.  I made the following QFN part.  However, still do not know how to make a part that has ONLY one side of the pad round.

     

    Any suggestions

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer