Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) making oval SMD Pads in V6
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 189 subscribers
  • Views 1418 views
  • Users 0 members are here
Related

making oval SMD Pads in V6

e14 Contributor
e14 Contributor over 12 years ago

Hi Everyone,

 

I want to make oval pads for a QFN package.  The recommended approach I have seen is to create an official SMD INSIDE a polygon on TOP layer.  I have done this but there are 2 noticeable issues.

 

1) The resulting pad does not look smooth in gerber viewer in the arc region

2) I get many Eagle DRC and PCB mfg errors because I used a width of 0 for the polygon.  If I use bigger widths then it will look even more choppy.

 

Do I have the methodology correct or is there another way?  Why doesn't Eagle allow oval shaped or arbitrary shaped pads to start with?

 

Best regards,

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    OK,  found out that you can change the roundness % in SMD properties to create oval pads by setting it to 100%.  I made the following QFN part.  However, still do not know how to make a part that has ONLY one side of the pad round.

     

    Any suggestions

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    OK,  found out that you can change the roundness % in SMD properties to create oval pads by setting it to 100%.  I made the following QFN part.  However, still do not know how to make a part that has ONLY one side of the pad round.

     

    Any suggestions

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • jameslittlefield
    0 jameslittlefield over 12 years ago in reply to e14 Contributor

    Its sort of a messy solution but what I do is create two pads for each

    actual pad.   One pad is rectangular and of the proper dimension.    I then

    overlay one end of the pad with a circular pad of the right diameter and

    offset from the inside edge by one radius.    This gives you an overall

    shape that has right angle corners on one end and rounded on the other end.

       In eagle 6.x you can assign multiple pads to the same pin on the

    symbol.

     

    Regards,

    Jim

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.