Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) cap round flat is not selectable in line properties
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 838 views
  • Users 0 members are here
Related

cap round flat is not selectable in line properties

e14 Contributor
e14 Contributor over 12 years ago

I am following the manual tutorial to create components and I see lines with square endings (not round). I also noticed there is a property Cap round/ flat for lines but it is not selectable (greyed out and forced to "round"). Also there is a Cap round/flat under the wrench change tool which IS selectable but has no effect, my line is still rounded ends no matter what. I hope somebody figure that out.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 6/25/2014 12:39 PM, Jarvis Weiruiqwfeubaygui wrote:

    I am following the manual tutorial to create components and I see lines

    with square endings (not round). I also noticed there is a property Cap

    round/ flat for lines but it is not selectable (greyed out). Also there

    is a Cap round/flat under the wrench change tool which IS selectable but

    has no effect, my line is still rounded ends no matter what. I hope

    somebody figure that out.

     

    Hi Jarvis,

     

    I hope you're doing well. The ROUND and FLAT cap options only apply to

    ARCs. WIRES and ARCS are fundamentally the same thing in EAGLE hence why

    the options show up in both dialogs.

     

    hth,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to autodeskguest

    Wow you're right, thanks for that, but it does not make sense why the option is blocked with wires and available with arcs. Actually I do need it for arcs foremost (custom RF board)  so that's great it's there at least. There seems there is an untold story here, it should  be available for wires too ( some RF routes must end flat). But i can do as long as it's available with arcs image.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to autodeskguest

    Wow you're right, thanks for that, but it does not make sense why the option is blocked with wires and available with arcs. Actually I do need it for arcs foremost (custom RF board)  so that's great it's there at least. There seems there is an untold story here, it should  be available for wires too ( some RF routes must end flat). But i can do as long as it's available with arcs image.