Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) 9v Battery - VDD and Ground Nets not connecting to battery
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 188 subscribers
  • Views 2502 views
  • Users 0 members are here
Related

9v Battery - VDD and Ground Nets not connecting to battery

e14 Contributor
e14 Contributor over 11 years ago

As the subject describes, I am having trouble connecting my +VDD and -Ground nets to the 9v battery on my current board.

 

I am new to eagle software and am using some Sparkfun libraries. Can anybody provide any insight?

 

I have fully designed the schematic with great success. When switching to board view, to begin tracing out the components - I wanted to start with the source: a 9v battery (thank you sparkfun for the cradle footprint). I have the 9v going to a 5v regulator. The input of the regulator I have connected to the net labeled "VDD" and the output is connected to the net labeled "VCC."

 

The issue is that in schematic view, the battery's + and - terminals clearly are connected to the VDD and Ground nets going to the 5v regulator inputs. When switching to the board view, the battery's terminals will not accept placing a trace to connect to the regulators footprint.

 

What am I doing wrong? The cradle has 2 pins providing a direct connection to the board from the battery. The footprint for these pins, or the two pads, will not accept a trace being placed to make the connection to the regulator.

 

Can anybody identify where my mistake lies?

imageimage

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    Matt Horner wrote:

     

    As the subject describes, I am having trouble connecting my +VDD and

    -Ground nets to the 9v battery on my current board.

     

    I am new to eagle software and am using some Sparkfun libraries. Can

    anybody provide any insight?

     

    I have fully designed the schematic with great success. When switching

    to board view, to begin tracing out the components - I wanted to start

    with the source: a 9v battery (thank you sparkfun for the cradle

    footprint). I have the 9v going to a 5v regulator. The input of the

    regulator I have connected to the net labeled "VDD" and the output is

    connected to the net labeled "VCC."

     

    The issue is that in schematic view, the battery's + and - terminals

    clearly are connected to the VDD and Ground nets going to the 5v

    regulator inputs. When switching to the board view, the battery's

    terminals will not accept placing a trace to connect to the regulators

    footprint.

     

    What am I doing wrong? The cradle has 2 pins providing a direct

    connection to the board from the battery. The footprint for these pins,

    or the two pads, will not accept a trace being placed to make the

    connection to the regulator.

     

    Can anybody identify where my mistake lies?

     

     

    I think you (mis-)used the bus command to draw part of your

    connections.

    That won't work. The purpose of a bus is to bundle multiply signals.

    It never connects directly to a pin. A netstub is allways needed to

    determine which signal (from the bus) is connected to the pin.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago

    Matt Horner wrote:

     

    As the subject describes, I am having trouble connecting my +VDD and

    -Ground nets to the 9v battery on my current board.

     

    I am new to eagle software and am using some Sparkfun libraries. Can

    anybody provide any insight?

     

    I have fully designed the schematic with great success. When switching

    to board view, to begin tracing out the components - I wanted to start

    with the source: a 9v battery (thank you sparkfun for the cradle

    footprint). I have the 9v going to a 5v regulator. The input of the

    regulator I have connected to the net labeled "VDD" and the output is

    connected to the net labeled "VCC."

     

    The issue is that in schematic view, the battery's + and - terminals

    clearly are connected to the VDD and Ground nets going to the 5v

    regulator inputs. When switching to the board view, the battery's

    terminals will not accept placing a trace to connect to the regulators

    footprint.

     

    What am I doing wrong? The cradle has 2 pins providing a direct

    connection to the board from the battery. The footprint for these pins,

    or the two pads, will not accept a trace being placed to make the

    connection to the regulator.

     

    Can anybody identify where my mistake lies?

     

     

    I think you (mis-)used the bus command to draw part of your

    connections.

    That won't work. The purpose of a bus is to bundle multiply signals.

    It never connects directly to a pin. A netstub is allways needed to

    determine which signal (from the bus) is connected to the pin.

    --

     

    Lorenz