Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) 9v Battery - VDD and Ground Nets not connecting to battery
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 188 subscribers
  • Views 2499 views
  • Users 0 members are here
Related

9v Battery - VDD and Ground Nets not connecting to battery

e14 Contributor
e14 Contributor over 11 years ago

As the subject describes, I am having trouble connecting my +VDD and -Ground nets to the 9v battery on my current board.

 

I am new to eagle software and am using some Sparkfun libraries. Can anybody provide any insight?

 

I have fully designed the schematic with great success. When switching to board view, to begin tracing out the components - I wanted to start with the source: a 9v battery (thank you sparkfun for the cradle footprint). I have the 9v going to a 5v regulator. The input of the regulator I have connected to the net labeled "VDD" and the output is connected to the net labeled "VCC."

 

The issue is that in schematic view, the battery's + and - terminals clearly are connected to the VDD and Ground nets going to the 5v regulator inputs. When switching to the board view, the battery's terminals will not accept placing a trace to connect to the regulators footprint.

 

What am I doing wrong? The cradle has 2 pins providing a direct connection to the board from the battery. The footprint for these pins, or the two pads, will not accept a trace being placed to make the connection to the regulator.

 

Can anybody identify where my mistake lies?

imageimage

  • Sign in to reply
  • Cancel
Parents
  • ingit
    0 ingit over 11 years ago

    Not to worry much about it follow these simple steps image image

    1.) Open the layer selection dialog box.

    image

    2.) In that select the "Pins Layer" and hit apply.

    3.) After that you will see some bubble kind of things around the pins of each component, as shown below.

    image

    4.) Now connect a net to that bubble and connect to another components pin with the bubble, or simply use the junction tool, below buss tool.

    Actually connection is from bubble to bubble, not any other part of the component.

    Connection is possible when there is a bubble. If pins layer is disabled then also connection is between bubbles.

    image

    that plus symbol with a dot in center. use that.

    If there is no connection between two pins i.e. bubbles, no net will be seen on the board.image image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ingit
    0 ingit over 11 years ago

    Not to worry much about it follow these simple steps image image

    1.) Open the layer selection dialog box.

    image

    2.) In that select the "Pins Layer" and hit apply.

    3.) After that you will see some bubble kind of things around the pins of each component, as shown below.

    image

    4.) Now connect a net to that bubble and connect to another components pin with the bubble, or simply use the junction tool, below buss tool.

    Actually connection is from bubble to bubble, not any other part of the component.

    Connection is possible when there is a bubble. If pins layer is disabled then also connection is between bubbles.

    image

    that plus symbol with a dot in center. use that.

    If there is no connection between two pins i.e. bubbles, no net will be seen on the board.image image