Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) SOT223; Joining pad to tab
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 2668 views
  • Users 0 members are here
  • sot223
Related

SOT223; Joining pad to tab

e14 Contributor
e14 Contributor over 11 years ago

Hi folks.

 

I'm having a problem with using the tab on SOT223 voltage regulators that use the tab as a heatsink and is usually the same connection as the centre pin. But when I add a  polygon around it to increase the surface area, it either leaves the centre pin disconnected or the tab is isolated.

 

Is there a nice way to achieve this?

 

Thank you.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Name the poly the same name network connected to that pad has. Via naming button, not via info window.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    I've tried this, but it does not work. It does work with other components, but not this type for some reason.

     

    There seems to be only 3 connections allowed on this 4 connection component. I would rather there be 4, even if it means a messy schematic, as this is mainly a board design program. I would rather have to link the tab on the schematic manually to one of the pins to match the component needed.

     

    Can I edit the component to add this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Which voltage regulator? Tell me how it is called and in what library it is, I'll investigate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hpvoelpel
    0 hpvoelpel over 11 years ago in reply to e14 Contributor

    Am 14.12.2014 um 12:39 schrieb Richard Perkins.:

    I have tried other components with this method and it seems simple with

    those, but I'm sure I was trying the same thing with the two I

    mentioned, and it just wasn't working. The main difference I see is that

    the others have the tab numbered 4, so if this is present, then there is

    no problem. The problem seems to start when the tab is not numbered.

    Maybe I just found an awkward couple. If you want to check other sot223

    devices to find one without that number 4 tab, and try connecting to it.

     

    Well I have learned a lot more by confronting a problem and finding

    helpful people, and I am still a novice with Eagle, so I expect I will

    be back with more dumb questions.:^0

     

    Thank you all for your help.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/134754

     

     

    PADs are what you see in the board and in the packages, PINs are what

    you see in the schematic and the symbols. You can connect multiple PADs

    to one PIN. This will solve your problem. It has to be done in zthe LBR

    editor. If you want to have a heatsink copper area around a PAD without

    thermals, just draw a polygon in the board and give it the same name as

    the signal the PAD is connected to, and uncheck 'Thermals'. You will see

    the checkbox by activating 'INFO' and clicking on the poly.

    Ever tried 'help connect', 'help poly' etc?

    And, after all, it would be a really good idea to read the manual...

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to autodeskguest

    I have tried other components with this method and it seems simple with those, but I'm sure I was trying the same thing with the two I mentioned, and it just wasn't working. The main difference I see is that the others have the tab numbered 4, so if this is present, then there is no problem. The problem seems to start when the tab is not numbered. Maybe I just found an awkward couple. If you want to check other sot223 devices to find one without that number 4 tab, and try connecting to it.

     

    Well I have learned a lot more by confronting a problem and finding helpful people, and I am still a novice with Eagle, so I expect I will be back with more dumb questions.image

     

    Thank you all for your help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to autodeskguest

    I have tried other components with this method and it seems simple with those, but I'm sure I was trying the same thing with the two I mentioned, and it just wasn't working. The main difference I see is that the others have the tab numbered 4, so if this is present, then there is no problem. The problem seems to start when the tab is not numbered. Maybe I just found an awkward couple. If you want to check other sot223 devices to find one without that number 4 tab, and try connecting to it.

     

    Well I have learned a lot more by confronting a problem and finding helpful people, and I am still a novice with Eagle, so I expect I will be back with more dumb questions.image

     

    Thank you all for your help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • hpvoelpel
    0 hpvoelpel over 11 years ago in reply to e14 Contributor

    Am 14.12.2014 um 12:39 schrieb Richard Perkins.:

    I have tried other components with this method and it seems simple with

    those, but I'm sure I was trying the same thing with the two I

    mentioned, and it just wasn't working. The main difference I see is that

    the others have the tab numbered 4, so if this is present, then there is

    no problem. The problem seems to start when the tab is not numbered.

    Maybe I just found an awkward couple. If you want to check other sot223

    devices to find one without that number 4 tab, and try connecting to it.

     

    Well I have learned a lot more by confronting a problem and finding

    helpful people, and I am still a novice with Eagle, so I expect I will

    be back with more dumb questions.:^0

     

    Thank you all for your help.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/134754

     

     

    PADs are what you see in the board and in the packages, PINs are what

    you see in the schematic and the symbols. You can connect multiple PADs

    to one PIN. This will solve your problem. It has to be done in zthe LBR

    editor. If you want to have a heatsink copper area around a PAD without

    thermals, just draw a polygon in the board and give it the same name as

    the signal the PAD is connected to, and uncheck 'Thermals'. You will see

    the checkbox by activating 'INFO' and clicking on the poly.

    Ever tried 'help connect', 'help poly' etc?

    And, after all, it would be a really good idea to read the manual...