Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) SOT223; Joining pad to tab
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 2677 views
  • Users 0 members are here
  • sot223
Related

SOT223; Joining pad to tab

e14 Contributor
e14 Contributor over 11 years ago

Hi folks.

 

I'm having a problem with using the tab on SOT223 voltage regulators that use the tab as a heatsink and is usually the same connection as the centre pin. But when I add a  polygon around it to increase the surface area, it either leaves the centre pin disconnected or the tab is isolated.

 

Is there a nice way to achieve this?

 

Thank you.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Name the poly the same name network connected to that pad has. Via naming button, not via info window.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    I've tried this, but it does not work. It does work with other components, but not this type for some reason.

     

    There seems to be only 3 connections allowed on this 4 connection component. I would rather there be 4, even if it means a messy schematic, as this is mainly a board design program. I would rather have to link the tab on the schematic manually to one of the pins to match the component needed.

     

    Can I edit the component to add this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 11 years ago in reply to e14 Contributor

    You are right, the schematic symbol should have a pin for each pin on the device. You can edit the device to add the pin. You could check the 78L05F device in the Linear library to see how they did it there in the SOT89, but note they connected the 2 pins in the device package.

    The LD117AS12TR device in the V-Reg library has an unconnected pad, you can just add a pin to the symbol and connect it in the device window, or create a new symbol with 4 pins.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 11 years ago in reply to e14 Contributor

    You are right, the schematic symbol should have a pin for each pin on the device. You can edit the device to add the pin. You could check the 78L05F device in the Linear library to see how they did it there in the SOT89, but note they connected the 2 pins in the device package.

    The LD117AS12TR device in the V-Reg library has an unconnected pad, you can just add a pin to the symbol and connect it in the device window, or create a new symbol with 4 pins.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to dougw

    Thank you for your help. I have finally solved it !

     

    As you say, I've edited the part after finding it in the library and added a pin which was the easy part.  What I had to do then was to "connect" it which was a little complicated and took me a while to find out how.  I saw a "Connect" tab in the lower right window but I've forgotten how I got there. Anyway, this shows you the pins and pad connections. I got confused with the centre panel, as anything in there got added to the top right panel, sometimes with a link symbol, and sometimes a broken link symbol. I'm sure I can find out why eventually, but I did manage to get 4 pins connected to 4 pads, and got a green tick. After saving, this was easy to replace the part I had  - and gave me that extra connection on the schematic. When this was connected, I got an airwire on the board which was correct. Clicking ratsnest filled it in as my ground around the pad with no gaps!

     

    So happy.image

     

    One wrinkle is the pin is given a name which I couldn't see a way to edit that at the time, but maybe it is easy to re-name it before I placed it.