Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Can part bodies overlap onto SMD pads?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 187 subscribers
  • Views 756 views
  • Users 0 members are here
  • eagle
  • overlap
Related

Can part bodies overlap onto SMD pads?

edwardmatos
edwardmatos over 11 years ago

Hello, I suspect this is a question that has been asked and answered before, but my searches for the answer are made difficult by the large number of other discussion topics on other overlapping objects in Eagle. So, apologies in advance if you've already answered/discussed this before - I couldn't find the topic!

 

The screenshot below shows a large surface mount diode placed next to a through-hole mount connector. The body outlines of these components are shown in white and yellow lines:

 

image

The body outlines would suggest that the diode body is going to sit on the through hole pad, and the connector body is going to sit on the surface mount pad. My question is: is this a problem? The bodies themselves aren't close to each other, but are there any issues I should be wary of during reflow soldering or any other process during assembly that would make this a problem?

 

Clearly in this screenshot there is plenty of space to move the components further apart and avoid this overlap. I just thought I'd use this as clear example to illustrate my question.

 

Many thanks for any thoughts!

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 26/01/15 17:51, Edward Matos wrote:

    The body outlines would suggest that the diode body is going to sit on

    the through hole pad, and the connector body is going to sit on the

    surface mount pad. My question is: is this a problem? The bodies

    themselves aren't close to each other, but are there any issues I should

    be wary of during reflow soldering or any other process during assembly

    that would make this a problem?

     

    I'm sure there will be a more expert opinion shortly, but...

     

    I would be cautious of the diode overlapping the through hole pad. There

    would be a risk of capillary bleeding and potentially a short (although

    in this particular case the pads are connected anyway).

     

    The through-hole connector will usually be fitted later and soldered

    from the other side, so it's not a problem for it to overlap a pad, but

    you can't rely on that in mass production so it would be better to avoid

    that overlap too. Besides, if the soldering of the diode is built up a

    bit (which can happen) then it might foul and prevent the connector

    sitting flush.

     

    All in all, you may well get away with it but it has a potential to

    cause problems so don't do it.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 26/01/15 17:51, Edward Matos wrote:

    The body outlines would suggest that the diode body is going to sit on

    the through hole pad, and the connector body is going to sit on the

    surface mount pad. My question is: is this a problem? The bodies

    themselves aren't close to each other, but are there any issues I should

    be wary of during reflow soldering or any other process during assembly

    that would make this a problem?

     

    I'm sure there will be a more expert opinion shortly, but...

     

    I would be cautious of the diode overlapping the through hole pad. There

    would be a risk of capillary bleeding and potentially a short (although

    in this particular case the pads are connected anyway).

     

    The through-hole connector will usually be fitted later and soldered

    from the other side, so it's not a problem for it to overlap a pad, but

    you can't rely on that in mass production so it would be better to avoid

    that overlap too. Besides, if the soldering of the diode is built up a

    bit (which can happen) then it might foul and prevent the connector

    sitting flush.

     

    All in all, you may well get away with it but it has a potential to

    cause problems so don't do it.