Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Which part for ends?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 477 views
  • Users 0 members are here
Related

Which part for ends?

autodeskguest
autodeskguest over 11 years ago

Which Eagle part should I use when the end of a component goes to

nowhere (actually it does, but to another circuit which I'm not building)

 

or....

 

a schematic which has connections on the PCB without connectors (i.e.

cables are soldered directly to the PCB)?

 

Should I just leave the end of the nets in open air and label them with

a description, or should there be some sort of connection pin, circle,

arrow or whatever?

 

L.

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to dukepro

    On 21/09/2015 14:31, Chuck Huber wrote:

     

    >> On 09/21/2015 05:18 AM, Logyx wrote:

    >> Which Eagle part should I use when the end of a component goes to

    >> nowhere (actually it does, but to another circuit which I'm not

    >> building)

    >>

    >> or....

    >>

    >> a schematic which has connections on the PCB without connectors (i.e.

    >> cables are soldered directly to the PCB)?

     

     

    You're going to need a place on the board to connect the cable.  It'd be

    best to create a connector with an SMD or through-hole pad.

     

    Yes, that makes sense.

    I found a library called "Wirepad" which seems to be what I need.

     

     

    The connector symbol on the schematic would show the connection so some

    external device, and should be noted as such.

     

    I've done some schematics which are extracted from a bigger one (i.e.

    I'm working on just a specific section of the whole circuit).

    Obviously I'm not going to make a PCB for this but I'm only developing

    something. So I should add a connector part in this case to where it

    attaches to the rest of the circuit, to keep it neat and tidy?

     

    L.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 11 years ago

     

    You're going to need a place on the board to connect the cable.  It'd be

    best to create a connector with an SMD or through-hole pad.

     

    The connector symbol on the schematic would show the connection so some

    external device, and should be noted as such.

     

    HTH,

        - Chuck

     

    On 09/21/2015 05:18 AM, Logyx wrote:

    Which Eagle part should I use when the end of a component goes to

    nowhere (actually it does, but to another circuit which I'm not building)

     

    or....

     

    a schematic which has connections on the PCB without connectors (i.e.

    cables are soldered directly to the PCB)?

     

    Should I just leave the end of the nets in open air and label them

    with a description, or should there be some sort of connection pin,

    circle, arrow or whatever?

     

    L.