Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) v7.3.0 GUI Update? (Release Notes)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Subscribers 191 subscribers
  • Views 1468 views
  • Users 0 members are here
Related

v7.3.0 GUI Update? (Release Notes)

JasonTraud
JasonTraud over 11 years ago

The release notes for v7.3.0 mentions a more modern look and feel of the Eagle GUI. Is this something that is possible with the updated graphics libraries or were there just minor polishing changes.

 

I've noticed no issues with the newer version and it runs great. Just curious about this line in the release notes.

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago
    • Library overview screen that enables the user to see the complete chosen library at a glance. The user can easily rename and remove devices, packages and symbols directly from the library overview screen

    • New library cross-references: direct access from the library overview to the cross referenced packages and symbols for devices. Back-references to devices are also available with one click.

    • New and simplified full library context view and easy submenu access available. Descriptions can be viewed and changed directly from context menu

    • Additional icon and command to view full library structure with one click

     

    In my view these are much needed requests from users and not so much a major change.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 11 years ago
    • Library overview screen that enables the user to see the complete chosen library at a glance. The user can easily rename and remove devices, packages and symbols directly from the library overview screen

    • New library cross-references: direct access from the library overview to the cross referenced packages and symbols for devices. Back-references to devices are also available with one click.

    • New and simplified full library context view and easy submenu access available. Descriptions can be viewed and changed directly from context menu

    • Additional icon and command to view full library structure with one click

     

    In my view these are much needed requests from users and not so much a major change.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • JasonTraud
    0 JasonTraud over 11 years ago in reply to clem57

    That is actually really awesome. It looks like it cuts out the need to ever jump into a text editor to manage libraries. 

     

    Hopefully the cross-referencing works like I hope it does, just not finding documentation on it.