Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Help?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 187 subscribers
  • Views 2427 views
  • Users 0 members are here
Related

Help?

autodeskguest
autodeskguest over 11 years ago

Hi, I am new to this program. I have tried everything and can't figure out

why nothing I do is working.

 

I need a simple adapter board. I watched videos and everything. I am trying

to simply make a small board that has 42 holes for a m27c160 eprom to fit a

36 hole board.

 

I have went here http://schematicpal.com/ and downloaded the eprom

M27C801-100B1 it shows two boxes the left red box and the right green

circles in the black box. I can only place the red box in the schematic

when I need the other one to just place the holes for me. When I click on

circles they are not circles but pads, I need holes!

 

Plus the eprom clearly has 42 legs yet the only Library file you can place

in is missing majority of pins. This blows my mind it's not even accurate?

You go to the board view and magically it shows the entire chip but

completely useless as it will not let you run traces, that has to be done

in the schematic where they don't exist!!!

 

I have tried drawing circles "holes" manually but when I switch to board

view it does not bring them in? I tried grouping the 42 circles together as

that is what I need for the 27c160 eprom but it does nothing.

 

I can't believe how difficult this is. I want to order these boards but I

need a gerber file. I could whip this thing out in paint in like 10

minutes, here I have wasted countless hours trying to decipher this program

that will not do anything I want it to.

 

I think learning a new language would be easier them deciphering this

program.

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 11 years ago

    Are you sure you're using the right software for your particular desired workflow?

    It doesn't sound like it.

    EAGLE is all about schematics and then building a circuit board from there.

    Schematics parts often don't use the same number of pins as a physical part.

    If you just want to lay 'holes', then there may be other software out there that

    you could be using - EAGLE would be extreme overkill for that -

    although it could do it, you'd have to plough through the user documentation -

    it's not intended to a MS Paint replacement and so the workflow isn't as simple

    with EAGLE.

    By the way, your part number M27C801-100B1 really is a 32-pin device,

    not a 42-pin device.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to shabaz

    I know the M27C801-100B1 is a 32 dip, however it is the chip I currently

    use right now for my boards. I need to move up to the bigger chip which is

    why I need the adapter board made. I only chose that from the library as it

    was all there was and I knew the hole sizes and spacing was what I needed.

     

    I was hoping I could just lay that chip out twice or something and over lap

    the pins or just add the extra holes needed. I'm just going to call it a

    day and pay somebody to do this. I really wanted to do it myself but I

    can't waste all this time into this program.

     

    As far as other programs, maybe but I'm pretty burnt out and annoyed right

    now that I don't think I want to waste any more time learning another

    program that may not be correct for what I need done.

     

    Thanks for the reply. It's nice to get some input from someone.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    On 27/09/15 03:49, Greg wrote:

    As far as other programs, maybe but I'm pretty burnt out and annoyed right

    now that I don't think I want to waste any more time learning another

    program that may not be correct for what I need done.

     

    It seems to me you've not made any effort to learn this one, nor to

    learn the basic principles of the task this one is designed for. Now you

    are fully at liberty to not want to put the effort in, but if you do

    take that tack then you have a moral duty to accept the blame yourself

    and NOT BLAME THE TOOL. It's a perfectly good tool, you just don't want

    to use it right. Like the blunt edge of the pizza knife, or the

    screwdriver as a hammer.

     

    The work flow in electronics design IS ALWAYS to start with a schematic,

    select components with appropriate packages, create library parts as

    required, and only then start to worry about layout. THIS DOES STILL

    APPLY in the trivial case you have, regardless of whether you think "oh

    it's just..." - because even that statement is a description of the

    schematic you should start by drawing. Or rather, the statement is a

    vague, hand-wavy marketing overview of the requirement. You really need

    to formalise that requirement by drawing a schematic. Only then can you

    consider how to implement it on a PCB.

     

    If you give up on your preconception that "it's too trivial" and admit

    that for a proper job you need to be precise in your requirements, then

    you'll find that Eagle does help a lot. Sure, it's a non-trivial

    learning curve, but then all such tools are.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    Well it has pads on both sides. I used a "header pin" layout remember.

    Trust me I barely understand what I did. I just dropped the library file

    and sent it out. I actually got some boards in today. I only ordered 10 to

    make sure they will work.

     

    I need the 1/4" hole as the case it goes into has a 3/16" peg that pushes

    against the main pcb that this will be sitting atop of.

     

    The only thing I did not do that I have heard mixed feelings about is

    ground the unused pins. I guess I could do that before I order the bulk of

    the load, but I made a test board and ran like 35 wires by hand and just

    bent up the pins to nothing and it works fine, that was months ago I did

    that and it still works fine?

     

    http://s14.photobucket.com/user/icemanxp300/media/100_1030_zps9sraditr.jpg.html

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    Quote:

    M27C801-100B1

     

    Except for the mounting hole, you need PADS not holes. A pad is a hole with

    copper around it. You cannot connect copper traces to holes. You can only

    connect traces to pads. According the the drill symbols, your mounting hole

    is actually the same diameter as the drill for the pads. To make it 1/4",

    click on "i", then click on the hole. In the dialog box you can edit the

    drill size of the hole. BTW, 1/4" is HUGE. You will then have to re-route

    your board. First, you need to rip-up the traces. Type "RIP *" (without the

    quotes) into the command line. Then route the board.

    I see that there are several pins that aren't connected to anything. All

    CMOS inputs *MUST* be connected to either +V via a resistor (i.e. 10K) or

    directly to ground. CMOS inputs will act erratically (bounce between '0'

    and '1') if left floating (unconnected), and your board will act

    erratically, too. Floating inputs also draw more power. You may be able to

    get away with leaving them float, but then you will have failures in the

    field.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    Quote:

    M27C801-100B1

     

    Except for the mounting hole, you need PADS not holes. A pad is a hole with

    copper around it. You cannot connect copper traces to holes. You can only

    connect traces to pads. According the the drill symbols, your mounting hole

    is actually the same diameter as the drill for the pads. To make it 1/4",

    click on "i", then click on the hole. In the dialog box you can edit the

    drill size of the hole. BTW, 1/4" is HUGE. You will then have to re-route

    your board. First, you need to rip-up the traces. Type "RIP *" (without the

    quotes) into the command line. Then route the board.

    I see that there are several pins that aren't connected to anything. All

    CMOS inputs *MUST* be connected to either +V via a resistor (i.e. 10K) or

    directly to ground. CMOS inputs will act erratically (bounce between '0'

    and '1') if left floating (unconnected), and your board will act

    erratically, too. Floating inputs also draw more power. You may be able to

    get away with leaving them float, but then you will have failures in the

    field.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    Well it has pads on both sides. I used a "header pin" layout remember.

    Trust me I barely understand what I did. I just dropped the library file

    and sent it out. I actually got some boards in today. I only ordered 10 to

    make sure they will work.

     

    I need the 1/4" hole as the case it goes into has a 3/16" peg that pushes

    against the main pcb that this will be sitting atop of.

     

    The only thing I did not do that I have heard mixed feelings about is

    ground the unused pins. I guess I could do that before I order the bulk of

    the load, but I made a test board and ran like 35 wires by hand and just

    bent up the pins to nothing and it works fine, that was months ago I did

    that and it still works fine?

     

    http://s14.photobucket.com/user/icemanxp300/media/100_1030_zps9sraditr.jpg.html

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.