Hi Guys
I'm totally new to this. I'm trying to build a 4 channel opamp (boost my signal about 100x)
I'm hoping someone has the time to quickly check my design and see if it makes sense and perhaps let me know how to improve it.
Thanks
Jacob
Hi Guys
I'm totally new to this. I'm trying to build a 4 channel opamp (boost my signal about 100x)
I'm hoping someone has the time to quickly check my design and see if it makes sense and perhaps let me know how to improve it.
Thanks
Jacob
| opamp.zip |
Am 07.10.2015 um 14:02 schrieb Jacob Thastrup:
Hi Guys
I'm totally new to this. I'm trying to build a 4 channel opamp (boost my
signal about 100x)
I'm hoping someone has the time to quickly check my design and see if it
makes sense and perhaps let me know how to improve it.
Thanks
Jacob
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/162669
Attachments:
opamp.zip
No capacitors?
--
Mit freundlichen Grüßen / With best regards
Joern Paschedag
You mean to filter the input?
Hi,
At least capacitors should be added on the supply...
I don"t know the purpose of your circuit but you should add at least a small one capacitor (10 to 100 nF) placed near the power supply input pins of the LM324, and a electrolytic caacitor (few µF) rignt after the supply input connector.
En large 24V supply trace, and for the GND you can enlarge the trace or better add a GND plane (polygon).
Guillaume
Guillaume barrey[1
wrote on Sun, 11 October 2015 08:04]Hi,
The sensor cell will produce a voltage, between the 2 signals :
- the signal you will connect to your amplifier input
- and the GND.
Only the voltage between these 2 signals (the difference) is
important.
The current that will flow out from your cell into the input of the
amplifier is exactly the same than the current flowing from the GND of
your board into the GND pin of your cell.
So, the role played by the 2 wires of the oxygen cell (signal and
GND)
is equivalent, and there is no reason to have a different path (except
if GND is also used to supply the sensor see (*) ).
On the amplifier side : it amplifies the difference between the
input
signal and the GND plane, the GND plane is a REFERENCE.
If instead of connecting directly the GND of sensor to your board, you
connect it to a point away from the plane (name it STAR point), with
all
the other sensor GND and supply GND, then you connect this start point
to your board with a single wire. On the paper this will work....
but....
In this last GND segment (wire from the GND plane and star point)
you
will have the sum of all the currents of all sensors, plus the current
drained by the amplifier it self (and this last one is far more
important than the others).
Where is the problem ?
The problem is that the copper is a good conductor, but not an ideal
one
!
You will have a little voltage difference between your GND plane and
the
start point, that will be dependent of that current, and the length of
the wire, and so amplifier REFERENCE will not be exactly the reference
of the sensor.
In other word, each signal will be polluted with the signal of the
other
cell and the consumption of the amplifier...
There is also other advantages of using same path for your sensor: you
can use twisted pair wire, that way you reduce noise, specially if
your
sensor are far away from the borad.
Just one thing (*) : I don't know your sensor: is this sensor need a
supply ? How this supply is wired? is the GND of sensor is only a
output
reference or also used for the return path of the supply ? because in
that case you have to figure how best can the GND be wired.... there
is
no magic solution, and we can help you unless you give us more info...
Sorry with this very quick fast ultra simplified explanation... and if
you want to have more fun... you can also question yourself about the
output of your amplifier : How the GND path mcan be optimised and
wired,
on the output side (I suppose you will connect it to an acquisition
device...)
Guillaume
--
To view any images and attachments in this post, visit:
Hi Guillaume
Thank you again for your reply.
Just to make sure I understand. I should still connect all the GND signals
together, just at different points on the GND plane?
The Sensor does not require any power, it generates it itself though a
chemical reaction (dependent on the oxygen fraction).
The amplified signal will be going to an acquisition device, should I also
wire their GND "away" from the power supply GND? I guess I could wire them
in the same terminal as the GND from each sensor?
Thanks
Jacob
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
Hi,
The sensor cell will produce a voltage, between the 2 signals :
- the signal you will connect to your amplifier input
- and the GND.
Only the voltage between these 2 signals (the difference) is important. The current that will flow out from your cell into the input of the amplifier is exactly the same than the current flowing from the GND of your board into the GND pin of your cell.
So, the role played by the 2 wires of the oxygen cell (signal and GND) is equivalent, and there is no reason to have a different path (except if GND is also used to supply the sensor see (*) ).
On the amplifier side : it amplifies the difference between the input signal and the GND plane, the GND plane is a REFERENCE.
If instead of connecting directly the GND of sensor to your board, you connect it to a point away from the plane (name it STAR point), with all the other sensor GND and supply GND, then you connect this start point to your board with a single wire. On the paper this will work.... but....
In this last GND segment (wire from the GND plane and star point) you will have the sum of all the currents of all sensors, plus the current drained by the amplifier it self (and this last one is far more important than the others).
Where is the problem ?
The problem is that the copper is a good conductor, but not an ideal one !
You will have a little voltage difference between your GND plane and the start point, that will be dependent of that current, and the length of the wire, and so amplifier REFERENCE will not be exactly the reference of the sensor.
In other word, each signal will be polluted with the signal of the other cell and the consumption of the amplifier...
There is also other advantages of using same path for your sensor: you can use twisted pair wire, that way you reduce noise, specially if your sensor are far away from the borad.
Just one thing (*) : I don't know your sensor: is this sensor need a supply ? How this supply is wired? is the GND of sensor is only a output reference or also used for the return path of the supply ? because in that case you have to figure how best can the GND be wired.... there is no magic solution, and we can help you unless you give us more info...
Sorry with this very quick fast ultra simplified explanation... and if you want to have more fun... you can also question yourself about the output of your amplifier : How the GND path mcan be optimised and wired, on the output side (I suppose you will connect it to an acquisition device...)
Guillaume
Guillaume barrey[1
wrote on Sat, 10 October 2015 05:53]Hi,
That last design is better, the ground plane is OK.. You remove the
big
capacitor (your 5µF) I suggested to check the value and the
package,
but not t remove it ? If it was one of my design I would put a 10µF
electrolytic capacitor between GND and +24V, just right after the
supply
connector...
Nice work ....
Ah ok hehe, I've added the 10uF capasitor now.
Quote:
I think there should be a ground connection for each channel. In other
words, you will need 3-pin instead of 2-pin connectors. Otherwise your
only ground connection is through the power supply connector. The ground
pin should be between each input and output pin.
I'm not sure I understand this bit.
The signal I'm trying to amplify is coming from small oxygen cells
(galvanic cells). If I understand what you are suggesting, is that I use
the GND from each cell to connect to their respective inverting input of
the opamp? My original idea was to tie all the GND lines from the cells
into the same GND connector (the one I also connect the power supply to).
Potentially a stupid question.. will that work? I don't need to ground
everything "together"?
Quote:
If you swap the ends of R5 and R6, then you can have a single trace for
OUT3, instead of 2 traces. You can do the same thing for the other
channels.
Once again thanks for all the help!!
-Jacob
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
| test5-3.zip |
Jacob Thastrup wrote on Fri, 09 October 2015 12:34
Once again thank you guys!!
Guillaume, thank you for the explanation it really helps!
I've added a ground plane to Joern's design... does that make sense?
I hope you can see the attached file..otherwise I'll go register at
eaglecentral as well.
-Jacob
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/162904
Attachments:
test5.zip
I think there should be a ground connection for each channel. In other
words, you will need 3-pin instead of 2-pin connectors. Otherwise your only
ground connection is through the power supply connector. The ground pin
should be between each input and output pin. I agree with others that you
should have a cap across the power supply terminals. Also, on your layout,
if you switch to a finer grid (i.e. 10 mil aka(0.01")), you can move some
traces slightly and improve the ground plane near the left end of the chip
(also changing the polygon width to 12 mils helps). If you swap the ends of
R5 and R6, then you can have a single trace for OUT3, instead of 2 traces.
You can do the same thing for the other channels.
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
Am 09.10.2015 um 18:34 schrieb Jacob Thastrup:
Once again thank you guys!!
Guillaume, thank you for the explanation it really helps!
I've added a ground plane to Joern's design... does that make sense?
I hope you can see the attached file..otherwise I'll go register at
eaglecentral as well.
-Jacob
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/162904
Attachments:
test5.zip
You should go there anyway. It is just the better link to the cadsoft
They don't have trouble with attachments (as you have seen).
BTW my "design" was just a suggestion.
Maybe you should add an electrolytic capacitor in general and foresee
some holes to screw this print somewhere.
--
Mit freundlichen Grüßen / With best regards
Joern Paschedag
Hi,
That last design is better, the ground plane is OK.. You remove the big capacitor (your 5µF) I suggested to check the value and the package, but not t remove it ? If it was one of my design I would put a 10µF electrolytic capacitor between GND and +24V, just right after the supply connector...
Nice work ....
Once again thank you guys!!
Guillaume, thank you for the explanation it really helps!
I've added a ground plane to Joern's design... does that make sense?
I hope you can see the attached file..otherwise I'll go register at eaglecentral as well.
-Jacob
| test5.zip |
On 09.10.2015 11:12, Joern Paschedag wrote:
Am 09.10.2015 um 10:42 schrieb Joern Paschedag:
Am 08.10.2015 um 17:38 schrieb Jacob Thastrup:
Hi Joern
Maybe I'm getting it wrong. But I don't see any files from you?
Thanks
-Jacob
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/162826
I attached it but I suppose it is the glorious interconnection between
the newsgroup and element 14 that never works since years...
Next try now...
No, sorry it didn't go throu, maybe because I'm not registered at
element14 .
And I'm not interested to register there.
You can find them here
http://www.eaglecentral.ca/forums/index.php/t/51848/5abd43c14367c14cffef482390e897d4/
Am 09.10.2015 um 10:42 schrieb Joern Paschedag:
Am 08.10.2015 um 17:38 schrieb Jacob Thastrup:
Hi Joern
Maybe I'm getting it wrong. But I don't see any files from you?
Thanks
-Jacob
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/162826
I attached it but I suppose it is the glorious interconnection between
the newsgroup and element 14 that never works since years...
Next try now...
No, sorry it didn't go throu, maybe because I'm not registered at
element14 .
And I'm not interested to register there.
--
Mit freundlichen Grüßen / With best regards
Joern Paschedag
Am 08.10.2015 um 17:38 schrieb Jacob Thastrup:
Hi Joern
Maybe I'm getting it wrong. But I don't see any files from you?
Thanks
-Jacob
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/162826
I attached it but I suppose it is the glorious interconnection between
the newsgroup and element 14 that never works since years...
Next try now...
--
Mit freundlichen Grüßen / With best regards
Joern Paschedag
Am 08.10.2015 um 17:38 schrieb Jacob Thastrup:
Hi Joern
Maybe I'm getting it wrong. But I don't see any files from you?
Thanks
-Jacob
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/162826
I attached it but I suppose it is the glorious interconnection between
the newsgroup and element 14 that never works since years...
Next try now...
--
Mit freundlichen Grüßen / With best regards
Joern Paschedag
hi,
I've viewed your layout and edit it.
some tips for your next pcb
* first of all: place parts, route power supply & gnd, critical tracks like bus and the all the other things
* layout the pcb by following your nets of the schematics
* try parts in different ways THT (horizontal / vertical) or SMD
* route the tracks as short as possible
* place holes to fix or parts to screw your pcb on something
An example off your pcb with short tracks, etc. is attached. 
| Test5_edit.zip |
Guillaume barrey[1
wrote on Wed, 14 October 2015 13:10]Hi,
That's Great !
Just a last little advice for the GND plane.
When my board is almost finish, I do some little adjustment to be sure
that my GND plane will be good.... It's hard to explain with my poor
English....(sorry to be a French frog:p)
I hide all layer except the dimension, via, pads and the copper layer
on
which I work, and I run a ratsnest command to process the polygons
Then you use the show command and select the polygon (in your case
you
only have GND). The polygon is highlighted so you can see it well.
Now you try to imagine how the current can flow from here and there...
Sometime you will see that for connecting to point that are not
really
far from each other, the current need to do a huge travel because the
plane is interrupted by some other tracks. Sometime it's easy to
reduce
drastically the effective distance just by moving a little bit a track
or a part.
In your example, the +24V track going from C1 to IC1 completely cut he
polygon. If you move down a little this track, the GND plane will be
not
cut any more...
That way, I check all the little improvement I can do, and some time
it's not enough, so I reduce the isolation or the wire of the polygon.
I do that for all polygons, layer by layer (copper layers of course).
But any way good job !
Guillaume.
--
To view any images and attachments in this post, visit:
Hi Guys
Sorry for the slow response.
Thank you all for all the help. I feel I have learned a lot already!
Best wishes
Jacob
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
Hi,
That's Great !
Just a last little advice for the GND plane.
When my board is almost finish, I do some little adjustment to be sure that my GND plane will be good.... It's hard to explain with my poor English....(sorry to be a French frog
)
I hide all layer except the dimension, via, pads and the copper layer on which I work, and I run a ratsnest command to process the polygons
Then you use the show command and select the polygon (in your case you only have GND). The polygon is highlighted so you can see it well.
Now you try to imagine how the current can flow from here and there...
Sometime you will see that for connecting to point that are not really far from each other, the current need to do a huge travel because the plane is interrupted by some other tracks. Sometime it's easy to reduce drastically the effective distance just by moving a little bit a track or a part.
In your example, the +24V track going from C1 to IC1 completely cut he polygon. If you move down a little this track, the GND plane will be not cut any more...
That way, I check all the little improvement I can do, and some time it's not enough, so I reduce the isolation or the wire of the polygon.
I do that for all polygons, layer by layer (copper layers of course).
But any way good job !
Guillaume.
Guillaume barrey[1
wrote on Mon, 12 October 2015 05:20]Hi,
Yes you understand very well, all GND will be connected together. Here
we only speak about where physically it's better to do it. You can
do
it every where, it will work, but some location can reduce noise and
measurement error, and other will be introduce more noise.
Since your cell need no power, the best will be to use a *+twisted
pair
wire+* for each cell, and connect it directly to the board, so for
each
channel you need to add an extra connection for the GND of the cell.
For the acquisition device, it's dependent on if it have an extra pin
for GND or not.... If yes, you use a separate twisted pair wire
for
each channel and use this extra pin.
if not, then you can also use twisted pair wire but on the
acquisition device side you connect all the GND to the acquisition
device GND pin.
In both case on your amplifier board, you choose a 3 pins connector
for
each channel: input, GND and output. On the GND pin, you connect the
GND
wire from your cell and the GND wire from the acquisition device
together.
Guillaume
--
To view any images and attachments in this post, visit:
OK, cool thanks.
So version god knows what is attached 
(I must admit I think the traces on this version are a lot cleaner than
some of my previous ones)
With regard to twisted pair I guess I could use some CAT 5e Ethernet cable
I have lying around (somewhere).
Thanks once again!
-Jacob
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
| test6.zip |
Hi,
Yes you understand very well, all GND will be connected together. Here we only speak about where physically it's better to do it. You can do it every where, it will work, but some location can reduce noise and measurement error, and other will be introduce more noise.
Since your cell need no power, the best will be to use a twisted pair wire for each cell, and connect it directly to the board, so for each channel you need to add an extra connection for the GND of the cell.
For the acquisition device, it's dependent on if it have an extra pin for GND or not.... If yes, you use a separate twisted pair wire for each channel and use this extra pin.
if not, then you can also use twisted pair wire but on the acquisition device side you connect all the GND to the acquisition device GND pin.
In both case on your amplifier board, you choose a 3 pins connector for each channel: input, GND and output. On the GND pin, you connect the GND wire from your cell and the GND wire from the acquisition device together.
Guillaume
Guillaume barrey[1
wrote on Sun, 11 October 2015 08:04]Hi,
The sensor cell will produce a voltage, between the 2 signals :
- the signal you will connect to your amplifier input
- and the GND.
Only the voltage between these 2 signals (the difference) is
important.
The current that will flow out from your cell into the input of the
amplifier is exactly the same than the current flowing from the GND of
your board into the GND pin of your cell.
So, the role played by the 2 wires of the oxygen cell (signal and
GND)
is equivalent, and there is no reason to have a different path (except
if GND is also used to supply the sensor see (*) ).
On the amplifier side : it amplifies the difference between the
input
signal and the GND plane, the GND plane is a REFERENCE.
If instead of connecting directly the GND of sensor to your board, you
connect it to a point away from the plane (name it STAR point), with
all
the other sensor GND and supply GND, then you connect this start point
to your board with a single wire. On the paper this will work....
but....
In this last GND segment (wire from the GND plane and star point)
you
will have the sum of all the currents of all sensors, plus the current
drained by the amplifier it self (and this last one is far more
important than the others).
Where is the problem ?
The problem is that the copper is a good conductor, but not an ideal
one
!
You will have a little voltage difference between your GND plane and
the
start point, that will be dependent of that current, and the length of
the wire, and so amplifier REFERENCE will not be exactly the reference
of the sensor.
In other word, each signal will be polluted with the signal of the
other
cell and the consumption of the amplifier...
There is also other advantages of using same path for your sensor: you
can use twisted pair wire, that way you reduce noise, specially if
your
sensor are far away from the borad.
Just one thing (*) : I don't know your sensor: is this sensor need a
supply ? How this supply is wired? is the GND of sensor is only a
output
reference or also used for the return path of the supply ? because in
that case you have to figure how best can the GND be wired.... there
is
no magic solution, and we can help you unless you give us more info...
Sorry with this very quick fast ultra simplified explanation... and if
you want to have more fun... you can also question yourself about the
output of your amplifier : How the GND path mcan be optimised and
wired,
on the output side (I suppose you will connect it to an acquisition
device...)
Guillaume
--
To view any images and attachments in this post, visit:
Hi Guillaume
Thank you again for your reply.
Just to make sure I understand. I should still connect all the GND signals
together, just at different points on the GND plane?
The Sensor does not require any power, it generates it itself though a
chemical reaction (dependent on the oxygen fraction).
The amplified signal will be going to an acquisition device, should I also
wire their GND "away" from the power supply GND? I guess I could wire them
in the same terminal as the GND from each sensor?
Thanks
Jacob
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
Hi,
The sensor cell will produce a voltage, between the 2 signals :
- the signal you will connect to your amplifier input
- and the GND.
Only the voltage between these 2 signals (the difference) is important. The current that will flow out from your cell into the input of the amplifier is exactly the same than the current flowing from the GND of your board into the GND pin of your cell.
So, the role played by the 2 wires of the oxygen cell (signal and GND) is equivalent, and there is no reason to have a different path (except if GND is also used to supply the sensor see (*) ).
On the amplifier side : it amplifies the difference between the input signal and the GND plane, the GND plane is a REFERENCE.
If instead of connecting directly the GND of sensor to your board, you connect it to a point away from the plane (name it STAR point), with all the other sensor GND and supply GND, then you connect this start point to your board with a single wire. On the paper this will work.... but....
In this last GND segment (wire from the GND plane and star point) you will have the sum of all the currents of all sensors, plus the current drained by the amplifier it self (and this last one is far more important than the others).
Where is the problem ?
The problem is that the copper is a good conductor, but not an ideal one !
You will have a little voltage difference between your GND plane and the start point, that will be dependent of that current, and the length of the wire, and so amplifier REFERENCE will not be exactly the reference of the sensor.
In other word, each signal will be polluted with the signal of the other cell and the consumption of the amplifier...
There is also other advantages of using same path for your sensor: you can use twisted pair wire, that way you reduce noise, specially if your sensor are far away from the borad.
Just one thing (*) : I don't know your sensor: is this sensor need a supply ? How this supply is wired? is the GND of sensor is only a output reference or also used for the return path of the supply ? because in that case you have to figure how best can the GND be wired.... there is no magic solution, and we can help you unless you give us more info...
Sorry with this very quick fast ultra simplified explanation... and if you want to have more fun... you can also question yourself about the output of your amplifier : How the GND path mcan be optimised and wired, on the output side (I suppose you will connect it to an acquisition device...)
Guillaume
Guillaume barrey[1
wrote on Sat, 10 October 2015 05:53]Hi,
That last design is better, the ground plane is OK.. You remove the
big
capacitor (your 5µF) I suggested to check the value and the
package,
but not t remove it ? If it was one of my design I would put a 10µF
electrolytic capacitor between GND and +24V, just right after the
supply
connector...
Nice work ....
Ah ok hehe, I've added the 10uF capasitor now.
Quote:
I think there should be a ground connection for each channel. In other
words, you will need 3-pin instead of 2-pin connectors. Otherwise your
only ground connection is through the power supply connector. The ground
pin should be between each input and output pin.
I'm not sure I understand this bit.
The signal I'm trying to amplify is coming from small oxygen cells
(galvanic cells). If I understand what you are suggesting, is that I use
the GND from each cell to connect to their respective inverting input of
the opamp? My original idea was to tie all the GND lines from the cells
into the same GND connector (the one I also connect the power supply to).
Potentially a stupid question.. will that work? I don't need to ground
everything "together"?
Quote:
If you swap the ends of R5 and R6, then you can have a single trace for
OUT3, instead of 2 traces. You can do the same thing for the other
channels.
Once again thanks for all the help!!
-Jacob
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
| test5-3.zip |
Jacob Thastrup wrote on Fri, 09 October 2015 12:34
Once again thank you guys!!
Guillaume, thank you for the explanation it really helps!
I've added a ground plane to Joern's design... does that make sense?
I hope you can see the attached file..otherwise I'll go register at
eaglecentral as well.
-Jacob
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/162904
Attachments:
test5.zip
I think there should be a ground connection for each channel. In other
words, you will need 3-pin instead of 2-pin connectors. Otherwise your only
ground connection is through the power supply connector. The ground pin
should be between each input and output pin. I agree with others that you
should have a cap across the power supply terminals. Also, on your layout,
if you switch to a finer grid (i.e. 10 mil aka(0.01")), you can move some
traces slightly and improve the ground plane near the left end of the chip
(also changing the polygon width to 12 mils helps). If you swap the ends of
R5 and R6, then you can have a single trace for OUT3, instead of 2 traces.
You can do the same thing for the other channels.
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
Am 09.10.2015 um 18:34 schrieb Jacob Thastrup:
Once again thank you guys!!
Guillaume, thank you for the explanation it really helps!
I've added a ground plane to Joern's design... does that make sense?
I hope you can see the attached file..otherwise I'll go register at
eaglecentral as well.
-Jacob
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/162904
Attachments:
test5.zip
You should go there anyway. It is just the better link to the cadsoft
They don't have trouble with attachments (as you have seen).
BTW my "design" was just a suggestion.
Maybe you should add an electrolytic capacitor in general and foresee
some holes to screw this print somewhere.
--
Mit freundlichen Grüßen / With best regards
Joern Paschedag