Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Could someone check my design?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 191 subscribers
  • Views 2869 views
  • Users 0 members are here
Related

Could someone check my design?

jacob-t
jacob-t over 11 years ago

Hi Guys

I'm totally new to this. I'm trying to build a 4 channel opamp (boost my signal about 100x)

I'm hoping someone has the time to quickly check my design and see if it makes sense and perhaps let me know how to improve it.

 

Thanks

Jacob

Attachments:
opamp.zip
  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to jacob-t

    hi,

     

    I've viewed your layout and edit it.

     

    some tips for your next pcb

    * first of all: place parts, route power supply & gnd, critical tracks like bus and the all the other things

    * layout the pcb by following your nets of the schematics

    * try parts in different ways THT (horizontal / vertical) or SMD

    * route the tracks as short as possible

    * place holes to fix or parts to screw your pcb on something

     

    An example off your pcb with short tracks, etc. is attached. image

    Attachments:
    Test5_edit.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jacob-t
    jacob-t over 10 years ago in reply to kikoun

    Guillaume barrey[1

    wrote on Wed, 14 October 2015 13:10]Hi,

     

    That's Great !

    Just a last little advice for the GND plane.

    When my board is almost finish, I do some little adjustment to be sure

    that my GND plane will be good.... It's hard to explain with my poor

    English....(sorry to be a French frog:p)

    I hide all layer except the dimension, via, pads and the copper layer

    on

    which I work, and I run a ratsnest command to process the polygons

    Then you use the show command and select the polygon (in your case

    you

    only have GND). The polygon is highlighted so you can see it well.

    Now you try to imagine how the current can flow from here and there...

    Sometime you will see that for connecting to  point that are not

    really

    far from each other, the current need to do a huge travel because the

    plane is interrupted by some other tracks. Sometime it's easy to

    reduce

    drastically the effective distance just by moving a little bit a track

    or a part.

     

    In your example, the +24V track going from C1 to IC1 completely cut he

    polygon. If you move down a little this track, the GND plane will be

    not

    cut any more...

     

    That way, I check all the little improvement I can do, and some time

    it's not enough, so I reduce the isolation or the wire of the polygon.

     

    I do that for all polygons, layer by layer (copper layers of course).

     

    But any way good job !

     

    Guillaume.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/163345

     

     

    Hi Guys

    Sorry for the slow response.

    Thank you all for all the help. I feel I have learned a lot already!

    Best wishes

    Jacob

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kikoun
    kikoun over 11 years ago in reply to jacob-t

    Hi,

     

    That's Great !

    Just a last little advice for the GND plane.

    When my board is almost finish, I do some little adjustment to be sure that my GND plane will be good.... It's hard to explain with my poor English....(sorry to be a French frogimage)

    I hide all layer except the dimension, via, pads and the copper layer on which I work, and I run a ratsnest command to process the polygons

    Then you use the show command and select the polygon (in your case you only have GND). The polygon is highlighted so you can see it well.

    Now you try to imagine how the current can flow from here and there...

    Sometime you will see that for connecting to  point that are not really far from each other, the current need to do a huge travel because the plane is interrupted by some other tracks. Sometime it's easy to reduce drastically the effective distance just by moving a little bit a track or a part.

     

    In your example, the +24V track going from C1 to IC1 completely cut he polygon. If you move down a little this track, the GND plane will be not cut any more...

     

    That way, I check all the little improvement I can do, and some time it's not enough, so I reduce the isolation or the wire of the polygon.

     

    I do that for all polygons, layer by layer (copper layers of course).

     

    But any way good job !

     

    Guillaume.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jacob-t
    jacob-t over 11 years ago in reply to kikoun

    Guillaume barrey[1

    wrote on Mon, 12 October 2015 05:20]Hi,

    Yes you understand very well, all GND will be connected together. Here

    we only speak about where physically it's better to do it. You can 

    do

    it every where, it will work, but some location can reduce noise and

    measurement error, and other will be introduce more noise.

     

    Since your cell need no power, the best will be to use a *+twisted

    pair

    wire+* for each cell, and  connect it directly to the board, so for

    each

    channel you need to add an extra connection for the GND of the cell.

     

    For the acquisition device, it's dependent on if it have an extra pin

    for GND or not.... If yes, you use a separate twisted pair wire

    for

    each channel and use this extra pin.

    if not, then you can also use twisted pair wire but on the

    acquisition device side you connect all the GND to the acquisition

    device GND pin.

     

    In both case on your amplifier board, you choose a 3 pins connector

    for

    each channel: input, GND and output. On the GND pin, you connect the

    GND

    wire from your cell and the GND wire from the acquisition device

    together.

     

    Guillaume

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/163048

     

     

    OK, cool thanks.

     

    So version god knows what is attached image

     

    (I must admit I think the traces on this version are a lot cleaner than

    some of my previous ones)

     

    With regard to twisted pair I guess I could use some CAT 5e Ethernet cable

    I have lying around (somewhere).

     

    Thanks once again!

    -Jacob

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    Attachments:
    test6.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kikoun
    kikoun over 11 years ago in reply to jacob-t

    Hi,

    Yes you understand very well, all GND will be connected together. Here we only speak about where physically it's better to do it. You can  do it every where, it will work, but some location can reduce noise and measurement error, and other will be introduce more noise.

     

    Since your cell need no power, the best will be to use a twisted pair wire for each cell, and  connect it directly to the board, so for each channel you need to add an extra connection for the GND of the cell.

     

    For the acquisition device, it's dependent on if it have an extra pin for GND or not.... If yes, you use a separate twisted pair wire for each channel and use this extra pin.

    if not, then you can also use twisted pair wire but on the acquisition device side you connect all the GND to the acquisition device GND pin.

     

    In both case on your amplifier board, you choose a 3 pins connector for each channel: input, GND and output. On the GND pin, you connect the GND wire from your cell and the GND wire from the acquisition device together.

     

    Guillaume

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jacob-t
    jacob-t over 11 years ago in reply to kikoun

    Guillaume barrey[1

    wrote on Sun, 11 October 2015 08:04]Hi,

     

    The sensor cell will produce a voltage, between the 2 signals :

    - the signal you will connect to your amplifier input

    - and the GND.

    Only the voltage between these 2 signals (the difference) is

    important.

    The current that will flow out from your cell into the input of the

    amplifier is exactly the same than the current flowing from the GND of

    your board into the GND pin of your cell.

    So, the role played  by the 2 wires of the oxygen cell (signal and

    GND) 

    is equivalent, and there is no reason to have a different path (except

    if GND is also used to supply the sensor see (*) ).

     

    On the amplifier side : it amplifies the difference between the

    input

    signal and the GND plane, the GND plane is a REFERENCE.

     

    If instead of connecting directly the GND of sensor to your board, you

    connect it to a point away from the plane (name it STAR point), with

    all

    the other sensor GND and supply GND, then you connect this start point

    to your board with a single wire. On the paper this will work....

    but....

    In this last GND segment (wire from the GND plane and star point) 

    you

    will have the sum of all the currents of all sensors, plus the current

    drained by the amplifier it self (and this last one is far more

    important than the others).

    Where is the problem ?

    The problem is that the copper is a good conductor, but not an ideal

    one

    !

    You will have a little voltage difference between your GND plane and

    the

    start point, that will be dependent of that current, and the length of

    the wire, and so amplifier REFERENCE will not be exactly the reference

    of the sensor.

     

    In other word, each signal will be polluted with the signal of the

    other

    cell and the consumption of the amplifier...

     

    There is also other advantages of using same path for your sensor: you

    can use twisted pair wire, that way you reduce noise, specially if

    your

    sensor are far away from the borad.

     

    Just one thing (*) : I don't know your sensor: is this sensor need a

    supply ? How this supply is wired? is the GND of sensor is only a

    output

    reference or also used for the return path of the supply ? because in

    that case you have to figure how best can the GND be wired.... there

    is

    no magic solution, and we can help you unless you give us more info...

     

    Sorry with this very quick fast ultra simplified explanation... and if

    you want to have more fun... you can also question yourself about the

    output of your amplifier : How the GND path mcan be optimised and

    wired,

    on the output side (I suppose you will connect it to an acquisition

    device...)

     

    Guillaume

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/162998

     

     

    Hi Guillaume

    Thank you again for your reply.

    Just to make sure I understand. I should still connect all the GND signals

    together, just at different points on the GND plane?

     

    The Sensor does not require any power, it generates it itself though a

    chemical reaction (dependent on the oxygen fraction).

     

    The amplified signal will be going to an acquisition device, should I also

    wire their GND "away" from the power supply GND? I guess I could wire them

    in the same terminal as the GND from each sensor?

     

    Thanks

    Jacob

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kikoun
    kikoun over 11 years ago in reply to jacob-t

    Hi,

     

    The sensor cell will produce a voltage, between the 2 signals :

    - the signal you will connect to your amplifier input

    - and the GND.

    Only the voltage between these 2 signals (the difference) is important. The current that will flow out from your cell into the input of the amplifier is exactly the same than the current flowing from the GND of your board into the GND pin of your cell.

    So, the role played  by the 2 wires of the oxygen cell (signal and GND)  is equivalent, and there is no reason to have a different path (except if GND is also used to supply the sensor see (*) ).

     

    On the amplifier side : it amplifies the difference between the input signal and the GND plane, the GND plane is a REFERENCE.

     

    If instead of connecting directly the GND of sensor to your board, you connect it to a point away from the plane (name it STAR point), with all the other sensor GND and supply GND, then you connect this start point to your board with a single wire. On the paper this will work.... but....

    In this last GND segment (wire from the GND plane and star point)  you will have the sum of all the currents of all sensors, plus the current drained by the amplifier it self (and this last one is far more important than the others).

    Where is the problem ?

    The problem is that the copper is a good conductor, but not an ideal one !

    You will have a little voltage difference between your GND plane and the start point, that will be dependent of that current, and the length of the wire, and so amplifier REFERENCE will not be exactly the reference of the sensor.

     

    In other word, each signal will be polluted with the signal of the other cell and the consumption of the amplifier...

     

    There is also other advantages of using same path for your sensor: you can use twisted pair wire, that way you reduce noise, specially if your sensor are far away from the borad.

     

    Just one thing (*) : I don't know your sensor: is this sensor need a supply ? How this supply is wired? is the GND of sensor is only a output reference or also used for the return path of the supply ? because in that case you have to figure how best can the GND be wired.... there is no magic solution, and we can help you unless you give us more info...

     

    Sorry with this very quick fast ultra simplified explanation... and if you want to have more fun... you can also question yourself about the output of your amplifier : How the GND path mcan be optimised and wired, on the output side (I suppose you will connect it to an acquisition device...)

     

    Guillaume

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jacob-t
    jacob-t over 11 years ago in reply to kikoun

    Guillaume barrey[1

    wrote on Sat, 10 October 2015 05:53]Hi,

     

    That last design is better, the ground plane is OK.. You remove the

    big

    capacitor  (your 5µF) I suggested to check the value and the

    package,

    but not t remove it ? If it was one of my design I would  put a 10µF

    electrolytic capacitor between GND and +24V, just right after the

    supply

    connector...

     

    Nice work ....

     

    Ah ok hehe, I've added the 10uF capasitor now.

     

     

    Quote:

    I think there should be a ground connection for each channel. In other

    words, you will need 3-pin instead of 2-pin connectors. Otherwise your

    only ground connection is through the power supply connector. The ground

    pin should be between each input and output pin.

     

    I'm not sure I understand this bit.

    The signal I'm trying to amplify is coming from small oxygen cells

    (galvanic cells). If I understand what you are suggesting, is that I use

    the GND from each cell to connect to their respective inverting input of

    the opamp? My original idea was to tie all the GND lines from the cells

    into the same GND connector (the one I also connect the power supply to).

    Potentially a stupid question.. will that work? I don't need to ground

    everything "together"?

     

    Quote:

    If you swap the ends of R5 and R6, then you can have a single trace for

    OUT3, instead of 2 traces. You can do the same thing for the other

    channels.

     

     

    Cool, that does look better image

     

    Once again thanks for all the help!!

     

    -Jacob

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    Attachments:
    test5-3.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to jacob-t

    Jacob Thastrup wrote on Fri, 09 October 2015 12:34

    Once again thank you guys!!

    Guillaume, thank you for the explanation it really helps!

     

    I've added a ground plane to Joern's design... does that make sense?

     

    I hope you can see the attached file..otherwise I'll go register at

    eaglecentral as well.

    -Jacob

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/162904

     

    Attachments:

    test5.zip

     

     

    I think there should be a ground connection for each channel. In other

    words, you will need 3-pin instead of 2-pin connectors. Otherwise your only

    ground connection is through the power supply connector. The ground pin

    should be between each input and output pin. I agree with others that you

    should have a cap across the power supply terminals. Also, on your layout,

    if you switch to a finer grid (i.e. 10 mil aka(0.01")), you can move some

    traces slightly and improve the ground plane near the left end of the chip

    (also changing the polygon width to 12 mils helps). If you swap the ends of

    R5 and R6, then you can have a single trace for OUT3, instead of 2 traces.

    You can do the same thing for the other channels.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to jacob-t

    Am 09.10.2015 um 18:34 schrieb Jacob Thastrup:

    Once again thank you guys!!

    Guillaume, thank you for the explanation it really helps!

     

    I've added a ground plane to Joern's design... does that make sense?

     

    I hope you can see the attached file..otherwise I'll go register at

    eaglecentral as well.

    -Jacob

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/162904

     

    Attachments:

    test5.zip

     

    You should go there anyway. It is just the better link to the cadsoft

    newsgroups image

    They don't have trouble with attachments (as you have seen).

    BTW my "design" was just a suggestion.

    Maybe you should add an electrolytic capacitor in general and foresee

    some holes to screw this print somewhere.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>