EAGLE User Chat (English) Eagle v8 licensing...
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
  • Replies 415 replies
  • Subscribers 218 subscribers
  • Views 32102 views
  • Users 0 members are here
  • eagle
  • license
  • freeware
  • 8.0
Related

Eagle v8 licensing...

technolomaniac
technolomaniac over 9 years ago

Hi All --

 

Moving this to a separate thread so it doesn't get lost in the ether.  Here's my two cents on licensing and I'd love your feedback:

 

Firstly, the Autodesk licensing model is subscription and the EAGLE paid license will require that you install the SW and then generate an account to retrieve your license entitlement.  Once you have this, you are good to go and the SW will run as expected.  If you lose your network connection, the SW has a 14-day heartbeat that will enable you to work offline for 14 days.  I know that some folks would prefer to never have to connect, but this is required to support a monthly subscription model that can be selectively enabled and disabled when you use the SW (so you only pay when you use it).  The total cost of ownership for those folks using it less than a few weeks a year will thus be substantially lower and still enables you to access the full software for less money.  <Insert revolt here>  image

 

WRT to "what happens if autodesk decides to one day just shut off the license server?" ...ok, sure, that's possible, but so is a reality TV star becoming President of the..cough...nevermind, bad example.

 

Point is, that's a pretty remote possibility (think: time travel and alien invasions) and it wouldn't benefit us *at all* to upset the users we just spent real money hoping to bring into autodesk and earn their business.  As the guy with both development and P&L for the product, I can tell you that it's counterintuitive and wouldn't benefit us at all.  We know this.  We make SW used by governments, movie studios, game developers, MEs, Civil Engineers, machinists, etc. and you can bet that shutting down a license server is not to our benefit in any of these categories.  To demonstrate this behavior in one category, without a path for user SW and data, calls into question ALL of our tools' viability under this model.  Not helpful.

 

Now...a question was raised about "but what if I drop my subscription and I want my data".  Awesome, the data is yours and lives on your machine.  And for SW that stores data in the cloud (we have some of these) we always provide a path to your data.  If this again fails with one product, it puts all of the others up for discussion.  Again, not helpful.  (Read:  strategy = doomed).

 

"So what about needing an entitlement for the freeware to open the data I created in another version (a *paid* version) and reading it?  What if I want access and I dont want the 14-day time out?"

 

So here's the deal...We can do better here.  So we will.  Here's my commitment to the group here for freeware that ensures you always have a license that you can fall back on without need of internet connection *except when you first install it* (which after all, you would have had to get it in the first place):  in version 8.1 or 8.0.1 or whathaveyou (let's call it 'a future release'), if you install the SW and authenticate once, we'll remove the timer req.  So what I'm saying another way is, the freeware will require you to login the first time to get your license, but if you log out beyond that, you're good.  You got your entitlement and you can use it freely without connection.

 

Caveat:  to install an update, you will need to login.  The update server (which issues the new version...e.g. 8.1 or 8.2. or 8.0.1, etc.) requires that you login and get the update, but beyond that, logout.  Thus if you want to go off-grid in a mountain cabin somewhere, get your license at Starbucks (blagh! I understand they have 'free' wifi, but no frappucinos!  ...that stuff is bad for you) then get your license and go on your merry way up to the snow drenched peaks.  When you hear from the other mountaineers or your local yodeler that a new version of EAGLE is available...download, login, get your license, get your 'decaf double-pump vanilla non-fat latte macchiato' and head back up the slopes.

 

Point being, we can do the freeware better.  So we will.

 

Hope this is clear.  Let us know if you have questions!

 

Best regards,

 

Matt Berggren

Director - Autodesk

@technolomaniac

hackaday.io/matt

  • Sign in to reply
  • Cancel

Top Replies

  • COMPACT
    COMPACT over 8 years ago in reply to autodeskguest +4
    Not to worry, it's back to the Drawing board for me.
  • shabaz
    shabaz over 9 years ago +3
    Hi Matt, When will the EAGLE Maker version (or another solution for hobbiests) be v8-ready? I see the subscription for 'EAGLE Standard' and 'EAGLE Premium' are now available on the website, but not EAGLE…
  • albertovignati
    albertovignati over 8 years ago in reply to techsupport +3
    Il 21/02/2017 22:54, Ed Robledo ha scritto: The customers are the sole driving force to the improvements to EAGLE. Some of these 'wants' take time to be done right, that's the reason they were not done…
Parents
  • sauerwald
    sauerwald over 9 years ago

    Matt


    I purchased the full commercial licence for Eagle last month.  My understanding is that if I want to upgrade, I need to convert to the subscription model, and I have essentially lost the investment that I made in purchasing a license.

     

    Mark Sauerwald

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14candies
    e14candies over 9 years ago in reply to sauerwald

     

    from a few posts not too long ago....

     

    Autodesk acquires 'EAGLE': Official Q&A Discussion, New Website & What This

    Means!

    jwatson Employee Jul 20, 2016 10:57

    OFFICIAL NEWS from Matt Berggren, Director  Autodesk Circuits / Tinkercad /

    123D and now...EAGLE!

    Hello EAGLE users one and all!

     

    Will there still be a free version?

     

    Absolutely yes. We have no plans to eliminate the free tier at all.  This

    is central to EAGLE's success and aligns with how Autodesk does business

    today.  We'll continue this license to ensure everyone has access to

    powerful, easy to use schematic and PCB software.

     

     

    How does this affect upgrades?

     

    Upgrades work as they had in the past, for the most part.  If you want to

    upgrade from v6 Layout + Schematic to v7 Layout + Schematic, then you pay

    33% of the license price.  Simple.

     

    If you want to upgrade from v6 Layout + Schematic to v7 Layout + Schematic

    + Autorouter, then you first pay the upgrade cost of 33% to v7 Layout +

    Schematic and finally, you pay the difference in cost between the two v7

    license types.  Same as before.

     

    What's different?  For a limited time, we've reduced the price to upgrade

    legacy v5 licenses of EAGLE from 66% to 33% of the license price.  So if

    you've got a version 5 license, rather than paying 66% of the new license

    cost to upgrade, do it now for only 33%!

     

     

     

    Will I be required to pay 'maintenance'?

     

    Simply put, no.

     

     

     

    You should see some improvements in the pricing starting next week. The

    site has given some incorrect prices as of late so we should these

    issues addressed very soon.

     

    I'd say check the pricing next week, I think you'll be pleasantly

    surprised.

     

    Best Regards,

    Jorge Garcia

     

     

     

     

    --

    http://www.eaglecentral.ca :: The original and best browser access to CadSoft EAGLE support forums.  Supported by EAGLE licenses purchased through us :: http://www.eaglelicenses.com

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • reverant
    reverant over 9 years ago in reply to e14candies

    I was about to post the same thing.

     

    How does this affect upgrades?

    Upgrades work as they had in the past, for the most part.

     

    Will I be required to pay ‘maintenance’?

    Simply put, no.

     

    I feel really, really betrayed here. That was just 6 months ago.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • reverant
    reverant over 9 years ago in reply to e14candies

    I was about to post the same thing.

     

    How does this affect upgrades?

    Upgrades work as they had in the past, for the most part.

     

    Will I be required to pay ‘maintenance’?

    Simply put, no.

     

    I feel really, really betrayed here. That was just 6 months ago.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Joop14
    Joop14 over 9 years ago in reply to reverant

    Quote from reply #126: (technolomaniac aka Matt Berggren, the Director of

    Autodesk Circuits)

     

    Quote:

    ...it's not going subscription.

     

     

    http://www.eevblog.com/forum/eda/autodesk-buys-eagle/126/

     

    In six months, Autodesk can change completely their opinion. How reliable

    are they?

    What about all their statements here? What are they worth after six

    months?

     

     

    --

    http://www.eaglecentral.ca :: The original and best browser access to CadSoft EAGLE support forums.  Supported by EAGLE licenses purchased through us :: http://www.eaglelicenses.com