Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle- How do I put a hole in my PCB?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 191 subscribers
  • Views 10201 views
  • Users 0 members are here
Related

Eagle- How do I put a hole in my PCB?

stevemann
stevemann over 6 years ago

This is likely a silly question, but I am asking anyone with more Eagle PCB experience than I, which would be just about anyone, how do I put a hole for a 4-40 screw into my PCB?

I tried placing a hole using the command HOLE 0.125 *

But the PCB manufacturer bounced the order because the holes were only 0.003mm.

 

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    dukepro over 6 years ago

    On 1/10/20 01:10, Stephen Mann wrote:

    This is likely a silly question, but I am asking anyone with more Eagle PCB experience than I, which would be just about anyone, how do I put a hole for a 4-40 screw into my PCB?

    I tried placing a hole using the command HOLE 0.125 *

    But the PCB manufacturer bounced the order because the holes were only 0.003mm.

     

    You forgot the inches.  Your current grid is in mils (1/1000").  So when

    you asked for a 0.125 hole, it gave you one that's 0.125 mils in diameter.

     

       

    1. convert 0.125mil to mm.

        linux> units .125mil mm

               

    • 0.003175

                / 314.96063

     

     

     

    Try  HOLE 0.125" *+    You can use "in" for inches instead of the quote.

     

    Take a look at https://littlemachineshop.com/Reference/tapdrill.php.

    For a #4-40 screw, a close fit is 0.1160, a loose fit is 0.1285.  

    INCHES, of course.

     

    Joern,  The OP is referring to a standard screw size.  The "#4"

    represents the screw diameter, the "40" refers the number of threads per

    inch.  A #4-40 screw requires a 0.0820" (about 2mm) drill bit.

     

    HTH,

        - Chuck

     

    Attachments:
    46513.att1.html.zip
    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 6 years ago in reply to dukepro

    Am 13.01.2020 um 19:11 schrieb Chuck Huber:

    On 1/10/20 01:10, Stephen Mann wrote:

    This is likely a silly question, but I am asking anyone with more Eagle PCB experience than I, which would be just about anyone, how do I put a hole for a 4-40 screw into my PCB?

    I tried placing a hole using the command HOLE 0.125 *

    But the PCB manufacturer bounced the order because the holes were only 0.003mm.

     

    You forgot the inches.  Your current grid is in mils (1/1000").  So when

    you asked for a 0.125 hole, it gave you one that's 0.125 mils in diameter.

     

       

    1. convert 0.125mil to mm.

        linux> units .125mil mm

                

    • 0.003175

                 / 314.96063

     

     

     

    Try  HOLE 0.125" *+    You can use "in" for inches instead of the quote.

     

    Take a look at https://littlemachineshop.com/Reference/tapdrill.php.

    For a #4-40 screw, a close fit is 0.1160, a loose fit is 0.1285. INCHES,

    of course.

     

    Joern,  The OP is referring to a standard screw size.  The "#4"

    represents the screw diameter, the "40" refers the number of threads per

    inch.  A #4-40 screw requires a 0.0820" (about 2mm) drill bit.

     

    HTH,

        - Chuck

     

    Hi Chuck,

    IMHO the Standard is mm nowerdays. IC manufactories using it and even NASA.

    I could have checked or calculate it, but was 1. too lazy and 2. wanted

    to kick the OP to use precise information image

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 6 years ago in reply to autodeskguest

    On 1/14/20 04:34, Joern Paschedag wrote:

     

    Hi Chuck,

    IMHO the Standard is mm nowerdays. IC manufactories using it and even

    NASA.

    I could have checked or calculate it, but was 1. too lazy and 2.

    wanted to kick the OP to use precise information image

     

     

    Yeah... After I posted, by client updated the thread, which is when I

    found out that Rob had answered the question hours earlier.

     

    As far as standards go, it's good to hear that metric is fairly

    pervasive in Europe.  It should be world wide.

     

    Back in the late 70's, the US mounted a government mandated conversion. 

    Actually, I don't think "mandated" is the right word - it was more of a

    strong recommendation.  This effort is where we got the 2-liter Coke

    bottles and the 0.8-liter water bottles.  The drink industry adopted it

    well, but overall the effort failed miserably.  After that, the slow

    learners running our government figured out that this conversion was

    going to have to be done on a voluntary basis.

     

    Metric IC packages remained on imperial units until surface mount took

    off... mostly.  R's and C's are still referenced as 0603 or 0805 which

    reference mils.  I am glad to see that these jelly beans are also being

    referenced with their metric equivalents.  This divergence from metric

    probably stems from the fact that resistors as small as 0402 were

    available only to the military in the '50's.  At the time they were

    classified - I don't know when they were declassified.  The textual

    descriptions of R's and C's still contain the imperial sizes.  Eagle

    libraries (as late as v7 contain) contain imperial sizes for these

    components, further slowing the adoption of metric.

     

    I truly wish we would standardize on a single system of units on a

    world-wide basis.  There have been too many mishaps because of these

    differences.  I believe in NASA's case, it was the loss of the Mars

    Orbiter in 1999 wherein the engine manufacturer provided the thrust of

    the engine in pounds of thrust, when NASA used the same number as

    Newtons of thrust, that caused NASA to force all suppliers to publish

    specifications in SI units.  NASA started using SI units since at least

    1990, and 9 years later nobody bothered to verify the units.

     

    The culinary industry hasn't even thought about it.  Every recipe my

    wife has is measured in teaspoons, tablespoons, cups, pints, quarts,

    degrees Farenheit...

     

    Aviation: Altitude is still measured in feet (pretty much world wide)

    while temperature is measured in degrees Celsius.  The thrust of a jet

    engine is still measured in pounds instead of Newtons, and weight of an

    aircraft is measured in pounds instead of kg.  U.S. Government published

    charts show runway length in feet.  Charts published by a private

    company (Jeppesen/Boeing) have both feet and meters.

     

    But I digress.

     

    While I agree with you about what /should/ be done, I disagree with the

    extent of deployment, at least in the US.  Imperial units are still very

    pervasive in the consumer markets.  Sciences are being taught in SI

    units, so that will help the young understand just how long a meter is,

    and what a kg feels like when it's picked up.

     

    (BTW, I do have a 2 kg reference mass that I use for calibrating

    scales.  And yes, it does weigh less closer to the equator (N = mg -

    mv^2/r).  One must compensate for this based on latitude when calibrating.)

     

    It will be nice when we reach such a status...  One set of tools in the

    garage.

     

    Best regards,

        - Chuck

     

     

    Attachments:
    6403.att1.html.zip
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 6 years ago in reply to dukepro

    On 1/15/20 15:56, Chuck Huber wrote:

    True, at least to an American.  I immediately recognized that "4-40"

    was a SAE screw size.

     

    Not "SAE".  Freidrich pointed out correctly that it's "UNC".

     

    Enjoy,

        - Chuck

     

    Attachments:
    5102.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dukepro
    dukepro over 6 years ago in reply to dukepro

    On 1/15/20 15:56, Chuck Huber wrote:

    True, at least to an American.  I immediately recognized that "4-40"

    was a SAE screw size.

     

    Not "SAE".  Freidrich pointed out correctly that it's "UNC".

     

    Enjoy,

        - Chuck

     

    Attachments:
    5102.att1.html.zip