Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Serial Flash Memory - W25Q32FV HOW TO MAKE SMD!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 189 subscribers
  • Views 2314 views
  • Users 0 members are here
  • serial flash memory - w25q32fv
  • flash memory
  • scuplex
  • w25q32fv
Related

Serial Flash Memory - W25Q32FV HOW TO MAKE SMD!

scuplex
scuplex over 6 years ago

So i'm back for help cause im a starter!!!
I came a cross a problem where i cant make a part with SMD

i want to exactly make a

Serial Flash Memory - W25Q32FV
but in the datesheet it doesnt show to exact lenght and height for the SMD !

How can i came a library for this flash memory and if cant is there something else to use like this one?

Thanks a lot !!!





  • Sign in to reply
  • Cancel
Parents
  • dukepro
    dukepro over 6 years ago

    George,

     

    I'm looking at the datasheet for this.  The length and height are

    published for several packages.  Look in section 10 titled "Package

    Specifications".  Look at dimensions D1 and E1.  You can grab a copy of

    the datasheet at:

       

    https://www.mouser.com/datasheet/2/813/w25q32fv_revj_06032016-1669822.pdf

     

    Which package is of interest?  There is likely a matching package in

    smd-ipc.lbr.  Copy this to your library with:

     

        copy SOP08.pac@smd-ipc.lbr

     

    Verify the all properties of everything.  Many times you can start with

    something from the library, and tweak it for a specific purpose.  If you

    choose this tweaking route, be sure to rename the package accordingly.

     

    HTH,

        - Chuck

     

     

     

    On 3/6/20 10:31, george karatzas wrote:

    So i'm back for help cause im a starter!!!

    I came a cross a problem where i cant make a part with SMD

     

    i want to exactly make a

    h1. Serial Flash Memory - W25Q32FV

    but in the datesheet it doesnt show to exact lenght and height for the SMD !

    How can i came a library for this flash memory and if cant is there something else to use like this one?

     

    Thanks a lot !!!

     

     

     

     

     

     

     

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/289256

     

     

    Attachments:
    3660.att1.html.zip
    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • scuplex
    scuplex over 6 years ago in reply to dukepro

    Sorry if im being annoying but i was wondering how can i connect those CS ports to the teensy board!






    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • scuplex
    scuplex over 6 years ago in reply to dukepro

    Sorry if im being annoying but i was wondering how can i connect those CS ports to the teensy board!






    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dukepro
    dukepro over 6 years ago in reply to scuplex

    On 3/6/20 14:34, george karatzas wrote:

    Sorry if im being annoying but i was wondering how can i connect those CS ports to the teensy board!

     

    First of all, the CS lines are usually active low.  I see the signals

    SD-CS and FLASH-CS, neither have a bar over them indicating an active

    high status.  Double check the datasheet.  My bet is that they should be

    active low.  To get the bar over the signal name, change the NAME of the

    nets to include a leading bang: "!SD-CS", and "!FLASH-CS".

     

    As far as connecting them, they're usually connected to a GPIO on the

    microcontroller (uC).  You have at least two devices on the SPI bus, and

    therefore you MUST control the chip selects manually in code.

     

    Additionally, you'll need to add external pull-up resistors on them -

    anywhere from 47k to 100k should be fine.  A 1/16W resistor should work

    (0402).  The reason for the pull-up is during power-up and power-down. 

    The 5V line will ramp up slowly.  Until the uC comes out of

    brown-out-reset (BOR) and the code initializes the specific GPIOs to be

    driven, the GPIO's usually default to high-Z.  But during this process,

    the SPI slave could very easily come out of reset first.  i.e. The +5V

    line reaches the minimum VCC on the slave before it reaches the BOR

    voltage of the uC.  If both slaves come up, the CS lines could very

    easily be below the Vlow and as such would be interpreted as active.  If

    both slaves are active, then both MISO ports are driving the MISO line. 

    This is a ripe condition for one slave to drive it high while the other

    slave drives it low.

     

    This bus contention is solved by adding the pull-up resistors to the CS

    lines.  This assures that the CS is at the same voltage as the +5V line,

    and can not be interpreted as a logic low.  No bus contention.  No blown

    SDO ports.

     

    Another point to consider, is the voltage on which the GPIOs are

    operating.  I see two power supplies going into the uC - 5V and 3.3V. 

    If the GPIOs are operating at 3.3V, it may not be a good thing to drive

    them with a slave that's operating at 5V.  The GPIOs need to be 5V

    tolerant.  Consider the case when the uC is driving the CS, SCK, and

    MOSI.  The minimum Vout-hi on the uC might not be high enough to reach

    the minimum Vin-high (logic high level) on the slaves.  The GPIOs will

    emit about 3.2V.  The slaves may need VDD-1.0.

     

    On chips that can host different voltages usually have a separate VDDIO

    power pin.  I don't see that on the excerpt image.

     

    As for hand soldering super small pads, the first thing I start with is

    a super-fine soldering iron tip.  They don't exist in any store,

    though.  You have to make one.  Start with a fine tip and put it in the

    end of a drill.  Using a belt sander with a fine grit, I sand the tip to

    a needle point while turning it with the drill.  The down side is that

    this removes the nickel plating on the tip, and the underlying copper

    will erode faster.  As the copper erodes over time, I repeat the

    process, squeezing as much time out of a $2 soldering iron tip as I can.

     

    Another trick I've done in the past is I'll make a special package in

    Eagle that has all the same dimensions except that the SMD pads extend

    out away from the center of the chip longer than standard.  This allows

    easier access when using the aforementioned custom needle-point

    soldering iron tip.  This is a temporary fix and should be used only

    when hand soldering.  For production, I switch back to the package with

    the spec SMD pads.

     

    Yet another trick:  When soldering pins to pads that are 0.5mm spacing,

    it's easier to just flood the entire side with solder, bridging all the

    pins together.  Come back with some solder wick and wick away the excess

    solder.  Reflow each pin to get a good bond and verify that there are no

    bridges.  A bit of Chemtronics Flux-off will wash the excess resin away.

     

    Use a microscope.  Look at amscope.com -

    https://www.amscope.com/applications/electronics/circuit-boards-general-electronics.html 

    Don't be cheap.  Get one with an arm, preferably two arms.  Use a

    C-clamp to clamp it to your desk.

     

    HTH

        - Chuck

     

     

     

    Attachments:
    3225.att1.html.zip