Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Selecting inches/mm with the RS_274x CAM processor
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 189 subscribers
  • Views 2662 views
  • Users 0 members are here
Related

Selecting inches/mm with the RS_274x CAM processor

e14 Contributor
e14 Contributor over 16 years ago

Is there any way to output Gerbers files with the RS_274X CAM processor

in anything other than inches?  I'm capturing in mm, so I would think

that the Gerber files would be output in mm, but looking at the files I

can see that I am getting inches instead.  I don't see any place in the

CAM processor dialog to select unit systems.

 

Truly, what I'd really like is a Gerber output in microns (um), but I'll

take mm.  Inches are a problem.

 

Thanks,

 

Michael

 

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 16 years ago

    Michael Sansom schrieb:

    Is there any way to output Gerbers files with the RS_274X CAM processor

    in anything other than inches?  I'm capturing in mm, so I would think

    that the Gerber files would be output in mm, but looking at the files I

    can see that I am getting inches instead.  I don't see any place in the

    CAM processor dialog to select unit systems.

     

    Truly, what I'd really like is a Gerber output in microns (um), but I'll

    take mm.  Inches are a problem.

     

    Thanks,

     

    Michael

     

     

    Michael,

     

     

    the default output of Gerber data is in inches. If you prefer to have

    "mm" you could change the Gerber device in the eagle.def file or even

    better define a new device. That's the place we define the output

    devices. It's located in the eagle/bin folder.

     

    Examples for Gerber output in mm 3.3 format:

     

     

    Type     = PhotoPlotter

    Long     = "Gerber photoplotter"

    Init     = "G01\nX000000Y000000D02\n"

    Reset    = "X000000Y000000D02\nM02\n"

    ResX     = 25400

    ResY     = 25400

    ;Wheel    = ""

    Move     = "X%0.6dY%0.6dD02*\n"    ; (x, y)

    Draw     = "X%0.6dY%0.6dD01*\n"    ; (x, y)

    Flash    = "X%0.6dY%0.6dD03*\n"    ; (x, y)

    Aperture = "%s*\n"               ; (Aperture code)

    Units    = mm

    Decimals = 4

    Info     = "Plotfile Info:\n"\

               "\n"\

               " Coordinate Format : 3.3\n"\

               " Coordinate Units  : mm\n"\

               " Data Mode         : Absolute\n"\

               " Zero Suppression  : None\n"\

               " End Of Block      : *\n"\

               "\n"

     

     

    @GERBER_MM_33

    Long          = "Gerber photoplotter with automatic aperture wheel

    generation"

    Wheel         = "" ; avoids message!

    AutoAperture  = "D%d" ; (Aperture number)

    FirstAperture = 10

    Decimals      = 4

    Units         = mm

     

     

     

     

    @GERBERAUTO_MM_33

    Long          = "Gerber photoplotter with RS-274-X aperture generation"

    Units         = mm

    Init          = "G75*\n"           \ allow positive and negative coordinates

                    "G71*\n"           \ units are mm

                    "%%OFA0B0*%%\n"    \ horizonal and vertical OFfset is 0

                    "%%FSLAX33Y33*%%\n"\ Format Statement is Absolute (I for

    incremental) 3.3

                    "%%IPPOS*%%\n"     \ Image Polarity is POSitive (NEG for

    nagative)

                    "%%LPD*%%\n"       \ Layer Polarity Dark (C for clear on

    negative planes)

                    "%%AMOC8\n5,1,8,0,0,1.08239X$1,22.5\n"\ Octagons are

    emulated with a circle (using 8 vertices)

                    "%%\n"            ; and therefore the diameter must be

    enlarged with '1 / cos(pi / 8)'

    Reset         = "M02*\n"

    Circle        = "%%AD%sC,%6.3f*%%\n"        ; (code, diameter)

    Rectangle     = "%%AD%sR,%6.3fX%6.3f*%%\n"  ; (code, dx, dy)

    Oval          = "%%AD%sO,%6.3fX%6.3f*%%\n"  ; (code, dx, dy)

    ; According to the RS-274-X specs there is an aperture macro

    ; primitive that allows us to specify an octagon (i.e. a polygon with

    ; 8 vertices). As some Gerber viewers seem to have problems with that,

    ; we would have to use a round shape for that.

    ; If your Gerber processor cannot handle the polygon primitive you may

    ; uncomment the following line and comment out the line after it:

    ;Octagon       = "%%AD%sC,%6.3f*%%\n"   ; (code, diameter) (looks like

    there is no octagon, so we take a circle)

    Octagon       = "%%AD%sOC8,%6.3f*%%\n" ; (code, diameter)

    Annulus       = "%%AMAN%s\n1,1,%6.3f,0,0\n1,0,%6.3f,0,0*\n"\

                    "%%\n"\

                    "%%AD%sAN%s*%%\n" ; (code, diameter, inner diameter,

    code, code)

    Thermal       = "%%AMTH%sX\n1,1,%6.3f,0,0\n1,0,%6.3f,0,0*\n"\

                    "21,0,%6.3f,%6.3f,0,0,45\n21,0,%6.3f,%6.3f,0,0,135\n"\

                    "%%\n"\

                    "%%AD%sTH%sX*%%\n"; (code, diameter, inner diameter,

    diameter + 2mil, gap, diameter + 2mil, gap, code, code)

     

     

     

    HTH

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bbartley
    bbartley over 10 years ago in reply to Richard_H

    Hi,

    This worked just fine for me. (More specifically, this version: http://www.eaglecentral.ca/forums/index.php/mv/msg/34173/117557/ did.)

     

    Is there some reason this isn't in the normal EAGLE distribution? While inches seems to be the most common, I've dealt with a couple of shops that prefer mm.

     

    Thanks!

    Brad

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to bbartley

     

     

    Is there some reason this isn't in the normal EAGLE distribution? While

    inches seems to be the most common, I've dealt with a couple of shops

    that prefer mm.

     

    Hi Brad,

     

    This is part of the normal EAGLE distribution, at least now anyway ;).

    You'll find the drivers listed for EXCELLON_33MM and GERBER_RS274X_33MM.

     

    This was added recently with the release of 7.3 if memory serves.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 10 years ago in reply to bbartley

     

     

    Is there some reason this isn't in the normal EAGLE distribution? While

    inches seems to be the most common, I've dealt with a couple of shops

    that prefer mm.

     

    Hi Brad,

     

    This is part of the normal EAGLE distribution, at least now anyway ;).

    You'll find the drivers listed for EXCELLON_33MM and GERBER_RS274X_33MM.

     

    This was added recently with the release of 7.3 if memory serves.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia