EAGLE User Support (English) Can a generic symbol (sup) be created?
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
  • Replies 14 replies
  • Subscribers 180 subscribers
  • Views 2384 views
  • Users 0 members are here
Related

Can a generic symbol (sup) be created?

alank2
alank2 over 15 years ago

Hi,

 

I noticed in the supply libraries that there is a symbol for each type, 5v, 3.3v, etc.  It looks like the SUP type is what makes this work.  I tried to create a symbol with this type with the idea that I could use it for many nets.  For example, add it.  Use the name to assign a name.  Then add another.  Assign the same name.  Items with the same name would be linked.  I have discovered that that links them is the PIN name in the symbol itself, which there is no way to change when adding to a schematic.  Must you create a seperate symbol for each symbol type?

 

Thanks,

 

Alan

  • Sign in to reply
  • Cancel
Parents
  • alank2
    alank2 over 15 years ago

    Hi,

     

    I guess part two of this question is how do you connect nets between multiple schematic sheets.

     

    If you run a net and give them both the same name, the ERC says "Segment of net X has no visual connection.  Surely there must be a right way to do this between multiple sheets.

     

    Thanks,

     

    Alan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to alank2

    On Thu, 2 Sep 2010, alank2 wrote to us saying :

    >If you run a net and give them both the same name, the ERC says

    >"Segment of net X has no visual connection.  Surely there must be a

    >right way to do this between multiple sheets.

     

    Is that just a net from nowhere to nowhere? Because the way to connect

    nets between sheets is simply to give them the same name. As long as the

    net connects to at least one pin of at least one part on each sheet it

    appears on, then you shouldn't get that error. And if it doesn't then

    why is it even on that sheet?

    --

    Rob Pearce                       http://www.bdt-home.demon.co.uk

     

    The contents of     | If you believe Satan is found in pop can I

    this message are    | suggest you stop drinking it.

    purely my opinion.  |    - Dave Hyden, uk.r.c,

    Don't believe a     |    re: "Stairway to Heaven"

    word.               |

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 15 years ago in reply to alank2

    On Thu, 2 Sep 2010, alank2 wrote to us saying :

    >If you run a net and give them both the same name, the ERC says

    >"Segment of net X has no visual connection.  Surely there must be a

    >right way to do this between multiple sheets.

     

    Is that just a net from nowhere to nowhere? Because the way to connect

    nets between sheets is simply to give them the same name. As long as the

    net connects to at least one pin of at least one part on each sheet it

    appears on, then you shouldn't get that error. And if it doesn't then

    why is it even on that sheet?

    --

    Rob Pearce                       http://www.bdt-home.demon.co.uk

     

    The contents of     | If you believe Satan is found in pop can I

    this message are    | suggest you stop drinking it.

    purely my opinion.  |    - Dave Hyden, uk.r.c,

    Don't believe a     |    re: "Stairway to Heaven"

    word.               |