EAGLE User Support (English) Can a generic symbol (sup) be created?
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
  • Replies 14 replies
  • Subscribers 180 subscribers
  • Views 2387 views
  • Users 0 members are here
Related

Can a generic symbol (sup) be created?

alank2
alank2 over 15 years ago

Hi,

 

I noticed in the supply libraries that there is a symbol for each type, 5v, 3.3v, etc.  It looks like the SUP type is what makes this work.  I tried to create a symbol with this type with the idea that I could use it for many nets.  For example, add it.  Use the name to assign a name.  Then add another.  Assign the same name.  Items with the same name would be linked.  I have discovered that that links them is the PIN name in the symbol itself, which there is no way to change when adding to a schematic.  Must you create a seperate symbol for each symbol type?

 

Thanks,

 

Alan

  • Sign in to reply
  • Cancel
  • alank2
    alank2 over 15 years ago

    Hi,

     

    I guess part two of this question is how do you connect nets between multiple schematic sheets.

     

    If you run a net and give them both the same name, the ERC says "Segment of net X has no visual connection.  Surely there must be a right way to do this between multiple sheets.

     

    Thanks,

     

    Alan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to alank2

    On Thu, 2 Sep 2010, alank2 wrote to us saying :

    >If you run a net and give them both the same name, the ERC says

    >"Segment of net X has no visual connection.  Surely there must be a

    >right way to do this between multiple sheets.

     

    Is that just a net from nowhere to nowhere? Because the way to connect

    nets between sheets is simply to give them the same name. As long as the

    net connects to at least one pin of at least one part on each sheet it

    appears on, then you shouldn't get that error. And if it doesn't then

    why is it even on that sheet?

    --

    Rob Pearce                       http://www.bdt-home.demon.co.uk

     

    The contents of     | If you believe Satan is found in pop can I

    this message are    | suggest you stop drinking it.

    purely my opinion.  |    - Dave Hyden, uk.r.c,

    Don't believe a     |    re: "Stairway to Heaven"

    word.               |

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • alank2
    alank2 over 15 years ago

    Hi,

     

    If I put a single part on each sheet and then add a net to one pin on each part and then use the name to join the two nets together, the warning still comes up.  Do you put something at the end of the net when using multiple sheets and a net goes only from one pin on one sheet to one pin on another?

     

    The way Eagle handles these "unwired" but connected nets seems so much harder than it needs to be.  I don't know why they don't just have a single pin symbol you add and then tell it which net it goes to...

     

    Thanks,

     

    Alan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to alank2

    alank2 wrote:

    >If I put a single part on each sheet and then add a net to one pin on each part and then use the name

    to join the two nets together, the warning still comes up.  Do you put something at the end of the net

    when using multiple sheets and a net goes only from one pin on one sheet to one pin on another?

     

    help label

     

    >The way Eagle handles these "unwired" but connected nets seems so much harder than it needs to be.

    I don't know why they don't just have a single pin symbol you add and then tell it which net it goes to...

     

    I rather like this warning. It reminds me to put labels on nets that

    are present on more than one sheet.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to alank2

     

    "alank2" <communitymanager@premierfarnell.com> wrote in message

    news:245768910.5331283470906554.JavaMail.jive@flcspu-csapp-01.premierfarnell.com...

    Hi,

    >

    If I put a single part on each sheet and then add a net to one pin on each

    part and then use the name to join the two nets together, the warning

    still comes up. Do you put something at the end of the net when using

    multiple sheets and a net goes only from one pin on one sheet to one pin

    on another?

    >

    The way Eagle handles these "unwired" but connected nets seems so much

    harder than it needs to be. I don't know why they don't just have a single

    pin symbol you add and then tell it which net it goes to...

    >

    Thanks,

    >

    Alan

    >

     

    why do you think "xref" was invented?

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • alank2
    alank2 over 15 years ago in reply to Former Member

    Hi,

     

    Thanks guys, the label and xref were exactly what I needed to figure out how to use.  I just didn't know how they worked.

     

    Alan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • alank2
    alank2 over 15 years ago in reply to alank2

    Hi,

     

    So, what is the difference between using something like a supply +5V from the library vs. just drawing a net and naming it +5V and giving it an xref ?

     

    Thanks,

     

    Alan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to alank2

    >

    So, what is the difference between using something like a supply +5V from

    the library vs. just drawing a net and naming it +5V and giving it an xref

    ?

    >

    Thanks,

    >

     

    You can't give supply nets arbitrary names with supply symbols as

    implemented as a library component without overwriting the resulting power

    net name. When you drop a power symbol on a sheet and connect it to a net,

    it uses the name assigned to the SYMBOL PIN in the library SYMBOL (not the

    device name) as the new power net name to assign in the schematic.

     

    I can't tell you how many drawings folks have sent me with screwed up power

    symbols, nets, etc due to this. For instance, if you overwrite a supply

    symbol net name and then use the COPYcommand to duplicate that power symbol

    and connect it to a new net, the new net will have the original name that

    was assigned to the pin in the SYMBOL rather than the net it was currently

    assigned to. I see lots of drawings where beginners do this and have power

    nets all goofed up and/or not connected properly. I've seen lots of

    improperly created power symbols with the pin name different from the

    symbol/device name which can really cause havoc in a drawing with power nets

    all tied incorrectly to each other.

     

    In other systems, like Altium, the power symbol is a native object in the

    schematic and you can give it any arbitrary name you like when you add a

    power symbol. Your limited to a few power symbol types (like a t-bar, circle

    or arrow), but I like this for consistency reasons. If you duplicate the

    symbol and connect it to another net, then  it uses the arbitrary name

    assigned to that symbol instance (rather than using the original name from a

    lib object). None of this business of  "the power symbol net name was

    overwritten" warnings or confusion exists.

     

    It wouldn't be that big of a deal to add a native power symbol object in the

    schematic editor. But, converting all the old drawings that use the lib

    power symbols would be a little bit of a conversion headache.  I'd be

    perfectly happy to see these gone forever though! My only fear is that we'd

    end up with limited set of supply and gnd symbols that look bizzare (ala

    CADSoft) and can never be changed!

     

    Bob

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    On 9/3/2010 6:18 PM, Bob Starr wrote:

    >>

    >> So, what is the difference between using something like a supply +5V from

    >> the library vs. just drawing a net and naming it +5V and giving it an xref

    >> ?

    >>

    >> Thanks,

    >>

    >

    You can't give supply nets arbitrary names with supply symbols as

    implemented as a library component without overwriting the resulting power

    net name. When you drop a power symbol on a sheet and connect it to a net,

    it uses the name assigned to the SYMBOL PIN in the library SYMBOL (not the

    device name) as the new power net name to assign in the schematic.

    >

    I can't tell you how many drawings folks have sent me with screwed up power

    symbols, nets, etc due to this. For instance, if you overwrite a supply

    symbol net name and then use the COPYcommand to duplicate that power symbol

    and connect it to a new net, the new net will have the original name that

    was assigned to the pin in the SYMBOL rather than the net it was currently

    assigned to. I see lots of drawings where beginners do this and have power

    nets all goofed up and/or not connected properly. I've seen lots of

    improperly created power symbols with the pin name different from the

    symbol/device name which can really cause havoc in a drawing with power nets

    all tied incorrectly to each other.

    >

    In other systems, like Altium, the power symbol is a native object in the

    schematic and you can give it any arbitrary name you like when you add a

    power symbol. Your limited to a few power symbol types (like a t-bar, circle

    or arrow), but I like this for consistency reasons. If you duplicate the

    symbol and connect it to another net, then  it uses the arbitrary name

    assigned to that symbol instance (rather than using the original name from a

    lib object). None of this business of  "the power symbol net name was

    overwritten" warnings or confusion exists.

    >

    It wouldn't be that big of a deal to add a native power symbol object in the

    schematic editor. But, converting all the old drawings that use the lib

    power symbols would be a little bit of a conversion headache.  I'd be

    perfectly happy to see these gone forever though! My only fear is that we'd

    end up with limited set of supply and gnd symbols that look bizzare (ala

    CADSoft) and can never be changed!

    >

    Bob

    >

    >

    I also dislike the "predefined net" behavior of the power symbols.

     

    I have considered making some "dummy" power symbols that act like the

    "named ports" in the dports library and just using EAGLE's normal net

    naming/connecting facility. But it would be nice if it automagically

    popped up the name of the net without having to name it and label it,

    and then could be COPYed to spread it around the schematic. As you said,

    it would be good if this ability were built in and we could draw

    whatever symbol we liked. Maybe a pin visibility called "Net Name" that

    caused the displayed pin label to inherit the net name it's connected to

    or something like that. who knows. maybe someone has a better idea...

    maybe a ULP could encapsulate all these functions and add a new class of

    power symbols like in Altium.

     

    If something like this could be made, I would just leave the other

    system intact for those who still want to use it or for compatibility,

    no need to convert headache.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • alank2
    alank2 over 15 years ago in reply to Former Member

    Hi,

     

    While the xrefs do work, I think they look terrible on the schematic.  It may seem like a lot of work, but I'm just going to create a library item for each type that I want.  It is the difference between this:

     

    [img]http://home.earthlink.net/~alank2/avr/nettype.gif[/img]

    http://home.earthlink.net/~alank2/avr/nettype.gif

     

    PD6 is an xref

    and

    PD5 is a library component using the SUP type named PD5.

     

    Is there a way to adjust the xref size?  If I could make it smaller I'd probably just use xref's.

     

    Thanks,

     

    Alan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>