EAGLE User Support (English) Board DRC - Supposed to Generate Errors/Warnings on Unrouted Nets?
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
  • Replies 18 replies
  • Subscribers 179 subscribers
  • Views 2594 views
  • Users 0 members are here
Related

Board DRC - Supposed to Generate Errors/Warnings on Unrouted Nets?

Former Member
Former Member over 15 years ago

I just noticed that I have two unrouted nets on my board layout (i.e.

the ratsnets lines are visible but no copper tracks connect) and the DRC

isn't generating any errors/warning.  Is this correct?  What am I doing

wrong, I've never seen a DRC that wouldn't flag unrouted signals.

 

Michael

 

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 15 years ago +1
    Michael Sansom wrote: I just noticed that I have two unrouted nets on my board layout (i.e. the ratsnets lines are visible but no copper tracks connect) and the DRC isn't generating any errors/warning…
Parents
  • Former Member
    Former Member over 15 years ago

    Michael Sansom wrote:

    I just noticed that I have two unrouted nets on my board layout (i.e.

    the ratsnets lines are visible but no copper tracks connect) and the DRC

    isn't generating any errors/warning.  Is this correct?  What am I doing

    wrong, I've never seen a DRC that wouldn't flag unrouted signals.

     

    Michael

     

    Ok, I see the RATSNEST command (or button) will tell me how many

    unrouted airwires exist (I've never seen another package that didn't do

    this in the DRC check), but how do I find these unrouted airwires?  They

    are not apparent (if they were, they'd be routed).  Is there no way to

    jump to each unrouted airwire in the same way you can click on an DRC

    error have have the tool show you where the problem is?

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 15 years ago

    Michael Sansom wrote:

    I just noticed that I have two unrouted nets on my board layout (i.e.

    the ratsnets lines are visible but no copper tracks connect) and the DRC

    isn't generating any errors/warning.  Is this correct?  What am I doing

    wrong, I've never seen a DRC that wouldn't flag unrouted signals.

     

    Michael

     

    Ok, I see the RATSNEST command (or button) will tell me how many

    unrouted airwires exist (I've never seen another package that didn't do

    this in the DRC check), but how do I find these unrouted airwires?  They

    are not apparent (if they were, they'd be routed).  Is there no way to

    jump to each unrouted airwire in the same way you can click on an DRC

    error have have the tool show you where the problem is?

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    Michael Sansom wrote:

    Michael Sansom wrote:

    >> I just noticed that I have two unrouted nets on my board layout (i.e.

    >> the ratsnets lines are visible but no copper tracks connect) and the

    >> DRC isn't generating any errors/warning.  Is this correct?  What am I

    >> doing wrong, I've never seen a DRC that wouldn't flag unrouted signals.

    >>

    >> Michael

     

    Ok, I see the RATSNEST command (or button) will tell me how many

    unrouted airwires exist (I've never seen another package that didn't do

    this in the DRC check), but how do I find these unrouted airwires?  They

    are not apparent (if they were, they'd be routed).  Is there no way to

    jump to each unrouted airwire in the same way you can click on an DRC

    error have have the tool show you where the problem is?

     

     

    Ok, I'm sure everyone seen this before.  Turned out that I had these

    tiny airwires where a SMT pad ended up landing off grid.  In actuality,

    everything was in fact connected by copper.  Other layout systems seem

    to have an algorithm where when you connect a track to a pad it will

    force the connection if the center of the pad is slightly off grid

    within some tolerance.

     

    Be that as it may, the only way I was able to find these very small

    airwires was to turn off all layers except the Unrouted layer AND turn

    off the grid because these small airwires were being obscured by the

    grid dots.  A very frustrating experience.  Perhaps there is a better

    way and I just haven't found it.

     

    In any case, if you are not going to force connections on these slight

    off grid pads, at LEAST you ought to make it easy to find these small

    airwires (perhaps there is an easy way to find these and I just don't

    know it yet).  If there isn't a better means to detect the location of

    these airwires, let me suggest that a command/button that puts a big

    yellow "X" at each end of the air wire would essentially fix this issue.

     

    My original error was in not understanding that the DRC check did not

    catch unrouted connections.  Fortunately, none of these airwires were real.

     

     

    Michael

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

     

    Michael Sansom wrote:

    I just noticed that I have two unrouted nets on my board layout (i.e.

    the ratsnets lines are visible but no copper tracks connect) and the DRC

    isn't generating any errors/warning.  Is this correct?

     

    ..................how do I find these unrouted airwires?  They

    are not apparent (if they were, they'd be routed).  Is there no way to

    jump to each unrouted airwire in the same way you can click on an DRC

    error have have the tool show you where the problem is?

    >

     

    Try these ULPs. There are others that produce text and script files but

    these enable you to locate the airwires quickly

    Once you choose your favourite ULP, add it to a Command Text menu button to

    your Board editor so you can check for airwires with a single click of the

    mouse.

     

    zoom-unrouted.ulp

    • simple script to zoom to the first unrouted wire in board editor.

     

    • this might be helpful when searching for tiny left-overs.

     

    statistic-brd.ulp

    *Unrouted count is in red in the summary section on the BOARD tab.

     

    length.ulp

    *This ULP calculates the signal length of routed tracks in the layout

    • airwires will be shown separately. Easily spotted in their own column

     

    Warren

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    Warren Brayshaw wrote:

     

    Try these ULPs. There are others that produce text and script files but

    these enable you to locate the airwires quickly

    Once you choose your favourite ULP, add it to a Command Text menu button to

    your Board editor so you can check for airwires with a single click of the

    mouse.

     

    zoom-unrouted.ulp

    • simple script to zoom to the first unrouted wire in board editor.

     

    • this might be helpful when searching for tiny left-overs.

     

    statistic-brd.ulp

    *Unrouted count is in red in the summary section on the BOARD tab.

     

    length.ulp

    *This ULP calculates the signal length of routed tracks in the layout

    • airwires will be shown separately. Easily spotted in their own column

     

    Warren

     

     

    Thanks Warren, these will be most helpful.

     

    I'm very glad that these things are taken care of with ULPs, and I very

    much appreciate the ability to add custom feature to the system, but

    sometimes I think that Eagle relies inappropriately on the availability

    of external ULPs.  I think you can make a very persuasive argument that

    there are just some core features that should be integrated into the

    package as it ships.  This is I think one of those cases.  Every other

    PCB layout system I've used has the ability to quickly locate these sort

    of unrouted nets.  I really don't mean to be too critical since I do

    like Eagle very much.

     

    Since your knowledge of ULPs seems very extensive, there is one more

    feature that I have looked for from the beginning but it seems to be

    absent.  I would like the ability to click on one copper feature, then a

    second copper feature, and have the tool tell me the straight line

    distance between the closest points on those two features on whatever is

    the "active" copper layer.  This is most useful when a board has to pass

    certain U.L., VDE or similar creepage requirements.  Is there a ULP that

    can do this?

     

    Michael

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    On 9/10/2010 3:28 PM, Michael Sansom wrote:

    Warren Brayshaw wrote:

    >

    >> Try these ULPs. There are others that produce text and script files but

    >> these enable you to locate the airwires quickly

    >> Once you choose your favourite ULP, add it to a Command Text menu

    >> button to

    >> your Board editor so you can check for airwires with a single click of

    >> the

    >> mouse.

    >>

    >> zoom-unrouted.ulp

    >> * simple script to zoom to the first unrouted wire in board editor.

    >> * this might be helpful when searching for tiny left-overs.

    >>

    >> statistic-brd.ulp

    >> *Unrouted count is in red in the summary section on the BOARD tab.

    >>

    >> length.ulp

    >> *This ULP calculates the signal length of routed tracks in the layout

    >> * airwires will be shown separately. Easily spotted in their own column

    >>

    >> Warren

    >>

    >

    Thanks Warren, these will be most helpful.

    >

    I'm very glad that these things are taken care of with ULPs, and I very

    much appreciate the ability to add custom feature to the system, but

    sometimes I think that Eagle relies inappropriately on the availability

    of external ULPs. I think you can make a very persuasive argument that

    there are just some core features that should be integrated into the

    package as it ships. This is I think one of those cases. Every other PCB

    layout system I've used has the ability to quickly locate these sort of

    unrouted nets. I really don't mean to be too critical since I do like

    Eagle very much.

    >

    Since your knowledge of ULPs seems very extensive, there is one more

    feature that I have looked for from the beginning but it seems to be

    absent. I would like the ability to click on one copper feature, then a

    second copper feature, and have the tool tell me the straight line

    distance between the closest points on those two features on whatever is

    the "active" copper layer. This is most useful when a board has to pass

    certain U.L., VDE or similar creepage requirements. Is there a ULP that

    can do this?

    >

    Michael

    >

    >

    don't know of a ULP to do this, but you can define a net class and it's

    clearance requirements in the DRC and assign both nets to that class and

    the DRC will check them for clearance violations. only problem is that

    this checks clearance to all other nets, rather than just the 2 you

    want, but this is generally desired anyway.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    On 9/10/2010 3:28 PM, Michael Sansom wrote:

    Warren Brayshaw wrote:

    >

    >> Try these ULPs. There are others that produce text and script files but

    >> these enable you to locate the airwires quickly

    >> Once you choose your favourite ULP, add it to a Command Text menu

    >> button to

    >> your Board editor so you can check for airwires with a single click of

    >> the

    >> mouse.

    >>

    >> zoom-unrouted.ulp

    >> * simple script to zoom to the first unrouted wire in board editor.

    >> * this might be helpful when searching for tiny left-overs.

    >>

    >> statistic-brd.ulp

    >> *Unrouted count is in red in the summary section on the BOARD tab.

    >>

    >> length.ulp

    >> *This ULP calculates the signal length of routed tracks in the layout

    >> * airwires will be shown separately. Easily spotted in their own column

    >>

    >> Warren

    >>

    >

    Thanks Warren, these will be most helpful.

    >

    I'm very glad that these things are taken care of with ULPs, and I very

    much appreciate the ability to add custom feature to the system, but

    sometimes I think that Eagle relies inappropriately on the availability

    of external ULPs. I think you can make a very persuasive argument that

    there are just some core features that should be integrated into the

    package as it ships. This is I think one of those cases. Every other PCB

    layout system I've used has the ability to quickly locate these sort of

    unrouted nets. I really don't mean to be too critical since I do like

    Eagle very much.

    >

    Since your knowledge of ULPs seems very extensive, there is one more

    feature that I have looked for from the beginning but it seems to be

    absent. I would like the ability to click on one copper feature, then a

    second copper feature, and have the tool tell me the straight line

    distance between the closest points on those two features on whatever is

    the "active" copper layer. This is most useful when a board has to pass

    certain U.L., VDE or similar creepage requirements. Is there a ULP that

    can do this?

    >

    Michael

    >

    >

    also it has been proposed that the DRC at least prominently warn the

    user that there are unrouted nets or that there are inactive, unchecked

    layers. not sure what became of this though...

     

    another proposal was to have a checklist of rats, drc and other

    necessary tests before running a CAM job, to make sure these things are

    caught before submitting gerbers.