Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) File Locking Fix on Mac Eagle 7.5.0
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 189 subscribers
  • Views 1551 views
  • Users 0 members are here
Related

File Locking Fix on Mac Eagle 7.5.0

lisamaxima
lisamaxima over 10 years ago

Hi Jorge,

 

I think I fixed the file locking problem on my Mac running Yosemite OS X and Eagle 7.5.0.

I posted about it online earlier.

 

I'm wondering if the fix could be as simple as requiring the user to open his schematics and

boards through the Eagle console while in an an open project, and defeating the user's ability

to open the schematic or board directly by clicking on it in the OS X Finder and thereby

bypassing opening the project.

 

Perhaps the schematic and board's System Open File With... Attribute could be set to an

auxiliary program that instead of opening it , tells the user to open it using Eagle in an open

project to not disturb the lock mechanism.

 

Could you check my post and see if there's a simpler solution in there?

 

Lisa

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    On 12/24/2015 7:14 PM, lisa fredrickson wrote:

    Hi Jorge,

     

    I think I fixed the file locking problem on my Mac running Yosemite OS X

    and Eagle 7.5.0.

    I posted about it online earlier.

     

    I'm wondering if the fix could be as simple as requiring the user to

    open his schematics and

    boards through the Eagle console while in an an open project, and

    defeating the user's ability

    to open the schematic or board directly by clicking on it in the OS X

    Finder and thereby

    bypassing opening the project.

     

    Perhaps the schematic and board's System Open File With... Attribute

    could be set to an

    auxiliary program that instead of opening it , tells the user to open it

    using Eagle in an open

    project to not disturb the lock mechanism.

     

    Could you check my post and see if there's a simpler solution in there?

     

    Lisa

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/170103

     

    Hi Lisa,

     

    There were a number of file-locking issues reported for the Mac

    platform. These have been addressed in our latest beta 7.5.1, if you

    could try it out and let me know if everything working that would be

    very helpful.

     

    Any feedback on the file-locking or any other feature of EAGLE is always

    welcome.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lisamaxima
    lisamaxima over 10 years ago in reply to autodeskguest

    I noticed another bug leftover from installation.  I had Eagle 6.4

    installed on

    my machine then installed 7.5.0.  I would create a new project in Eagle

    7.5.0.

    However, if I later started Eagle by clicking on the eagle.epf in the

    project folder,

    it started the earlier version of Eagle instead of the current version, and

    I could

    even end up with two versions running at the same time.  When you quit from

    the wrong

    version, it gives an error message about over-writnig the eagle.epf from

    another version

    of Eagle.

     

    On Mon, Dec 28, 2015 at 10:51 AM, lisa fredrickson <

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to lisamaxima

    On 12/28/2015 1:57 PM, lisa fredrickson wrote:

    I noticed another bug leftover from installation.  I had Eagle 6.4

    installed on

    my machine then installed 7.5.0.  I would create a new project in Eagle

    7.5.0.

    However, if I later started Eagle by clicking on the eagle.epf in the

    project folder,

    it started the earlier version of Eagle instead of the current version,

    and

    I could

    even end up with two versions running at the same time.  When you quit

    from

    the wrong

    version, it gives an error message about over-writnig the eagle.epf from

    another version

    of Eagle.

     

    Hello Lisa,

     

    This is probably not a bug but actually the intended behaviour. The .epf

    file stores all of the info about the last time the designed was opened,

    version of EAGLE, window positions, libraries in use, etc. If the last

    time that design was opened it was opened with 6.4 then the eagle.epf

    file would likely call for 6.4 to open it.

     

    Personally, I usually just open EAGLE and then from there open whatever

    I want to work on. When you have multiple versions of EAGLE installed

    this is usually easier than relying on the OS to figure out which

    version of EAGLE to call.

     

    hth,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lisamaxima
    lisamaxima over 10 years ago in reply to autodeskguest

    On the Mac, you change file association as follows:

     

    1. a. click on file, invoke File -> Get Info or b. right-click on file, ->

    Get Info

    2. the current (attempted) file association is shown in the Get Info dialog

    3. unlock the lock at the bottom of the Get Info dialog (requires admin or

    owner password)

    4. change the file association in the Get Info dialog

    5. if it won't change it:

    a. Check that the new association application is an allowed source in

    Applications -> System Preferences -> Security and Privacy

    b. If not, Allow from Anywhere

    c. change the file association in the Get Info dialog

    6. Lock the lock at the bottom of the Get Info dialog

    7. Go back to Applications -> System Preferences -> Security and Privacy

    and allow sources from identified developers only

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • lisamaxima
    lisamaxima over 10 years ago in reply to autodeskguest

    On the Mac, you change file association as follows:

     

    1. a. click on file, invoke File -> Get Info or b. right-click on file, ->

    Get Info

    2. the current (attempted) file association is shown in the Get Info dialog

    3. unlock the lock at the bottom of the Get Info dialog (requires admin or

    owner password)

    4. change the file association in the Get Info dialog

    5. if it won't change it:

    a. Check that the new association application is an allowed source in

    Applications -> System Preferences -> Security and Privacy

    b. If not, Allow from Anywhere

    c. change the file association in the Get Info dialog

    6. Lock the lock at the bottom of the Get Info dialog

    7. Go back to Applications -> System Preferences -> Security and Privacy

    and allow sources from identified developers only