Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Finding Components on a Schematic Design
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 187 subscribers
  • Views 5801 views
  • Users 0 members are here
Related

Finding Components on a Schematic Design

e14 Contributor
e14 Contributor over 15 years ago

Is there a way to find a specific component by typing a reference

designator that will have the schematic editor zoom in on that component

regardless of whether the component is on the current page or on a

different page on of the schematic.  I know that SHOW will highlight the

component, but if it's not on the current page or you've got a dense

schematic it is often difficult to see the highlight.  What I am looking

for is the ability to enter a ref des and have it automatically zoom to

that component no matter which page it is on.

 

Thanks

 

-Michael

 

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    BTW, is it possible to create your own button on the Eagle toolbar?

    I've assigned the find.ulp to be  F, which works nicely, but a

    toolbar button is a nice reminder for functions that are less frequently

    used.

     

    Thanks,

     

    -Michael

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago

    BTW, is it possible to create your own button on the Eagle toolbar?

    I've assigned the find.ulp to be  F, which works nicely, but a

    toolbar button is a nice reminder for functions that are less frequently

    used.

     

    Thanks,

     

    -Michael

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

     

    "Michael Sansom wrote

    BTW, is it possible to create your own button on the Eagle toolbar?

    I've assigned the find.ulp to be <CTRL> F, which works nicely, but a

    toolbar button is a nice reminder for functions that are less frequently

    used.

     

     

    You can customise the Command Text Menu which displays on the right of the

    editor window.

    If it is not displayed you can turn it on with Options/User Interface.

    Essentially, anything you can do from the command bar you can build a button

    to do and cascade other buttons from that button.

     

    By default Eagle comes with it pretty much duplicating the icons of the

    command button toolbar

    Read up on the Menu command and the section of the manual that illustrates

    the structure of the cascaded menu.

     

    Many strongly customise these text menus to perform many functions. Most

    often you modify your eagle.scr so that the appropriate customisation occurs

    in the Brd, Sch and Lib editors

     

    Attached is a script (crafted by the late Syd Levine). Run it and your

    Command Text menu will change and thus you'll see some of the possibilities.

    Clicking "Refresh Eagle.scr" within the menus will run your Eagle.scr and

    get you back to the way you were before running this script.

     

    Enjoy

    Warren

     

     

    begin 666 Analog3.scr

    M365N=2!!9&0@0V]P>2!$96QE=&4@1W)O=7 @+2!,87EE<B!-;W9E(%)E8W0@

    M4F]U=&4@4VEG;F%L(%-P;&ET(%1E>'0@5FEA(%=I<F4@)RTM+2<@)SLG("<M

    M2TG(%P-"D=R:60@7 T)T=R:60@061J=7-T('L@7 TC$P,"!'<FED("T@

    MC Q,"!!;'0@*"XQ,# @5FES:6)L92DZ($=R:60@C$P(#$[($=R:60@06QT

    M("XP,3L@?"!<#0HN,#4P($=R:60@2 N,#$P($%L=" HC$P,"!6:7-I8FQE

    M*3H@1W)I9" N,#4@,CL@1W)I9"!!;'0@+C Q.R!\(%P-"BXP,C4@1W)I9" M

    M("XP,3(U($%L=" H+C$P,"!6:7-I8FQE*3H@1W)I9" N,#(U(#0[($=R:60@

    M06QT("XP,3(U.R!\(%P-"BXP,C @1W)I9" M("XP,3 @06QT("@N,3 P(%9I

    M<VEB;&4I.B!'<FED("XP,B U.R!'<FED($%L=" N,#$[('P@7 T*06QT(%-E

    M='1I;F=S('L@7 T06QT("XQ,# Z($=R:60@06QT("XQ,# [('P@7 T06QT

    M("XP,3 Z($=R:60@06QT("XP,3 [('P@7 T*06QT("XP,#4Z($=R:60@06QT

    M("XP,#4[('P@7 T06QT("XP,C4Z($=R:60@06QT("XP,C4[('P@7 T06QT

    M("XP,3(U.B!'<FED($%L=" N,#$R-3L@?"!<#0I!;'0@+C P,3H@1W)I9"!!

    M;'0@+C P,3L@?"!<#0I!;'0@1FEN97-T.B!'<FED($%L="!&:6YE<W0[("!<

    M#0I]('P@7 T5FES:6)L92!'<FED('L@7 T3VXM3V9F(%1O9V=L93H@1W)I

    M9#L[('P@7 T3&EN97,Z($=R:60@3&EN97,@3VX[('P@7 T1&]T7,@,C8@,C@[('Q<#0IT1&]C=2!4;W @1&]C=2!4;V=G;&4@-3$Z(%)U;B!T

    M;V=L87ES(#4Q.R!\7 T*8D1O8W4@0F]T=&]M($1O8W4@5&]G9VQE(#4R.B!2

    M=6X@=&]G;&%Y<R U,CL@7 T*?2!\(%P-"E)E9G)E<V@@16%G;&4N<V-R.B!3

    I8W)I<'0@96%G;&4[7 T?2<@7 T)RTM+2<@7 T5W)I=&4@7 T.R `

    `

    end