EAGLE User Support (English) Swap level being ignored
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
  • Replies 6 replies
  • Subscribers 178 subscribers
  • Views 574 views
  • Users 0 members are here
Related

Swap level being ignored

Former Member
Former Member over 15 years ago

I have a library components (dual FET, Si4834BDY) that has two electrically

halves, yet the pin names are the same and number of pins are same for the

two halves. One FET has a schottky diode in parallel in from S-D, and one

FET does not.

 

I choose to use swap level 1 for each half, even though they are internally

different. The external pinouts are mirrors of each other.

 

What is the problem in allowing me to swap the two halves, so long as there

are similar pin assignments?

 

My sugggestion is, unless there is some commanding reason why you cannot do

so, then HONOR a request for swap-level = 1, and swap two electrically

different device halves - so long as the pin-assignments are the same, even

if those halves use two different symbols!

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 15 years ago

    "Brett Holden" wrote:

     

    >I have a library components (dual FET, Si4834BDY) that has two electrically

    >halves, yet the pin names are the same and number of pins are same for the

    >two halves. One FET has a schottky diode in parallel in from S-D, and one

    >FET does not.

    >I choose to use swap level 1 for each half, even though they are internally

    >different. The external pinouts are mirrors of each other.

    >What is the problem in allowing me to swap the two halves, so long as there

    >are similar pin assignments?

    >My sugggestion is, unless there is some commanding reason why you cannot do

    >so, then HONOR a request for swap-level = 1, and swap two electrically

    >different device halves - so long as the pin-assignments are the same, even

    >if those halves use two different symbols!

     

    since many years, my suggestion is to allow any swap on demand, IOW

    instead of the error message, there should be a dialog offering "swap

    anyway", maybe with some more information (see older postings, maybe

    in the German groups).

     

    And swaps should be possible from the board! Pinswaps are trivial,

    gateswap should highlight the pins belonging to the gate.

     

    Oliver

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    On 11/11/2010 11:30 PM, Oliver Betz wrote:

    "Brett Holden" wrote:

     

    >> I have a library components (dual FET, Si4834BDY) that has two electrically

    >> halves, yet the pin names are the same and number of pins are same for the

    >> two halves. One FET has a schottky diode in parallel in from S-D, and one

    >> FET does not.

    >>

    >> I choose to use swap level 1 for each half, even though they are internally

    >> different. The external pinouts are mirrors of each other.

    >>

    >> What is the problem in allowing me to swap the two halves, so long as there

    >> are similar pin assignments?

    >>

    >> My sugggestion is, unless there is some commanding reason why you cannot do

    >> so, then HONOR a request for swap-level = 1, and swap two electrically

    >> different device halves - so long as the pin-assignments are the same, even

    >> if those halves use two different symbols!

     

    since many years, my suggestion is to allow any swap on demand, IOW

    instead of the error message, there should be a dialog offering "swap

    anyway", maybe with some more information (see older postings, maybe

    in the German groups).

     

    And swaps should be possible from the board! Pinswaps are trivial,

    gateswap should highlight the pins belonging to the gate.

     

    Oliver

    yeah, and pinswaps would be nicer if they would swap the pins on the

    schematic instead of the nets, especially if initiated in board view.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    On 11/11/2010 11:30 PM, Oliver Betz wrote:

    "Brett Holden" wrote:

     

    >> I have a library components (dual FET, Si4834BDY) that has two electrically

    >> halves, yet the pin names are the same and number of pins are same for the

    >> two halves. One FET has a schottky diode in parallel in from S-D, and one

    >> FET does not.

    >>

    >> I choose to use swap level 1 for each half, even though they are internally

    >> different. The external pinouts are mirrors of each other.

    >>

    >> What is the problem in allowing me to swap the two halves, so long as there

    >> are similar pin assignments?

    >>

    >> My sugggestion is, unless there is some commanding reason why you cannot do

    >> so, then HONOR a request for swap-level = 1, and swap two electrically

    >> different device halves - so long as the pin-assignments are the same, even

    >> if those halves use two different symbols!

     

    since many years, my suggestion is to allow any swap on demand, IOW

    instead of the error message, there should be a dialog offering "swap

    anyway", maybe with some more information (see older postings, maybe

    in the German groups).

     

    And swaps should be possible from the board! Pinswaps are trivial,

    gateswap should highlight the pins belonging to the gate.

     

    Oliver

    yeah, and pinswaps would be nicer if they would swap the pins on the

    schematic instead of the nets, especially if initiated in board view.