I have a library components (dual FET, Si4834BDY) that has two electrically
halves, yet the pin names are the same and number of pins are same for the
two halves. One FET has a schottky diode in parallel in from S-D, and one
FET does not.
I choose to use swap level 1 for each half, even though they are internally
different. The external pinouts are mirrors of each other.
What is the problem in allowing me to swap the two halves, so long as there
are similar pin assignments?
My sugggestion is, unless there is some commanding reason why you cannot do
so, then HONOR a request for swap-level = 1, and swap two electrically
different device halves - so long as the pin-assignments are the same, even
if those halves use two different symbols!