Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) need to remove pads on a chip
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 189 subscribers
  • Views 4253 views
  • Users 0 members are here
Related

need to remove pads on a chip

e14 Contributor
e14 Contributor over 15 years ago

Need some assistance getting rid of four pads that should not exist, it is

messing with pcb-gcode and these pads are not nessesary.  Need to get this

done without messing up the consistency between the schematic and board.

 

These pads are not actually connected to pins but show up on the board, it

is a QFN28 chip and shows corner pads which dont actually do anything.

I wanted to attach a picture of what Im talking about but cant due to size

limit.

 

Thanks in advance.

Andy

 

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    On 11/8/10 9:32 AM, Andrew T wrote:

    Need some assistance getting rid of four pads that should not exist, it is

    messing with pcb-gcode and these pads are not nessesary.  Need to get this

    done without messing up the consistency between the schematic and board.

     

    These pads are not actually connected to pins but show up on the board, it

    is a QFN28 chip and shows corner pads which dont actually do anything.

    I wanted to attach a picture of what Im talking about but cant due to size

    limit.

     

    Thanks in advance.

    Andy

     

    >

    If you can locate the device AND the package of the IC, then you can

    delete the pads.  So, basically, the steps are:

     

     

    1. Make the EaglePart of the IC, just in case you have to refer that back.

     

    2. Open the *.lbr file that contains the device for the IC.

     

    3. Click on the Device button and select the device for that IC.

     

    4. Disconnect all the pins connected to the pads that you want to

    remove.  Save it.

     

    5. Click on the Package button and select the package for that IC.

     

    6. Right click on each of the pads you want to delete and delete it.

    Save the file.

     

    7. Click on the Symbol button and select the symbol for that IC.

     

    8. Right lick on each of the I/O pin that were created for the pads you

    just delete and delete those pins.  Save the file.

     

    9. Reload your schematic/brd files and select Library and update the

    *.lbr file that contains the IC package/device/symbol that you just

    modified per the above steps.

     

    Hope the above helps.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago

    On 11/8/10 9:32 AM, Andrew T wrote:

    Need some assistance getting rid of four pads that should not exist, it is

    messing with pcb-gcode and these pads are not nessesary.  Need to get this

    done without messing up the consistency between the schematic and board.

     

    These pads are not actually connected to pins but show up on the board, it

    is a QFN28 chip and shows corner pads which dont actually do anything.

    I wanted to attach a picture of what Im talking about but cant due to size

    limit.

     

    Thanks in advance.

    Andy

     

    >

    If you can locate the device AND the package of the IC, then you can

    delete the pads.  So, basically, the steps are:

     

     

    1. Make the EaglePart of the IC, just in case you have to refer that back.

     

    2. Open the *.lbr file that contains the device for the IC.

     

    3. Click on the Device button and select the device for that IC.

     

    4. Disconnect all the pins connected to the pads that you want to

    remove.  Save it.

     

    5. Click on the Package button and select the package for that IC.

     

    6. Right click on each of the pads you want to delete and delete it.

    Save the file.

     

    7. Click on the Symbol button and select the symbol for that IC.

     

    8. Right lick on each of the I/O pin that were created for the pads you

    just delete and delete those pins.  Save the file.

     

    9. Reload your schematic/brd files and select Library and update the

    *.lbr file that contains the IC package/device/symbol that you just

    modified per the above steps.

     

    Hope the above helps.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • siika
    siika over 8 years ago in reply to e14 Contributor

    I'm having issues on step 4-6:

    4. Disconnect all the pins connected to the pads that you want to remove.

    Save it.

     

    5. Click on the Package button and select the package for that IC.

     

    6. Right click on each of the pads you want to delete and delete it. Save

    the file.

    When I try to edit the device, I cannot find an option to disconnect pins from pads.
    I can right-click the package and click connect, here I can disconnect pin 2 from pad 2. When I try to delete the pad in the package, Eagle throws the following error:

    "Cannot delete pad 2 because it is connected to a pin"

     

    How do I disconnect pins from pads in the device?

     

    Best,

    F

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Got it and it worked correctly with no errors from it.  Thanks alot!

     

     

    "AL" <unbonnevie@yahoo.com> wrote in message

    news:ib9ddp$gst$1@cheetah.cadsoft.de...

    On 11/8/10 9:32 AM, Andrew T wrote:

    >> Need some assistance getting rid of four pads that should not exist, it

    >> is

    >> messing with pcb-gcode and these pads are not nessesary.  Need to get

    >> this

    >> done without messing up the consistency between the schematic and board.

    >>

    >> These pads are not actually connected to pins but show up on the board,

    >> it

    >> is a QFN28 chip and shows corner pads which dont actually do anything.

    >> I wanted to attach a picture of what Im talking about but cant due to

    >> size

    >> limit.

    >>

    >> Thanks in advance.

    >> Andy

    >>

    >>

    >>

    If you can locate the device AND the package of the IC, then you can

    delete the pads.  So, basically, the steps are:

     

    >

    1. Make the EaglePart of the IC, just in case you have to refer that back.

     

    2. Open the *.lbr file that contains the device for the IC.

     

    3. Click on the Device button and select the device for that IC.

     

    4. Disconnect all the pins connected to the pads that you want to remove.

    Save it.

     

    5. Click on the Package button and select the package for that IC.

     

    6. Right click on each of the pads you want to delete and delete it. Save

    the file.

     

    7. Click on the Symbol button and select the symbol for that IC.

     

    8. Right lick on each of the I/O pin that were created for the pads you

    just delete and delete those pins.  Save the file.

     

    9. Reload your schematic/brd files and select Library and update the *.lbr

    file that contains the IC package/device/symbol that you just modified per

    the above steps.

     

    Hope the above helps.