Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Bug in 7.3, can't export to TIF file
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 188 subscribers
  • Views 2981 views
  • Users 0 members are here
Related

Bug in 7.3, can't export to TIF file

autodeskguest
autodeskguest over 11 years ago

In version 7.3 on Windows 7 64 bit, there seems to be a bug in exporting a

board to a TIF image file.  In the board editor, if I run "EXPORT IMAGE

\temp\a.tif" I always get a popup that says "Out of memory while writing

'/temp/a.tif'".  This happens regardless of resolution.  For example,

"EXPORT IMAGE \temp\a.tif 50" fails the same way, even though that would

have only required 320 x 552 pixels in my case.

 

This is a important feature to me since that's how I make assembly

drawings.  The same procedure to make the same assembly drawing worked fine

in version 5.

 

 

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    Jorge Garcia wrote on Fri, 04 December 2015 12:49

    I have just now reported this to the devs.

     

     

    I just installed version 7.6, and this is still broken.

     

    What seems to be happening is that Eagle produces a TIFF file with CCITT

    (fax) compression when monochrome is checked.  It produces a more normal

    TIFF file when monochrome is unchecked, since CCITT is only for 1 bit per

    pixel images.  Lots of software doesn't support the ancient CCITT

    compression type of TIFF files, or interprets such files wrongly.  For

    example, if I open such a file from Eagle with MS Paint on a Windows 7

    system, it shows the values inverted.  The schematic lines are white and

    the background is black.

     

    Please just have Eagle produce TIFF files as it did in version 5.  I am

    disappointed that this wasn't fixed in version 7.6.

     

    Once again, DON'T MAKE GRATUITOUS CHANGES.  You will inevitably break

    something that someone has relied on.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    Jorge Garcia wrote on Fri, 04 December 2015 12:49

    I have just now reported this to the devs.

     

     

    I just installed version 7.6, and this is still broken.

     

    What seems to be happening is that Eagle produces a TIFF file with CCITT

    (fax) compression when monochrome is checked.  It produces a more normal

    TIFF file when monochrome is unchecked, since CCITT is only for 1 bit per

    pixel images.  Lots of software doesn't support the ancient CCITT

    compression type of TIFF files, or interprets such files wrongly.  For

    example, if I open such a file from Eagle with MS Paint on a Windows 7

    system, it shows the values inverted.  The schematic lines are white and

    the background is black.

     

    Please just have Eagle produce TIFF files as it did in version 5.  I am

    disappointed that this wasn't fixed in version 7.6.

     

    Once again, DON'T MAKE GRATUITOUS CHANGES.  You will inevitably break

    something that someone has relied on.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    Jorge Garcia wrote on Fri, 04 December 2015 12:49

    I have just now reported this to the devs.

     

     

    I just installed version 7.6, and this is still broken.

     

    What seems to be happening is that Eagle produces a TIFF file with CCITT

    (fax) compression when monochrome is checked.  It produces a more normal

    TIFF file when monochrome is unchecked, since CCITT is only for 1 bit per

    pixel images.  Lots of software doesn't support the ancient CCITT

    compression type of TIFF files, or interprets such files wrongly.  For

    example, if I open such a file from Eagle with MS Paint on a Windows 7

    system, it shows the values inverted.  The schematic lines are white and

    the background is black.

     

    Please just have Eagle produce TIFF files as it did in version 5.  I am

    disappointed that this wasn't fixed in version 7.6.

     

    Once again, DON'T MAKE GRATUITOUS CHANGES.  You will inevitably break

    something that someone has relied on.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    On 12/2/2015 9:05 AM, Olin Lathrop wrote:

    I'm now at version 7.5.0, and this is indeed fixed.

     

    However, you broke something else in the process.  Now the TIF file gets

    written using CCITT (old fax) compression when the monochrome box is

    checked.  This was never the case before.  Lots of software doesn't handle

    this compression scheme, including what I call from ULPs and scripts to do

    various things.  LZW compression or LZW with forward differencing are fine

    and pretty much universally supported.

     

    PLEASE RETURN THE TIF FILE WRITING FEATURE TO THE WAY IT WAS IN VERSION 5.

     

    Hi Olin,

     

    Sorry for the delay, haven't been able to get to the forums the last few

    days.

     

    I have just now reported this to the devs.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    CadSoft Support wrote on Mon, 27 July 2015 07:53

    This seems to be a problem that came with the newer Qt version

    we are using since EAGLE 7.3.0. We will check this......

     

     

    I'm now at version 7.5.0, and this is indeed fixed.

     

    However, you broke something else in the process.  Now the TIF file gets

    written using CCITT (old fax) compression when the monochrome box is

    checked.  This was never the case before.  Lots of software doesn't handle

    this compression scheme, including what I call from ULPs and scripts to do

    various things.  LZW compression or LZW with forward differencing are fine

    and pretty much universally supported.

     

    PLEASE RETURN THE TIF FILE WRITING FEATURE TO THE WAY IT WAS IN VERSION 5.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    I just installed latest Eagle for 64-bit Linux with the Element 14 free trial key on an Xubuntu 14.04 LTS x64 stable system.  When I try to export the Arduino project to ANY graphics format, I get the same result i.e. "Out of memory while writing ...".  So, this is not just Windows.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago

    Am 24.07.2015 um 14:35 schrieb Olin Lathrop:

    In version 7.3 on Windows 7 64 bit, there seems to be a bug in exporting a

    board to a TIF image file.  In the board editor, if I run "EXPORT IMAGE

    \temp\a.tif" I always get a popup that says "Out of memory while writing

    '/temp/a.tif'".  This happens regardless of resolution.  For example,

    "EXPORT IMAGE \temp\a.tif 50" fails the same way, even though that would

    have only required 320 x 552 pixels in my case.

     

     

    This seems to be a problem that came with the newer Qt version

    we are using since EAGLE 7.3.0. We will check this......

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<