EAGLE User Support (English) Escape key functionality?
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
  • Replies 6 replies
  • Subscribers 178 subscribers
  • Views 543 views
  • Users 0 members are here
Related

Escape key functionality?

Former Member
Former Member over 15 years ago

I asked before but I will ask again. Could you guys please make it so that

two taps of the ESCAPE betton will totally deactivate the MOVE command (or

any other command).

 

Apparently, your Options >SET >Misc Select factor ( % ) has no bearing on a

group, so that means that an accidental R-click of the mouse will move a

group, even with 2% "Select Factor", and even if the R-click was from planet

Pluto.

 

Being able to tap the escape key is sometimes much easier than having to use

the mouse to click the STOP button, except that it doesn't always work. The

Move command will stay active, even after 10 taps on the escape key. Is

there reason behind that?

 

I sorry, that was a rhetorical question.

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 15 years ago

     

    "Brett Holden"  wrote

    I asked before but I will ask again. Could you guys please make it so that

    two taps of the ESCAPE betton will totally deactivate the MOVE command (or

    any other command).

     

     

    I agree.

    The escape key action needs to be improved. The design decision for the

    level it currently escapes back to is wrong and it  should successively

    escape back to the "no command selected" state.

     

    Appreciating all the Eagle functionality around the Escape key it is not a

    matter of how many hits of the Escape key are needed to achieve a  result

    but a matter of the true functionality of that key.

    Brett asks for two hits of the key to get back to the idle state of no

    command selected. There is a situation where three hits would be required so

    its not the number of hits but the need to ESCAPE to the previous level.

    If you establish the idle "no command selected" state as the highest level,

    the escape key should take you there, step by step, hit by hit.

    Currently it stops one step short. It is inefficient to mouse click the stop

    button, a Text Command button  or type a ";" in the command line. The

    quickest alternate is an Assigned key (say Alt + Q) but that is still

    clumsy.

     

    Being able to get to a "no command selected" state, easily, is high on my

    want list.

    Correcting this oddity would be time well spent.

     

    Warren

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    warrenbrayshaw wrote on Sat, 13 November 2010 15:30

    It is inefficient to mouse click the stop button, a Text Command button

    or type a ";" in the command line.

     

    This makes no sense.  It only takes two key strokes (";", Enter) to end any

    command.  Whether those two key strokes are semicolon-Enter or Esc-Esc

    makes very little difference to the work flow.

     

    In fact I've gotten used to ESC escapes out to a certain level, which is

    easy to hit with the left hand.  Semi-Enter is just as easy to hit with the

    right hand.  It may be two key strokes, but it's one operation in the

    brain.  There is nothing to "fix" here, and trying would just break things.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    warrenbrayshaw wrote on Sat, 13 November 2010 15:30

    It is inefficient to mouse click the stop button, a Text Command button

    or type a ";" in the command line.

     

    This makes no sense.  It only takes two key strokes (";", Enter) to end any

    command.  Whether those two key strokes are semicolon-Enter or Esc-Esc

    makes very little difference to the work flow.

     

    In fact I've gotten used to ESC escapes out to a certain level, which is

    easy to hit with the left hand.  Semi-Enter is just as easy to hit with the

    right hand.  It may be two key strokes, but it's one operation in the

    brain.  There is nothing to "fix" here, and trying would just break things.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    Olin Lathrop schrieb:

     

    warrenbrayshaw wrote on Sat, 13 November 2010 15:30

    >> It is inefficient to mouse click the stop button, a Text Command button

    >>  or type a ";" in the command line.

     

    This makes no sense.  It only takes two key strokes (";", Enter) to end any

    command.  Whether those two key strokes are semicolon-Enter or Esc-Esc

    makes very little difference to the work flow.

     

    Please consider the different keyboard layouts. With my german keyboard,

    the semicolon is on top of the comma, so I need to press shift-comma for

    it. With the right hand continuously on the trackball, this is

    extremely uncomfortable to reach with only the left hand.

     

    Hitting ESC once, twice or any other count is far easier - and more

    intuitive, anyway.

     

    In fact I've gotten used to ESC escapes out to a certain level, which is

    easy to hit with the left hand.  Semi-Enter is just as easy to hit with the

    right hand.  It may be two key strokes, but it's one operation in the

    brain.  There is nothing to "fix" here, and trying would just break things.

     

    It is much more comfortable to use only the left hand for single

    keyboard actions, so the right hand can stay on the trackball.

     

    That said, I don't see a really urgent need for any change. For me and

    in most cases, ESC does what is expected. I rarely need to STOP any

    command, most of the time I simply activate the next command - most

    often by pressing the related function key (with the left hand, of

    course, to keep the right hand at the trackball image ).

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    Tilmann Reh wrote on Wed, 29 December 2010 08:17

    That said, I don't see a really urgent need for any change. For me and

    in most cases, ESC does what is expected. I rarely need to STOP any

    command, most of the time I simply activate the next command - most

    often by pressing the related function key (with the left hand, of

    course, to keep the right hand at the trackball image ).

     

    I agree in that ending a command is a relatively rare operation.  There is

    really no problem here to solve.

     

    Most of the time I do what you do.  The right hand is on the mouse and the

    left hand hits function keys I have set up for the common operations.  For

    example, in the board editor F12 does a RATSNEST and MOVE.  F8 does a

    RATSNEST and ROUTE.  F9, F10, and F11 change the grid to different

    finenesses, etc.

     

    The times I can remember doing ;-Enter is for cancelling a SHOW, or ending

    a WIRE sometimes.  There are probably a few other instances, but they are

    rare enough I'm not looking for a quicker way to do them.  Even then, I

    should be able to set up a function key if that's what I really wanted.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.