Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Newbie struggling with making edge connector
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 190 subscribers
  • Views 6144 views
  • Users 0 members are here
Related

Newbie struggling with making edge connector

oldtech1000
oldtech1000 over 10 years ago

Hi,

I am having trouble trying to make an edge connector in eagle.

I wish to make a PCB that plugs into a 20 pin edge connector, to make an extender board.

The board consists of only 20 tracks with a spacing of 0.1 inches. No components, just the tracks.

Have not been able to find anything in libraries,tried to modify other connectors but all appear to want me

to connect to other components (other than the tracks).

I am sure this is very easy for experience Eagle users but not obvious to a very New Newbie like me.

Thanks for your help

Regards

George

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    On 01/19/2016 04:59 AM, George LIVANES wrote:

    Hi,

    I am having trouble trying to make an edge connector in eagle.

    I wish to make a PCB that plugs into a 20 pin edge connector, to make an

    extender board.

    The board consists of only 20 tracks with a spacing of 0.1 inches. No

    components, just the tracks.

    Have not been able to find anything in libraries,tried to modify other

    connectors but all appear to want me

    to connect to other components (other than the tracks).

    I am sure this is very easy for experience Eagle users but not obvious

    to a very New Newbie like me.

    Thanks for your help

    Regards

    George

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/171865

     

    Assuming you need a male end and will be adding a female to the other side.

    Use smd pads to make the connector(s).

    See some of the db style connectors for an example of a edge mounted

    connector.

    Paul R.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • oldtech1000
    oldtech1000 over 10 years ago in reply to autodeskguest

    Hi Paul,

    Thanks for the reply.

    I tried this approach, using some small round pads I found and joined them with the wire command (made them a thick wire).

    However, when I went to lay out the PCB I had trouble moving some of the pads (I error checked it in the schematic). Some pads I could

    move into the box and some would not.

    I think that I kept the schematic in the allowable 100mm by 80mm for eagle light...Is there any way of checking if you have put schematics

    correctly into the allowable area for eagle lite ?

    Regards

    George

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to oldtech1000

    On 20/01/2016 2:30 p.m., George LIVANES wrote:

    Hi Paul,

    Thanks for the reply.

    I tried this approach, using some small round pads I found and joined

    them with the wire command (made them a thick wire).

    However, when I went to lay out the PCB I had trouble moving some of the

    pads (I error checked it in the schematic). Some pads I could

    move into the box and some would not.

    I think that I kept the schematic in the allowable 100mm by 80mm for

    eagle light...Is there any way of checking if you have put schematics

    correctly into the allowable area for eagle lite ?

    Regards

    George

     

     

    Hi

    Probably with a bit more information about what exactly you are

    endeavouring to create we could help.

     

    Will it be of this style

    http://www.jfmeng.com/extender_board.html

    If so what is the connector at the top?

     

    Have a look at the library that comes with Eagle for ideas

    con-pc.lbr

     

    Will you be etching at home or do you need a professional board with

    hard gold plating on the pins?

     

    The Eagle size restriction only applies to the Board Editor so the board

    can, at maximum, only be 100mm wide and 80mm tall.

     

    You could build an extender, like the one pictured in the link above,

    larger than 100x80 using the limited version if you approached it correctly.

     

    So provide a lot more detail on connectors and size, single sided/

    double sided. A picture of the socket you will plug into would all help.

     

    Warren

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to oldtech1000

    On 22/01/2016 2:50 p.m., George LIVANES wrote:

    Hi Warren,

    Thanks for the help.

    Yes, the extender i am trying to make looks exactly like this picture

    (Double sided).

    The edge connector is called a "PCB card edge connector" and are a

    simple 2 row connector.

    These extenders were very commonly used to service Tektronix and HP test

    equipment in the 70's.

    The one i'm making will have 20pins a side (40 pins total) and the pins

    on the connector are spaced 3.96mm apart (0.156 inches).

    I will etch the pcb at home but will not use gold plating.

    Regards

    George

     

     

    Hi George

    I too have used many of this style of extender board.

    I would build this using only the board editor.

    The advantage with the approach taken is that you can use Eagle Lite and

    make it as big as you like because you have no element origins or smds

    to keep within the limitations.

     

    The drawing skills needed are the same whether you do the actions in the

    package editor or directly to the board.

     

    I do feel some of the skills are a little beyond novice but basic and

    attainable with practice.

     

    I had a go and have attached a board which may be close to what you end

    up with.

    I did not know the width you needed and that would have made it easier

    to do that up front rather than get it right now.

     

    All you need to do to get the height right is group the area at the top

    and drag it to the desired height.

     

    As you will etch at home it's all copper plus extra to cut to.

    The is an outline that was established to help place the  cut-to copper

    areas which are rectangles

    There are some dimension on the documentation layer, turn that off

    before creating you etch mask

     

    The top and bottom are the same although this example is not symmetrical

    so watch out for that.View only the top and bottom layer separately to

    see that they are the same.

     

    The traces are simply wires of two different widths

     

    Placement and lengths is done easily by planning well and manipulating

    the grid size. That way you don't have to do any maths.

    From your description and a data sheet I created the edge connector

    tongue. That was the trickiest part. Establish construction lines and

    then trim them to  leave the step shape.

     

    So have a go

    Let us know if you get stuck

     

    Warren

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 10 years ago in reply to oldtech1000

    On 22/01/2016 2:50 p.m., George LIVANES wrote:

    Hi Warren,

    Thanks for the help.

    Yes, the extender i am trying to make looks exactly like this picture

    (Double sided).

    The edge connector is called a "PCB card edge connector" and are a

    simple 2 row connector.

    These extenders were very commonly used to service Tektronix and HP test

    equipment in the 70's.

    The one i'm making will have 20pins a side (40 pins total) and the pins

    on the connector are spaced 3.96mm apart (0.156 inches).

    I will etch the pcb at home but will not use gold plating.

    Regards

    George

     

     

    Hi George

    I too have used many of this style of extender board.

    I would build this using only the board editor.

    The advantage with the approach taken is that you can use Eagle Lite and

    make it as big as you like because you have no element origins or smds

    to keep within the limitations.

     

    The drawing skills needed are the same whether you do the actions in the

    package editor or directly to the board.

     

    I do feel some of the skills are a little beyond novice but basic and

    attainable with practice.

     

    I had a go and have attached a board which may be close to what you end

    up with.

    I did not know the width you needed and that would have made it easier

    to do that up front rather than get it right now.

     

    All you need to do to get the height right is group the area at the top

    and drag it to the desired height.

     

    As you will etch at home it's all copper plus extra to cut to.

    The is an outline that was established to help place the  cut-to copper

    areas which are rectangles

    There are some dimension on the documentation layer, turn that off

    before creating you etch mask

     

    The top and bottom are the same although this example is not symmetrical

    so watch out for that.View only the top and bottom layer separately to

    see that they are the same.

     

    The traces are simply wires of two different widths

     

    Placement and lengths is done easily by planning well and manipulating

    the grid size. That way you don't have to do any maths.

    From your description and a data sheet I created the edge connector

    tongue. That was the trickiest part. Establish construction lines and

    then trim them to  leave the step shape.

     

    So have a go

    Let us know if you get stuck

     

    Warren