Hi
i am trying to genrate gerber file but its taking too long 6 hours to generate that please suggest what can be done any help wil be appreciated
Hi
i am trying to genrate gerber file but its taking too long 6 hours to generate that please suggest what can be done any help wil be appreciated
On 20.01.2016 10:08, karan mittal wrote:
Hi
i am trying to genrate gerber file but its taking too long 6 hours
to generate that please suggest what can be done any help wil be
appreciated
My guess is that you got large filled polygons with width=0..
They will create enormous amount of data, as eagle will use its minimum
"pen" width to fill them.
It has reduced but still its getting slow .and one thing when I open my
file it opens too much zoomed out.
It has reduced but still its getting slow .and one thing when I open my
file it opens too much zoomed out.
On 20.01.2016 11:20, karan mittal wrote:
It has reduced but still its getting slow .and one thing when I open my
file it opens too much zoomed out.
Make sure your design is drawn to scale, and make sure the polygon wire
widht is a reasonable size (I'd sayt max 0.2mm, but its really up to
what your board manufacturer can handle of tools and details).
Check if your gerber file size is within a reasonable size. If its huge,
you most likely have more polygons with too small width.
You can use the statistic-brd.ulp to get an overview of your board.
Check the polygon tab.
And dont forget to run DRC.
On 20/01/2016 11:20 p.m., karan mittal wrote:
.........and one thing when I open my
file it opens too much zoomed out.
That suggests that you have an outlying object.
The result of that is your gerber will be the size of area the board
design is covering. Probably huge.
If so you need to find the objects outside your board are and delete them
HTH
Warren
Am 21.01.2016 um 06:02 schrieb warrenbrayshaw:
On 20/01/2016 11:20 p.m., karan mittal wrote:
.........and one thing when I open my
file it opens too much zoomed out.
That suggests that you have an outlying object.
The result of that is your gerber will be the size of area the board
design is covering. Probably huge.
If so you need to find the objects outside your board are and delete them
HTH
Warren
Additional to Warren I might suggest that if you don't find your outside
object you should transfer your project into a new project.
That sounds silly but sometimes some "Ghost Objects" arise.
I have never been able to identify these "objects" nor delete them 
The only way was the transfer into a new project.
Hope that helps.
--
Mit freundlichen Grüßen / With best regards
Joern Paschedag
That thing is solved other thing is I want to set inner layer clearance
different from outer layer can you help
On 22/01/2016 9:40 p.m., karan mittal wrote:
That thing is solved other thing is I want to set inner layer clearance
different from outer layer can you help
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/172176
Please start a new thread when the subject is different.
As for the answer. Eagle cannot do that
Warren