Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Using the ARC command
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 179 subscribers
  • Views 1523 views
  • Users 0 members are here
Related

Using the ARC command

Former Member
Former Member over 14 years ago

I have spent yesterday afternoon and this morning trying to understand how

to use the ARC command on the command line with no luck. All I want to do

is to draw and arc of radius 0.5" centered at 0.5", 1.7" with a specific

line width.

 

The eagle manual is of no help because the description of the command is

too cryptic for me to understand. Can anyone help me understand how to do

this?

 

Any enlightenment will be appreciated.

 

Vic

--

Vic Fraenckel

KC2GUI

windswaytoo ATSIGN gmail DOT com

 

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 14 years ago

    Am 25.01.2011 16:20, schrieb Victor Fraenckel:

    I have spent yesterday afternoon and this morning trying to understand how

    to use the ARC command on the command line with no luck. All I want to do

    is to draw and arc of radius 0.5" centered at 0.5", 1.7" with a specific

    line width.

    The eagle manual is of no help because the description of the command is

    too cryptic for me to understand. Can anyone help me understand how to do

    this?

     

    Any enlightenment will be appreciated.

     

    Vic

     

     

     

    Hi Vic,

     

    there are various options, for example:

     

    Set a relative origin first and then use the WIRE command which can draw

    arcs as well. You can use for example polar coordinates.....

     

     

    MARK (0.5 1.7);            # relative origin

    WIRE (P 0.5 0)  @+0.5  (P 0.5 90);   # polar starting point, radius,

                                            ending point of the arc

     

    inside ( ):  P for polar coordinates,

                  first value: radius from the origin, second: angle)

     

     

    2nd example with relative coodinates:

     

      MARK (0.5 1.7);            # relative origin

      WIRE (R0 0.5)  -90  (R0.5 0)    # relative starting point, curve,

                                        relative ending point

     

     

    Please see details about the syntax with radius and curve in the help of

    the WIRE command and Editor Commands/Command Syntax.

     

    I hope this helps.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago

    Victor Fraenckel schrieb:

     

    I have spent yesterday afternoon and this morning trying to understand how

    to use the ARC command on the command line with no luck. All I want to do

    is to draw and arc of radius 0.5" centered at 0.5", 1.7" with a specific

    line width.

     

    The eagle manual is of no help because the description of the command is

    too cryptic for me to understand. Can anyone help me understand how to do

    this?

     

    Did you also have a loop at HELP ARC, and did you realize how manually

    drawing ARCs works?

    You need to know that the command line syntax exactly follows the "mouse

    click syntax". At the command line, you simply provide coordinates as if

    they were clicked by mouse.

     

    You need to provide three coordinates: The first is the beginning of the

    ARC, the second is exactly the opposite side of the ARC (say, at 180

    degrees) - so your "center" coordinate is defined as the position right

    (centered) between those two coordinates.

    The third coordinate, finally, defines the angle of the ARC (related to

    the center) - regardless if it's on the ARC diameter or not.

     

    So, if you enter

         ARC 0.1 (-1 0) (1 0) (1 1);

    you'll get an ARC of width 0.1, starting at (-1 0) which is the first

    given coordinate, centered at (0 0) which is exactly halfway between the

    first two coordinates, and ending at 45 degrees (defined by the third

    coordinate).

     

    You didn't mention starting and ending angle of the ARC you need, so I

    can't provide a working command for your particular need. However,

    assuming you need a 180° arc, the command would look like:

         grid inch;

         arc  (0 1.7) (1 1.7) (1 1.7);

    You can specify the direction of the ARC with "CW" and "CCW" parameters.

     

    Tilmann