Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) How to create library part with thermal pad?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 55 replies
  • Subscribers 189 subscribers
  • Views 7639 views
  • Users 0 members are here
Related

How to create library part with thermal pad?

e14 Contributor
e14 Contributor over 15 years ago

Hi there,

 

I was hoping someone could give me the recommended flow for creating a

library package with a thermal pad.  I'm using an LME49600TS/NOPBLME49600TS/NOPB which has 5

pins and a thermal pad.  The pad is electrically connected internally

to Vee.

 

I initially tried just marking a tStop region in the shape of the pad

hoping that if I just drew a polygon over it in the layout editor and

hit ratsnest, all would work out.  All I got was a polygon around the

pad not connected to it.

 

I then tried to draw a polygon in the package and name it something but

I discovered you can't name polygons.  A square pad would work I guess

but this isn't the shape of the pad which is in the shape of a 'T'.

 

Any pointers on the correct way of doing this?  The demo board doesn't

have the pad polygon connected to the Vee pin so that shouldn't be an

issue.

 

Thanks, Shareef.

 

 

  • Sign in to reply
  • Cancel
Parents
  • justinhotban
    justinhotban over 9 years ago

    I think you should use SinoGuide TCP110U thermal pad for test, one side with fiberglass reinforcement;  TCP110U has a 1.1 W/mK thermal conductivity for exceptionally low thermal resistance. Naturally tacky on one side for easy assembly,  A special resin material that is easy to pull from the liner and place in the application enhances handling.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • justinhotban
    justinhotban over 9 years ago

    I think you should use SinoGuide TCP110U thermal pad for test, one side with fiberglass reinforcement;  TCP110U has a 1.1 W/mK thermal conductivity for exceptionally low thermal resistance. Naturally tacky on one side for easy assembly,  A special resin material that is easy to pull from the liner and place in the application enhances handling.