Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) "Flip View" button
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 38 replies
  • Subscribers 189 subscribers
  • Views 6307 views
  • Users 0 members are here
Related

"Flip View" button

e14 Contributor
e14 Contributor over 15 years ago

When routing the back of a board, it would be really nice to be able to

flip the view to see the back of the board as it really is.

 

It would be extremely useful when debugging a board, as it's really painful

to find a signal in eagle, then mentally flip it to find it on the physical

board.

 

It would also be useful for checking text layout on the back of the board.

Mentally flipping text is a bit of a pain, and almost impossible when

you're trying to evaluate its aesthetic appeal. Yes, I do consider

aesthetics important in PCB design!

 

I know I can print out the board mirrored, or group-then-mirror, and

various other hacks, but if this button existed, I'd click it every minute

or so when routing a complex design.

 

In fact, I'd prefer the board view to immediately mirror when I changed

routing layer to add a via! Other people probably wouldn't, so this would

have to be an option that defaulted to "off".

 

I've been using eagle for ten years, always wanting this feature, but only

just realised there was a suggestions forum!

 

gEDA, Orcad, Altium Designer, and probably others support this so I can't

be alone in desiring this feature! (see

http://wiki.altium.com/display/ADOH/AltiumDesignerViewer-ViewingPCBDocuments#AltiumDesignerViewer-ViewingPCBDocuments-FlippingtheBoard

for example)

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    +1 For quick board flip in view.  Board flip should also draw layers so that bottom obscures top layers, this would make routing traces and placing text on bottom just as easy as on top.

     

    ULP is not a good solution.  I just script ran it twice and diff'ed the before and after, and there some missing vertex's in the board that was flipped twice.  

    As mentioned before, this doesn't work when there are locked components (although the script could probably updated to fix this).

     

    The script I used:

    https://github.com/sparkfun/SparkFun_Eagle_Settings/blob/master/ulp/mirror-board.ulp

     

    The before and after diff showing some missing vertex lines:

    @@ -3502,14 +3502,12 @@

    </polygon>

    <polygon width="0.254" layer="16" thermals="no">

    <vertex x="71.247" y="27.559"/>

    -<vertex x="82.677" y="27.559"/>

    <vertex x="82.931" y="27.559"/>

    <vertex x="82.931" y="15.367"/>

    <vertex x="71.247" y="15.367"/>

    </polygon>

    <polygon width="0.254" layer="16" thermals="no">

    <vertex x="71.12" y="51.435"/>

    -<vertex x="82.55" y="51.435"/>

    <vertex x="82.804" y="51.435"/>

    <vertex x="82.804" y="39.243"/>

    <vertex x="71.12" y="39.243"/>

    @@ -3945,7 +3943,6 @@

    <wire x1="30.039" y1="18.626" x2="30.039" y2="18.126" width="0.3048" layer="16"/>

    <polygon width="0.254" layer="16" thermals="no">

    <vertex x="29.972" y="34.163"/>

    -<vertex x="29.972" y="32.893"/>

    <vertex x="29.972" y="32.766"/>

    <vertex x="31.369" y="32.766"/>

    <vertex x="31.369" y="34.163"/>

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kikoun
    kikoun over 11 years ago in reply to e14 Contributor

    hello,

     

    That would be a great feature for 2 particular task:

    - adjust text on bottom (silk layer)

    - debugging a board. (I know, I know, I can print, but on a printed paper highlight and search feature is very very limited...)

     

    Just one thing: a good visible indication must warn us if this mirrored mode is activated.

     

    Guillaume.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kikoun
    kikoun over 11 years ago in reply to e14 Contributor

    hello,

     

    That would be a great feature for 2 particular task:

    - adjust text on bottom (silk layer)

    - debugging a board. (I know, I know, I can print, but on a printed paper highlight and search feature is very very limited...)

     

    Just one thing: a good visible indication must warn us if this mirrored mode is activated.

     

    Guillaume.